<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX8Nano compactible RAM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8Nano-compactible-RAM/m-p/1852116#M222843</link>
    <description>&lt;P&gt;Hi Rajanand,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;well in that case this RAM should be suitable for IMX8PLUS designs right. As you mentioned that the RAM should be LPDDR4 or LPDDR4/LPDDR4X. But not LPDDR4X alone.&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;Yes, that is correct.&lt;/SPAN&gt;&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;So, I guess this RAM satisfies the condition and is there anything else I need to consider making the design to work properly?&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;Yes, just with the DRAM bus width caveat in case of i.MX8MNano. For more considerations regarding the design, please refer to the Hardware Developer's Guide.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jan&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 23 Apr 2024 05:47:40 GMT</pubDate>
    <dc:creator>jan_spurek</dc:creator>
    <dc:date>2024-04-23T05:47:40Z</dc:date>
    <item>
      <title>i.MX8Nano compactible RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8Nano-compactible-RAM/m-p/1851673#M222822</link>
      <description>&lt;P&gt;&lt;SPAN&gt;As a student exploring the i.MX8 series processor platform, I'm facing a challenge in selecting the right RAM for my application. After consulting&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/104383"&gt;@jan_spurek&lt;/a&gt;&amp;nbsp;'s&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-8M-Quad-8M-Mini-8M-Nano-8M-Plus-LPDDR4-DDR4-and-DDR3L/ta-p/1434761" target="_blank" rel="noopener"&gt;&amp;nbsp;RAM selection guide&lt;/A&gt;, I decided on the MT53E1G32D2FW-046 (1Gx32) 4GB module for my i.MX8Nano design. I would appreciate it if you could validate this RAM choice or provide guidance on the key aspects and specifications to consider for RAM selection if it's not compatible.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 14:04:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8Nano-compactible-RAM/m-p/1851673#M222822</guid>
      <dc:creator>Rajanand</dc:creator>
      <dc:date>2024-04-22T14:04:48Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8Nano compactible RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8Nano-compactible-RAM/m-p/1851692#M222824</link>
      <description>&lt;P&gt;Hi Rajanand,&lt;/P&gt;
&lt;P&gt;thank you for the question. Please attach the respective datasheet of the selected memory device so compatibility could be checked in more detail.&lt;/P&gt;
&lt;P&gt;From the available information, the selected device appears to have 32-bit wide data bus while i.MX8MNano only has 16-bit DRAM data bus. This is not a big functional problem in case of LPDDR4 as the 32-bit wide devices consist of two independent 16-bit channels and only one of them can be used. However, you would only be able to access half of its density - so only 2 out of 4 GB would be available. From this reason, it looks more practical to look for 16-bit LPDDR4 devices.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Jan&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 14:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8Nano-compactible-RAM/m-p/1851692#M222824</guid>
      <dc:creator>jan_spurek</dc:creator>
      <dc:date>2024-04-22T14:09:09Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8Nano compactible RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8Nano-compactible-RAM/m-p/1851698#M222825</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/104383"&gt;@jan_spurek&lt;/a&gt;&amp;nbsp;Thank you,&lt;BR /&gt;well in that case this RAM should be suitable for IMX8PLUS designs right. As you mentioned that the RAM should be LPDDR4 or LPDDR4/LPDDR4X. But not LPDDR4X alone.&lt;BR /&gt;&lt;BR /&gt;So, I guess this RAM satisfies the condition and is there anything else I need to consider making the design to work properly?&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 14:17:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8Nano-compactible-RAM/m-p/1851698#M222825</guid>
      <dc:creator>Rajanand</dc:creator>
      <dc:date>2024-04-22T14:17:56Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8Nano compactible RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8Nano-compactible-RAM/m-p/1852116#M222843</link>
      <description>&lt;P&gt;Hi Rajanand,&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;well in that case this RAM should be suitable for IMX8PLUS designs right. As you mentioned that the RAM should be LPDDR4 or LPDDR4/LPDDR4X. But not LPDDR4X alone.&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;Yes, that is correct.&lt;/SPAN&gt;&lt;/P&gt;
&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;So, I guess this RAM satisfies the condition and is there anything else I need to consider making the design to work properly?&lt;/SPAN&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;
&lt;P&gt;&lt;SPAN&gt;Yes, just with the DRAM bus width caveat in case of i.MX8MNano. For more considerations regarding the design, please refer to the Hardware Developer's Guide.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Jan&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 23 Apr 2024 05:47:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8Nano-compactible-RAM/m-p/1852116#M222843</guid>
      <dc:creator>jan_spurek</dc:creator>
      <dc:date>2024-04-23T05:47:40Z</dc:date>
    </item>
  </channel>
</rss>