<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックAsynchronous operation(clEnqueueMapBuffer) is not working properly</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Asynchronous-operation-clEnqueueMapBuffer-is-not-working/m-p/1851047#M222791</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;When executing clEnqueueMapBuffer, I want to set the argument blcoking_map=CL_FALSE to make it work asynchronously, but it only works synchronously.&lt;BR /&gt;When using OpenCL with i.MX8Mplus, does this function behave in accordance with the OpenCL specifications? Or are there any restrictions?&lt;BR /&gt;The SDK version used is 5.4.70 2.3.0.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;/P&gt;</description>
    <pubDate>Mon, 22 Apr 2024 00:23:01 GMT</pubDate>
    <dc:creator>tetsuro-okuyama</dc:creator>
    <dc:date>2024-04-22T00:23:01Z</dc:date>
    <item>
      <title>Asynchronous operation(clEnqueueMapBuffer) is not working properly</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Asynchronous-operation-clEnqueueMapBuffer-is-not-working/m-p/1851047#M222791</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;When executing clEnqueueMapBuffer, I want to set the argument blcoking_map=CL_FALSE to make it work asynchronously, but it only works synchronously.&lt;BR /&gt;When using OpenCL with i.MX8Mplus, does this function behave in accordance with the OpenCL specifications? Or are there any restrictions?&lt;BR /&gt;The SDK version used is 5.4.70 2.3.0.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;/P&gt;</description>
      <pubDate>Mon, 22 Apr 2024 00:23:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Asynchronous-operation-clEnqueueMapBuffer-is-not-working/m-p/1851047#M222791</guid>
      <dc:creator>tetsuro-okuyama</dc:creator>
      <dc:date>2024-04-22T00:23:01Z</dc:date>
    </item>
  </channel>
</rss>