<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Download line in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Download-line/m-p/1847980#M222583</link>
    <description>&lt;P&gt;Where can i find the&amp;nbsp; download line in imx93 evk.then i can use that line and flash the latest os.&lt;/P&gt;&lt;P&gt;I set the boot mode to CORTEX-M(then i am able to detect the usb in usb1 port), because i am unable to detect the usb if it is in CORTEX-A mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am flashing the latest BSP LINUX6.6.0_1.0.0 for imx93 evk.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;While flashing the image using uuu.I am getting this error.&lt;/P&gt;&lt;P&gt;"""LF_v6.6.3-1.0.0_images_IMX93EVK$ sudo uuu uuu.auto-imx93-11x11-lpddr4x-evk&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172&lt;/P&gt;&lt;P&gt;Success 0 Failure 1&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;3:1 1/ 1 [HID(W):LIBUSB_ERROR_NO_DEVICE ] SDPS: boot -f imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot"""&lt;/P&gt;</description>
    <pubDate>Tue, 16 Apr 2024 10:38:59 GMT</pubDate>
    <dc:creator>Mohan51</dc:creator>
    <dc:date>2024-04-16T10:38:59Z</dc:date>
    <item>
      <title>Download line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Download-line/m-p/1847980#M222583</link>
      <description>&lt;P&gt;Where can i find the&amp;nbsp; download line in imx93 evk.then i can use that line and flash the latest os.&lt;/P&gt;&lt;P&gt;I set the boot mode to CORTEX-M(then i am able to detect the usb in usb1 port), because i am unable to detect the usb if it is in CORTEX-A mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am flashing the latest BSP LINUX6.6.0_1.0.0 for imx93 evk.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;While flashing the image using uuu.I am getting this error.&lt;/P&gt;&lt;P&gt;"""LF_v6.6.3-1.0.0_images_IMX93EVK$ sudo uuu uuu.auto-imx93-11x11-lpddr4x-evk&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.21-0-g1f42172&lt;/P&gt;&lt;P&gt;Success 0 Failure 1&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;3:1 1/ 1 [HID(W):LIBUSB_ERROR_NO_DEVICE ] SDPS: boot -f imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot"""&lt;/P&gt;</description>
      <pubDate>Tue, 16 Apr 2024 10:38:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Download-line/m-p/1847980#M222583</guid>
      <dc:creator>Mohan51</dc:creator>
      <dc:date>2024-04-16T10:38:59Z</dc:date>
    </item>
    <item>
      <title>Re: Download line</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Download-line/m-p/1848854#M222646</link>
      <description>&lt;P&gt;Here you met unable to detect the usb if it is in CORTEX-A mode, you can try to setting the SW1301“&lt;STRONG&gt;0100&lt;/STRONG&gt;” from low to high when in the download mode. If it still not work tell me.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Apr 2024 08:27:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Download-line/m-p/1848854#M222646</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2024-04-17T08:27:33Z</dc:date>
    </item>
  </channel>
</rss>