<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX.8MP VPU Software in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX-8MP-VPU-Software/m-p/1847428#M222539</link>
    <description>&lt;P&gt;I'm using an IMX.8MP from MSC with &lt;STRONG&gt;5.15-kirkstone&lt;/STRONG&gt; and a kernel version version &lt;STRONG&gt;5.15.52+g244c28a772f6&lt;/STRONG&gt;, I can see from the &lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX_VPU_APPLICATION_PROGRAMMING_INTERFACE_LINUX_REFERENCE_MANUAL.pdf" target="_self"&gt;IMXVPUAPI Documentation&lt;/A&gt; that the IMX.8M Hantro VPU has user space libraries. I also have read through &lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf" target="_self"&gt;i.MX Linux Reference Manual Section 6.5&lt;/A&gt;. The documentation lists a workflow for decoding a H.264 stream, but I can't find any references to the user space library. I'm not using a NXP BSP since I have a MSC board, with a custom yocto build. Is there a way to add a layer to the image and/or is there more documentation surrounding the user space libraries.&lt;/P&gt;</description>
    <pubDate>Mon, 15 Apr 2024 19:34:30 GMT</pubDate>
    <dc:creator>hsuq7052</dc:creator>
    <dc:date>2024-04-15T19:34:30Z</dc:date>
    <item>
      <title>IMX.8MP VPU Software</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-8MP-VPU-Software/m-p/1847428#M222539</link>
      <description>&lt;P&gt;I'm using an IMX.8MP from MSC with &lt;STRONG&gt;5.15-kirkstone&lt;/STRONG&gt; and a kernel version version &lt;STRONG&gt;5.15.52+g244c28a772f6&lt;/STRONG&gt;, I can see from the &lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX_VPU_APPLICATION_PROGRAMMING_INTERFACE_LINUX_REFERENCE_MANUAL.pdf" target="_self"&gt;IMXVPUAPI Documentation&lt;/A&gt; that the IMX.8M Hantro VPU has user space libraries. I also have read through &lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX_REFERENCE_MANUAL.pdf" target="_self"&gt;i.MX Linux Reference Manual Section 6.5&lt;/A&gt;. The documentation lists a workflow for decoding a H.264 stream, but I can't find any references to the user space library. I'm not using a NXP BSP since I have a MSC board, with a custom yocto build. Is there a way to add a layer to the image and/or is there more documentation surrounding the user space libraries.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Apr 2024 19:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-8MP-VPU-Software/m-p/1847428#M222539</guid>
      <dc:creator>hsuq7052</dc:creator>
      <dc:date>2024-04-15T19:34:30Z</dc:date>
    </item>
    <item>
      <title>Re: IMX.8MP VPU Software</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-8MP-VPU-Software/m-p/1847437#M222540</link>
      <description>&lt;P&gt;There is a git repo with VPU related user space functions&amp;nbsp;&lt;A href="https://github.com/nxp-imx/imx-vpuwrap" target="_self"&gt;https://github.com/nxp-imx/imx-vpuwrap&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;information about it in this nxp form post&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MP-VPU-Tips-for-vpuwraper/ta-p/1697645" target="_self"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MP-VPU-Tips-for-vpuwraper/ta-p/1697645&lt;/A&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 Apr 2024 20:13:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-8MP-VPU-Software/m-p/1847437#M222540</guid>
      <dc:creator>JWL</dc:creator>
      <dc:date>2024-04-15T20:13:57Z</dc:date>
    </item>
    <item>
      <title>Re: IMX.8MP VPU Software</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-8MP-VPU-Software/m-p/1913490#M226427</link>
      <description>&lt;P&gt;Hi there, sorry for piggybacking but I would like to clarify below.&lt;BR /&gt;&lt;BR /&gt;The VPU reference &lt;A href="https://www.nxp.com/docs/en/reference-manual/IMX_VPU_APPLICATION_PROGRAMMING_INTERFACE_LINUX_REFERENCE_MANUAL.pdf" target="_self"&gt;manual&lt;/A&gt;&amp;nbsp;states that " GStreamer delivers the header for VPU wrapper" and this is via the "imx-gst1.0-plugin" package. There was no mention of "imx-vpuwrap&lt;SPAN&gt;" in the manual. But both packages have the&amp;nbsp;header files for the VPU wrapper (ex for Hantro: hantrodec.h and hx280enc.h.) and the library itself (ex for Hantro: libfslvpuwrap.so)&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Do you know (or can someone explain) which of these packages should be used? The artifacts seem to be the same files when you compare them, but I would like to know officially which one should be used.&lt;/P&gt;</description>
      <pubDate>Mon, 22 Jul 2024 00:22:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-8MP-VPU-Software/m-p/1913490#M226427</guid>
      <dc:creator>b_m</dc:creator>
      <dc:date>2024-07-22T00:22:19Z</dc:date>
    </item>
    <item>
      <title>Re: IMX.8MP VPU Software</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX-8MP-VPU-Software/m-p/2060160#M234973</link>
      <description>&lt;P&gt;I've tried using the imx-vpuwrap library, but it was a pain. I instead used &lt;A href="https://github.com/Freescale/libimxvpuapi" target="_self"&gt;ibimxvpuapi&lt;/A&gt;. There is recipe already defined within the &lt;A href="https://github.com/Freescale/meta-freescale/blob/ab64f135e9def28a1198d8107071aac76e6a424f/recipes-multimedia/libimxvpuapi/libimxvpuapi_git.bb#L3" target="_self"&gt;meta-freescale&lt;/A&gt; layer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://layers.openembedded.org/layerindex/recipe/105017/" target="_self"&gt;https://layers.openembedded.org/layerindex/recipe/105017/&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Mar 2025 07:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX-8MP-VPU-Software/m-p/2060160#M234973</guid>
      <dc:creator>hsuq7052</dc:creator>
      <dc:date>2025-03-12T07:01:59Z</dc:date>
    </item>
  </channel>
</rss>