<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: kernel logo</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/kernel-logo/m-p/1847234#M222532</link>
    <description>&lt;P&gt;Hello, thank you for your reply!&lt;/P&gt;&lt;P&gt;I probably guessed that it should be the driver loading order. I tried to load the logo driver on the sii9022 and mxsfb driver, which is implemented in kconfig. But the problem still exists. Do you have any solutions or ideas?&lt;/P&gt;&lt;P&gt;Wishing you all the best!&lt;/P&gt;</description>
    <pubDate>Mon, 15 Apr 2024 15:06:06 GMT</pubDate>
    <dc:creator>rainho</dc:creator>
    <dc:date>2024-04-15T15:06:06Z</dc:date>
    <item>
      <title>kernel logo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kernel-logo/m-p/1846844#M222500</link>
      <description>&lt;P&gt;Hello, now I have a question about kernel logo display!&lt;BR /&gt;I used sii9022 on the imx6u platform to successfully convert RGB signals to HDMI signals, and my application can display normally. But I need to display the Penguin logo during the kernel startup phase. It cannot display the startup logo. However, I changed the screen and no longer use rgb to hdmi. I can directly use the rgb888 interface screen to display the logo normally. How can I change this? The driver I use is mxsfb_sii902x.c. Finally, my kernel version is 4.1.15.&lt;BR /&gt;I would be very grateful if you get a reply!&lt;/P&gt;</description>
      <pubDate>Mon, 15 Apr 2024 07:15:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kernel-logo/m-p/1846844#M222500</guid>
      <dc:creator>rainho</dc:creator>
      <dc:date>2024-04-15T07:15:04Z</dc:date>
    </item>
    <item>
      <title>Re: kernel logo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kernel-logo/m-p/1847215#M222529</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;In This case you have to modify the driver that passed the logo to hdmi since the conversion enter after this logo is printed, please check it.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Mon, 15 Apr 2024 14:53:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kernel-logo/m-p/1847215#M222529</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-04-15T14:53:54Z</dc:date>
    </item>
    <item>
      <title>Re: kernel logo</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/kernel-logo/m-p/1847234#M222532</link>
      <description>&lt;P&gt;Hello, thank you for your reply!&lt;/P&gt;&lt;P&gt;I probably guessed that it should be the driver loading order. I tried to load the logo driver on the sii9022 and mxsfb driver, which is implemented in kconfig. But the problem still exists. Do you have any solutions or ideas?&lt;/P&gt;&lt;P&gt;Wishing you all the best!&lt;/P&gt;</description>
      <pubDate>Mon, 15 Apr 2024 15:06:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/kernel-logo/m-p/1847234#M222532</guid>
      <dc:creator>rainho</dc:creator>
      <dc:date>2024-04-15T15:06:06Z</dc:date>
    </item>
  </channel>
</rss>