<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248576#M22249</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which application you are using to decode this vector?&lt;/P&gt;&lt;P&gt;You can try with Default Gallery and check the logcat information. This will provide you more detail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Feb 2014 11:43:45 GMT</pubDate>
    <dc:creator>saurabh206</dc:creator>
    <dc:date>2014-02-20T11:43:45Z</dc:date>
    <item>
      <title>Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248575#M22248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I want to decode 3840x1080P 30frame/s(3840x1080p30) at i.MX6Q SabreSD Board. (Android Jellybean 4.2.2-1.1.0)&lt;/P&gt;&lt;P&gt;According to Maunal, I.MX6Quad/Dual can decode upto 1920X1080P 60frame/s.&lt;/P&gt;&lt;P&gt;So I think that it is possible, becase both have same bandwidth.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried to decode 3840x1080p30 Video, and It can be decoded but cannot use hadware decode function. so it is very slow (for only using software decoding).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please Let me know if anyone knows about the way.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hyungjun Yoon&lt;/P&gt;&lt;P&gt;SiliconCube.co, Ltd&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.siliconcube.co.kr/"&gt;www.siliconcube.co.kr&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 11:27:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248575#M22248</guid>
      <dc:creator>hyungjunyoon</dc:creator>
      <dc:date>2014-02-20T11:27:40Z</dc:date>
    </item>
    <item>
      <title>Re: Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248576#M22249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which application you are using to decode this vector?&lt;/P&gt;&lt;P&gt;You can try with Default Gallery and check the logcat information. This will provide you more detail.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 11:43:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248576#M22249</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-02-20T11:43:45Z</dc:date>
    </item>
    <item>
      <title>Re: Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248577#M22250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Default Gallery and Cactus Player were not able to decode the video.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I could only decode it at Mxplayer, but using software decoding. (it is very slow....)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 12:22:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248577#M22250</guid>
      <dc:creator>hyungjunyoon</dc:creator>
      <dc:date>2014-02-20T12:22:47Z</dc:date>
    </item>
    <item>
      <title>Re: Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248578#M22251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you provide the logcat detail? Only this will be helpful...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There may be limitation in VPU for dimensions...or may be some error in OMXPlayer framework...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Saurabh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 12:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248578#M22251</guid>
      <dc:creator>saurabh206</dc:creator>
      <dc:date>2014-02-20T12:27:45Z</dc:date>
    </item>
    <item>
      <title>Re: Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248579#M22252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It cannot be done by hardware, only by software but as you already saw, it will be painfully slow.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Feb 2014 23:03:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248579#M22252</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2014-02-20T23:03:58Z</dc:date>
    </item>
    <item>
      <title>Re: Can I decode 3840x1080P30 using Hardwre decoding function(it is called VPU).</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248580#M22253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank for your help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2014 00:05:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-I-decode-3840x1080P30-using-Hardwre-decoding-function-it-is/m-p/248580#M22253</guid>
      <dc:creator>hyungjunyoon</dc:creator>
      <dc:date>2014-02-24T00:05:58Z</dc:date>
    </item>
  </channel>
</rss>