<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248504#M22218</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chongbin Fan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you very much for the response..&amp;nbsp; &lt;/P&gt;&lt;P&gt;Actually my board uses&amp;nbsp;&amp;nbsp; 1GB or RAM, MT41J256M16&amp;nbsp; x 2Chips) at CS0.&amp;nbsp; The properties and data sheet of these chips is exactly similar to the ones used in SABRE-SDP.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For checking and debug pupose, I have configured the DDR INIT for both the 512MB and 1GB config&amp;nbsp; in the flash_header .&amp;nbsp; Pl. find the files attched for your reference.&amp;nbsp;&amp;nbsp;&amp;nbsp; But with both these configurations the result is still the same and the Kenal is not booting. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However , in our analysis it seems&amp;nbsp; to be some config issue in Andoid image files creation and settings in init.freescale.rc file.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; As the below behaviour is being observed: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; on the same board, able to download and write all the Android image files into the eMMC&amp;nbsp; through MFG tool.&lt;/P&gt;&lt;P&gt;2. Able to burn the eFUSES for the booting of i.MX6S&amp;nbsp; through eMMC&lt;/P&gt;&lt;P&gt;3. The mfg-bootloader and mfg-Kernel executes fully and completes entire process.&lt;/P&gt;&lt;P&gt;4.&amp;nbsp; If&amp;nbsp; only uboot-bin is created directly through "&amp;nbsp; Build U-Boot Images" process, and the same is put into the "Android" folder&amp;nbsp; of MFG-Tool , then even the Board boots through eMMC&amp;nbsp; but hangs at Kernal loading place.&lt;/P&gt;&lt;P&gt;5. However, if all the images ( Uboot.img, Boot.img, system.img, recovery.img)&amp;nbsp; are taken from the /OUT directory after Android build and flashed through MFG tool then the board does not boot at all. ..!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the above symptom indicates some issue with&amp;nbsp;&amp;nbsp; "init.freescale.rc"&amp;nbsp;&amp;nbsp;&amp;nbsp; or Boot.img&amp;nbsp;&amp;nbsp; which does not see any linkage / pointing betwwen the bootloader and rootfile system to initiate the boot process and kernel loading...&amp;nbsp;&amp;nbsp;&amp;nbsp; need the info and direction in this regard for the correct configuration of "init.rc" / "init.freescale.rc"&amp;nbsp;&amp;nbsp; for the generation of&amp;nbsp; properly configured and rightly pointing "Boot.img"....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any direction / debug / input in this regard will be heartly appreciated...&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;thanks and regards in advance..&lt;/P&gt;&lt;P&gt;Ujala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 01 Apr 2013 07:04:55 GMT</pubDate>
    <dc:creator>ujala</dc:creator>
    <dc:date>2013-04-01T07:04:55Z</dc:date>
    <item>
      <title>on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248502#M22216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am porting Android 13.4.1 BSP on custon Board based on DL- SABRE-SD plaform.&amp;nbsp;&amp;nbsp; I have applied 13.4.1.02 Android patch on the Android BSP downloaded from freescale site.&amp;nbsp;&amp;nbsp; Have built the U-boot, And android images and have put through the MFG tool in eMMC .. however, on booting, the board boots&amp;nbsp;&amp;nbsp; and hangs while loading Kernel...&amp;nbsp; below is LOG..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2009.08-dirty (Mar 31 2013 - 12:32:46)&lt;/P&gt;&lt;P&gt;CPU: Freescale i.MX6 family TO1.1 at 792 MHz&lt;BR /&gt;Temperature:&amp;nbsp;&amp;nbsp; 46 C, calibration data 0x5bb5465f&lt;BR /&gt;mx6q pll1: 792MHz&lt;BR /&gt;mx6q pll2: 528MHz&lt;BR /&gt;mx6q pll3: 480MHz&lt;BR /&gt;mx6q pll8: 50MHz&lt;BR /&gt;ipg clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 66000000Hz&lt;BR /&gt;ipg per clock : 66000000Hz&lt;BR /&gt;uart clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 80000000Hz&lt;BR /&gt;cspi clock&amp;nbsp;&amp;nbsp;&amp;nbsp; : 60000000Hz&lt;BR /&gt;ahb clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 132000000Hz&lt;BR /&gt;axi clock&amp;nbsp;&amp;nbsp; : 198000000Hz&lt;BR /&gt;emi_slow clock: 22000000Hz&lt;BR /&gt;ddr clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 396000000Hz&lt;BR /&gt;usdhc1 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;usdhc2 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;usdhc3 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;usdhc4 clock&amp;nbsp; : 198000000Hz&lt;BR /&gt;nfc clock&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; : 24000000Hz&lt;BR /&gt;Board: i.MX6DL/Solo-SABRESD: unknown-board Board: 0x61011 [POR ]&lt;BR /&gt;Boot Device: MMC&lt;BR /&gt;I2C:&amp;nbsp;&amp;nbsp; ready&lt;BR /&gt;DRAM:&amp;nbsp; 512 MB&lt;BR /&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_USDHC: 0,FSL_USDHC: 1,FSL_USDHC: 2,FSL_USDHC: 3&lt;BR /&gt;*** Warning - bad CRC or MMC, using default environment&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Out:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Err:&amp;nbsp;&amp;nbsp; serial&lt;BR /&gt;Found PFUZE100! deviceid=10,revid=11&lt;BR /&gt;Net:&amp;nbsp;&amp;nbsp; got MAC address from IIM: 00:00:00:00:00:00&lt;BR /&gt;FEC0 [PRIME]&lt;BR /&gt;Hit any key to stop autoboot:&amp;nbsp; 3&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 &lt;BR /&gt;kernel&amp;nbsp;&amp;nbsp; @ 10808000 (4091876)&lt;BR /&gt;ramdisk&amp;nbsp; @ 11800000 (167741)&lt;BR /&gt;kernel cmdline: &lt;BR /&gt; use uboot command line:&lt;BR /&gt; console=ttymxc0,115200 init=/init nosmp video=mxcfb0 video=mxcfb1:off video=mxcfb2:off gpumem=96M fbmem=10M fb0base=0x17b00000 vmalloc=400M androidboot.console=ttymxc0 &lt;/P&gt;&lt;P&gt;Starting kernel ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;unable to proceed further.. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;request help / guidance urgently&amp;nbsp; ..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 31 Mar 2013 08:45:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248502#M22216</guid>
      <dc:creator>ujala</dc:creator>
      <dc:date>2013-03-31T08:45:09Z</dc:date>
    </item>
    <item>
      <title>Re: on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248503#M22217</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Very like that the DDR is not very stable. I guess you just reused the DDR init script(flash_header.S) of smart_device board, while some parameters are board dependent. Please run DDR calibration to get the proper delay values and then update the flash_header.S, and pls also run DDR stress test using the tool attached. It is expected that the highest frequency which can pass the test should be with 15% margin, ie, if your target frequency is 400MHz, then the highest pass frequency should above 460Mhz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Apr 2013 02:07:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248503#M22217</guid>
      <dc:creator>JerryFan</dc:creator>
      <dc:date>2013-04-01T02:07:39Z</dc:date>
    </item>
    <item>
      <title>Re: on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248504#M22218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chongbin Fan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you very much for the response..&amp;nbsp; &lt;/P&gt;&lt;P&gt;Actually my board uses&amp;nbsp;&amp;nbsp; 1GB or RAM, MT41J256M16&amp;nbsp; x 2Chips) at CS0.&amp;nbsp; The properties and data sheet of these chips is exactly similar to the ones used in SABRE-SDP.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For checking and debug pupose, I have configured the DDR INIT for both the 512MB and 1GB config&amp;nbsp; in the flash_header .&amp;nbsp; Pl. find the files attched for your reference.&amp;nbsp;&amp;nbsp;&amp;nbsp; But with both these configurations the result is still the same and the Kenal is not booting. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However , in our analysis it seems&amp;nbsp; to be some config issue in Andoid image files creation and settings in init.freescale.rc file.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; As the below behaviour is being observed: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; on the same board, able to download and write all the Android image files into the eMMC&amp;nbsp; through MFG tool.&lt;/P&gt;&lt;P&gt;2. Able to burn the eFUSES for the booting of i.MX6S&amp;nbsp; through eMMC&lt;/P&gt;&lt;P&gt;3. The mfg-bootloader and mfg-Kernel executes fully and completes entire process.&lt;/P&gt;&lt;P&gt;4.&amp;nbsp; If&amp;nbsp; only uboot-bin is created directly through "&amp;nbsp; Build U-Boot Images" process, and the same is put into the "Android" folder&amp;nbsp; of MFG-Tool , then even the Board boots through eMMC&amp;nbsp; but hangs at Kernal loading place.&lt;/P&gt;&lt;P&gt;5. However, if all the images ( Uboot.img, Boot.img, system.img, recovery.img)&amp;nbsp; are taken from the /OUT directory after Android build and flashed through MFG tool then the board does not boot at all. ..!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the above symptom indicates some issue with&amp;nbsp;&amp;nbsp; "init.freescale.rc"&amp;nbsp;&amp;nbsp;&amp;nbsp; or Boot.img&amp;nbsp;&amp;nbsp; which does not see any linkage / pointing betwwen the bootloader and rootfile system to initiate the boot process and kernel loading...&amp;nbsp;&amp;nbsp;&amp;nbsp; need the info and direction in this regard for the correct configuration of "init.rc" / "init.freescale.rc"&amp;nbsp;&amp;nbsp; for the generation of&amp;nbsp; properly configured and rightly pointing "Boot.img"....&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;any direction / debug / input in this regard will be heartly appreciated...&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;thanks and regards in advance..&lt;/P&gt;&lt;P&gt;Ujala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Apr 2013 07:04:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248504#M22218</guid>
      <dc:creator>ujala</dc:creator>
      <dc:date>2013-04-01T07:04:55Z</dc:date>
    </item>
    <item>
      <title>Re: on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248505#M22219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What command you used to build the u-boot and kernel?&lt;/P&gt;&lt;P&gt;Are you building the u-boot for i.MX6S?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2013 03:14:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248505#M22219</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2013-04-17T03:14:28Z</dc:date>
    </item>
    <item>
      <title>Re: on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248506#M22220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If your log is stuck on "Starting kernel", it should not be related to "&lt;SPAN style="font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; background-color: #ffffff;"&gt;&amp;nbsp; "init.freescale.rc". Please check your kernel - As you mentioned, you are running SW on customer's board. So you should ensure you have changed relative board files and ensure they are aligned with your board design. You can add logs in your board init function and see whether the SW ran it to here firstly.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Apr 2013 04:30:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248506#M22220</guid>
      <dc:creator>lily_zhang</dc:creator>
      <dc:date>2013-04-17T04:30:01Z</dc:date>
    </item>
    <item>
      <title>Re: on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248507#M22221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xioali,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks for the reply,&lt;/P&gt;&lt;P&gt;i have solved the problem myself..&amp;nbsp; it was related to MFG version of UBOOT.&amp;nbsp; i was downloading my uboot.bin and Uimage using the MFGTool with the "u-boot-mx6dl.bin"&amp;nbsp; supplied&amp;nbsp; with the MFG Tool itself.&amp;nbsp; Once i generated my own MFG "u-boot-mx6dl.bin"&amp;nbsp; for my custom board and replaced that in the MFG Tool, then the board started working properly.&amp;nbsp; Now everything is booting properly and i am able to Load the kernel and Android.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However , now i am facing a peculiar&amp;nbsp; problem of&amp;nbsp;&amp;nbsp; "FSL Powerservices stopped:..&amp;nbsp;&amp;nbsp;&amp;nbsp; pl. see the attached image in this regard.&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i am using i.MX6S&amp;nbsp; cpu&amp;nbsp;&amp;nbsp; and Android 13.4.1 BSP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 May 2013 04:40:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248507#M22221</guid>
      <dc:creator>ujala</dc:creator>
      <dc:date>2013-05-08T04:40:52Z</dc:date>
    </item>
    <item>
      <title>Re: on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248508#M22222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I didn't see attached image. From your description, i suggest you to remove "System Profile Service and App".&lt;/P&gt;&lt;P&gt;See Android_Advanced_User_Guide.pdf and get known of "System Profile Service and App".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 May 2013 05:08:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248508#M22222</guid>
      <dc:creator>lily_zhang</dc:creator>
      <dc:date>2013-05-20T05:08:46Z</dc:date>
    </item>
    <item>
      <title>Re: on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248509#M22223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chongbin, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have elf files for the stress test?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jul 2013 16:50:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248509#M22223</guid>
      <dc:creator>Chris1z</dc:creator>
      <dc:date>2013-07-26T16:50:44Z</dc:date>
    </item>
    <item>
      <title>Re: on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248510#M22224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Even we have developed a customized board on the basic of Sabre-SD board design (iMX6 Quad core), i am trying to replace only the images i build from &lt;STRONG&gt;OUT/&lt;/STRONG&gt; folder into the folder by name &lt;STRONG&gt;android/ in MFG tool&lt;/STRONG&gt;, is this enough to boot the board or do i have to build/generate my &lt;STRONG&gt;OWN&lt;/STRONG&gt; u-boot-mx6q-sabresd.bin for &lt;STRONG&gt;MFG tool &lt;/STRONG&gt;again and then replace it inside &lt;STRONG&gt;OS Firmware &lt;/STRONG&gt;folder present inside MFG tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also we are using 2GB DDR3 in place of 1GB DDR3 by default present on Sabre-SD board.&lt;/P&gt;&lt;P&gt;Kindly request you to provide some pointers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Soujanya.K&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Dec 2013 07:40:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248510#M22224</guid>
      <dc:creator>soujanyak</dc:creator>
      <dc:date>2013-12-13T07:40:49Z</dc:date>
    </item>
    <item>
      <title>Re: on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248511#M22225</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We have to set the highest frequency more than 560MHz with 15% margin.But is giving limit for 520MHz.&lt;/P&gt;&lt;P&gt;Please help me to set the frequncy more than 560MHz with 15% margin.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Dec 2013 12:51:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248511#M22225</guid>
      <dc:creator>lakshmishetty</dc:creator>
      <dc:date>2013-12-26T12:51:41Z</dc:date>
    </item>
    <item>
      <title>Re: on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248512#M22226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chongbin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 15% margin on the max speed at room temperature make sure that the test will pass at the maximum speed across the full temperature range?&lt;/P&gt;&lt;P&gt;Or is it just a safety margin with respect to a real application (with all IPU/GPU/VPU running) since the tool issues pattern that can not 100% stimulate a worst case scenario?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Aug 2014 06:39:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248512#M22226</guid>
      <dc:creator>Rodrigue</dc:creator>
      <dc:date>2014-08-11T06:39:12Z</dc:date>
    </item>
    <item>
      <title>Re: on i.MX6S custom board, 32-bit mode, Booting hangs at Kernel loading..</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248513#M22227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. The 15% margin is based on our experience from tons of customer support.&lt;/P&gt;&lt;P&gt;2. Usually we tested is at rom temparature, rarely at very low/high. So I am not sure 15% is still workable at low/high.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Aug 2014 06:58:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/on-i-MX6S-custom-board-32-bit-mode-Booting-hangs-at-Kernel/m-p/248513#M22227</guid>
      <dc:creator>JerryFan</dc:creator>
      <dc:date>2014-08-11T06:58:24Z</dc:date>
    </item>
  </channel>
</rss>