<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx93evk cannot boot from sd-card in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1840847#M222131</link>
    <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I have an "MCIMX93-EVK" on my desk with the same "symthoms" as you are describing ... boot(s) OK from eMMC (prebuilt image delivered with board), and also from Yocto-based uSD/MMC Card (.wic image) but *not* from my own Buildroot-based "2024.02.1" (freescale_imx93evk_defconfig) build. No indications on console - i.e. board seem dead. I assume it is related to A0-processor, and am awaiting av A1-based evaluation board.&lt;/P&gt;&lt;P&gt;Anyway; just wanted to check with you whether you put any effort into getting the A0-board up-and-running, and possibly which tweaks you did to the Buildroot-based solution?&lt;/P&gt;&lt;P&gt;Appreciate it.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;/Eldor&lt;/P&gt;</description>
    <pubDate>Thu, 04 Apr 2024 14:42:18 GMT</pubDate>
    <dc:creator>eldorr</dc:creator>
    <dc:date>2024-04-04T14:42:18Z</dc:date>
    <item>
      <title>imx93evk cannot boot from sd-card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1779127#M217758</link>
      <description>&lt;P&gt;Working with an imx93evk (marked MCIMX93-EVKCM - date 2317) I've not been able to successfully boot from an SD-card.&lt;/P&gt;&lt;P&gt;The board comes with an image pre-loaded into the eMMC and it boots fine. I see text output on the debug UART (number 3 out of 4 COM ports created when connected to the DBG USB-C).&lt;/P&gt;&lt;P&gt;Trying to boot from SD-card I see no debug UART output at all. I've tried booting the following images from both a 4G and 64G SD-card:&lt;BR /&gt;- Pre-built image downloaded: imx-image-multimedia-imx93evk.wic&lt;BR /&gt;- Image built from Yocto SDK: imx-image-multimedia-imx93evk.wic&lt;BR /&gt;- Image built by Buildroot (which we normally use) - preliminary patches from &lt;A href="https://patchwork.ozlabs.org/project/buildroot/list/?series=377108&amp;amp;state=*" target="_blank"&gt;https://patchwork.ozlabs.org/project/buildroot/list/?series=377108&amp;amp;state=*&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I've set SW1301 according to the Quick Start Guide:&lt;BR /&gt;SW1301-1: 0&lt;BR /&gt;SW1301-2: 0&lt;BR /&gt;SW1301-3: 1&lt;BR /&gt;SW1301-4: 0&lt;/P&gt;&lt;P&gt;Based on &lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-mx93-evk-boot-from-sd-card/m-p/1707596#M211066" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/i-mx93-evk-boot-from-sd-card/m-p/1707596#M211066&lt;/A&gt; I've also tried:&lt;BR /&gt;SW1301-1: 0&lt;BR /&gt;SW1301-2: 1&lt;BR /&gt;SW1301-3: 0&lt;BR /&gt;SW1301-4: 0&lt;/P&gt;&lt;P&gt;I've tried flashing the SD-card both using BalenaEtcher (Windows) and according to &lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/user-guide/IMX_YOCTO_PROJECT_USERS_GUIDE.pdf&lt;/A&gt; with "zstdcat &amp;lt;image_name&amp;gt;.wic.zst | sudo dd of=/dev/sd&amp;lt;partition&amp;gt; bs=1M conv=fsync"&lt;/P&gt;&lt;P&gt;I've not tried to re-flash the eMMC since I don't want to do that before I have something else to bring the board to life.&lt;/P&gt;&lt;P&gt;I already have an additional imx93evk ordered, so when this arrives I can test with another board.&lt;/P&gt;&lt;P&gt;Any idea what the problem could be?&lt;/P&gt;&lt;P&gt;Can you point to a pre-built SD-card image that is certain to work with the imx93evk?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 22 Dec 2023 08:29:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1779127#M217758</guid>
      <dc:creator>djernaes</dc:creator>
      <dc:date>2023-12-22T08:29:54Z</dc:date>
    </item>
    <item>
      <title>Re: imx93evk cannot boot from sd-card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1779981#M217861</link>
      <description>&lt;P&gt;I download and flash the one (&lt;A href="https://www.nxp.com/webapp/Download?colCode=L6.1.36_2.1.0_MX93&amp;amp;appType=license)" target="_blank" rel="noopener"&gt;https://www.nxp.com/webapp/Download?colCode=L6.1.36_2.1.0_MX93&amp;amp;appType=license)&lt;/A&gt;&amp;nbsp;on i.MX93 EVK A1 and then boot it successfully with BMODE as&amp;nbsp;&lt;SPAN&gt;SW1301-1: 0,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;SW1301-2: 1,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;SW1301-3: 0,&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;SW1301-4: 0&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;uuu.exe -b sd_all .\imx-image-multimedia-imx93evk.wic&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 26 Dec 2023 09:05:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1779981#M217861</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2023-12-26T09:05:48Z</dc:date>
    </item>
    <item>
      <title>Re: imx93evk cannot boot from sd-card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1781602#M218082</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;U&gt;Trying to use the UUU utility I get the following error.&lt;/U&gt;&lt;BR /&gt;uuu.exe -b sd_all .\imx-image-multimedia-imx93evk.wic&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.125-0-gaeb3490&lt;BR /&gt;Success 0 Failure 1&lt;BR /&gt;1:3 1/ 1 [HID(W):LIBUSB_ERROR_PIPE ] SDPS: boot -scanterm -f .\imx-image-multimedia-imx93evk.wic -scan&lt;/P&gt;&lt;P&gt;Note that the BMODE setting indicated in your response and the BMODE setting for UUU to detect the EVK board is wrong in the paper Quick Start Guide delivered with my EVK. It has been corrected in the current online version (dip switch order reversed).&lt;BR /&gt;&lt;BR /&gt;While googling on this the above issue I noticed the "Migration Guide from imx93 A0 to A1". This indicates that later images might not work with A0.&lt;BR /&gt;The marking on my EVK imx93 MCU is "PIMX9352CVUXMAA" - is it an A0 then?&lt;BR /&gt;&lt;BR /&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 02 Jan 2024 09:16:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1781602#M218082</guid>
      <dc:creator>djernaes</dc:creator>
      <dc:date>2024-01-02T09:16:42Z</dc:date>
    </item>
    <item>
      <title>Re: imx93evk cannot boot from sd-card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1782582#M218178</link>
      <description>&lt;P&gt;Yes, this (&lt;SPAN&gt;PIMX9352CVUXMAA) is A0.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 04 Jan 2024 02:06:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1782582#M218178</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-01-04T02:06:34Z</dc:date>
    </item>
    <item>
      <title>Re: imx93evk cannot boot from sd-card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1782880#M218206</link>
      <description>Could this result in the pre-built images not booting?&lt;BR /&gt;Could this result in the uuu utility not working?</description>
      <pubDate>Thu, 04 Jan 2024 09:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1782880#M218206</guid>
      <dc:creator>djernaes</dc:creator>
      <dc:date>2024-01-04T09:09:09Z</dc:date>
    </item>
    <item>
      <title>Re: imx93evk cannot boot from sd-card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1783250#M218241</link>
      <description>&lt;P&gt;Yes, could result in not working for both cases.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 05 Jan 2024 00:11:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1783250#M218241</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-01-05T00:11:21Z</dc:date>
    </item>
    <item>
      <title>Re: imx93evk cannot boot from sd-card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1799486#M219491</link>
      <description>Yes looks like the bootloader on A0 doesn't support flashing the newer linux packages. With imx93 A0, you can successfully flash images of Linux 6.1.22_2.0.0​ [&lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt;]</description>
      <pubDate>Thu, 01 Feb 2024 05:05:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1799486#M219491</guid>
      <dc:creator>gaurav_sharma</dc:creator>
      <dc:date>2024-02-01T05:05:23Z</dc:date>
    </item>
    <item>
      <title>Re: imx93evk cannot boot from sd-card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1799705#M219511</link>
      <description>&lt;P&gt;I've received a new eval board with with an A1 and have everything running.&lt;/P&gt;&lt;P&gt;Thanks&lt;BR /&gt;Kim&lt;/P&gt;</description>
      <pubDate>Thu, 01 Feb 2024 08:59:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1799705#M219511</guid>
      <dc:creator>djernaes</dc:creator>
      <dc:date>2024-02-01T08:59:07Z</dc:date>
    </item>
    <item>
      <title>Re: imx93evk cannot boot from sd-card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1840847#M222131</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I have an "MCIMX93-EVK" on my desk with the same "symthoms" as you are describing ... boot(s) OK from eMMC (prebuilt image delivered with board), and also from Yocto-based uSD/MMC Card (.wic image) but *not* from my own Buildroot-based "2024.02.1" (freescale_imx93evk_defconfig) build. No indications on console - i.e. board seem dead. I assume it is related to A0-processor, and am awaiting av A1-based evaluation board.&lt;/P&gt;&lt;P&gt;Anyway; just wanted to check with you whether you put any effort into getting the A0-board up-and-running, and possibly which tweaks you did to the Buildroot-based solution?&lt;/P&gt;&lt;P&gt;Appreciate it.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;/Eldor&lt;/P&gt;</description>
      <pubDate>Thu, 04 Apr 2024 14:42:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1840847#M222131</guid>
      <dc:creator>eldorr</dc:creator>
      <dc:date>2024-04-04T14:42:18Z</dc:date>
    </item>
    <item>
      <title>Re: imx93evk cannot boot from sd-card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1841103#M222154</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I haven't done any further attempts with the A0 revision, but I have noted that Buildroot has the following target configuration options:&lt;BR /&gt;BR2_PACKAGE_FIRMWARE_SENTINEL_A0&lt;BR /&gt;BR2_PACKAGE_FIRMWARE_SENTINEL_A1&lt;/P&gt;&lt;P&gt;which selects different images in the firmware-sentnel package through BR2_PACKAGE_FIRMWARE_SENTINEL_AHAB_CONTAINER_IMAGE&lt;/P&gt;&lt;P&gt;Regards&lt;BR /&gt;Kim&lt;/P&gt;</description>
      <pubDate>Fri, 05 Apr 2024 06:55:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1841103#M222154</guid>
      <dc:creator>djernaes</dc:creator>
      <dc:date>2024-04-05T06:55:44Z</dc:date>
    </item>
    <item>
      <title>Re: imx93evk cannot boot from sd-card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1841150#M222157</link>
      <description>&lt;P&gt;Excellent - thanks!&lt;/P&gt;&lt;P&gt;I have at least some movement on the terminal now; but stops at&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;U-Boot SPL 2022.04-g92d918d0 (Apr 02 2024 - 15:49:58 +0200)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;SOC: 0xa0009300&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LC: 0x40010&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;M33 prepare ok&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Normal Boot&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Trying to boot from BOOTROM&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Boot Stage: Primary boot&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Load image from 0x4cc00 by ROM_API&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&amp;nbsp;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;U-Boot SPL 2022.04-g92d918d0 (Apr 02 2024 - 15:49:58 +0200)&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;SOC: 0xa0009300&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;LC: 0x40010&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;M33 prepare ok&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Normal Boot&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Trying to boot from BOOTROM&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Boot Stage: Primary boot&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;Load image from 0x4cc00 by ROM_API&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 05 Apr 2024 08:16:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1841150#M222157</guid>
      <dc:creator>eldorr</dc:creator>
      <dc:date>2024-04-05T08:16:50Z</dc:date>
    </item>
    <item>
      <title>Re: imx93evk cannot boot from sd-card</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1841562#M222189</link>
      <description>&lt;P&gt;FYI; remaining part of this issue was related to wrong format/build of bl31.bin (wrong make-options used). Correct was "make PLAT=imx93 bl31". Issue resolved.&lt;/P&gt;</description>
      <pubDate>Sat, 06 Apr 2024 08:12:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1841562#M222189</guid>
      <dc:creator>eldorr</dc:creator>
      <dc:date>2024-04-06T08:12:52Z</dc:date>
    </item>
  </channel>
</rss>