<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: iMX8 CAAM - How to create a dm-crypt block device in /dev/mapper without wiping it?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-CAAM-How-to-create-a-dm-crypt-block-device-in-dev-mapper/m-p/1840825#M222129</link>
    <description>&lt;P&gt;What I hadn't realised was that you MUST import the key from the black-blob (.bb) file after every reboot as the keys are session specific.&amp;nbsp; The initial "dmsetup -v create" command should be used on all subsequent reboots, with a newly imported key.&lt;/P&gt;</description>
    <pubDate>Thu, 04 Apr 2024 14:21:13 GMT</pubDate>
    <dc:creator>cmsd</dc:creator>
    <dc:date>2024-04-04T14:21:13Z</dc:date>
    <item>
      <title>iMX8 CAAM - How to create a dm-crypt block device in /dev/mapper without wiping it?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-CAAM-How-to-create-a-dm-crypt-block-device-in-dev-mapper/m-p/1840595#M222119</link>
      <description>&lt;P&gt;I can create a dm-crypt filesystem with:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@smarcimx8mq4g:~# cat /data/caam/randomkey | keyctl padd logon logkey: @s
731358804

root@smarcimx8mq4g:~# dmsetup -v create encrypted --table "0 $(blockdev --getsz /dev/mmcblk1p3) crypt capi:tk(cbc(aes))-plain :36:logon:logkey: 0 /dev/mmcblk1p3 0 1 sector_size:512"&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(I'm using the imx8's CAAM's implementation of `tk(cbc(aes))`.)&lt;/P&gt;&lt;P&gt;This is fine for the initial creation of the encrypted volume.&amp;nbsp; I then run "mkfs.ext4 /dev/mapper/encrypted" and "mount /dev/mapper/encrypted /mnt".&lt;/P&gt;&lt;P&gt;On subsequent reboots, this wipes the data in /dev/mmcblk1p3. I can mount /dev/mapper/encrypted, but only once I've run mkfs.ext4 on it again.&amp;nbsp; Otherwise I get superblock errors:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@smarcimx8mq4g:/data/caam# cat randomkey | keyctl padd logon logkey: @s
165039862

root@smarcimx8mq4g:/data/caam# dmsetup -v create encrypted --table "0 $(blockdev --getsz /dev/mmcblk1p3) crypt capi:tk(cbc(aes))-plain :36:logon:logkey: 0 /dev/mmcblk1p3 0 1 sector_size:512"
Name:              encrypted
State:             ACTIVE
Read Ahead:        256
Tables present:    LIVE
Open count:        0
Event number:      0
Major, minor:      252, 0
Number of targets: 1

root@smarcimx8mq4g:/data/caam# mkfs.ext4 /dev/mapper/encrypted 
mke2fs 1.46.2 (28-Feb-2021)
Creating filesystem with 6741631 4k blocks and 1687552 inodes
Filesystem UUID: 943f96ad-a875-425c-8d0e-808b929bdd1b
Superblock backups stored on blocks: 
	32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632, 2654208, 
	4096000

Allocating group tables: done                            
Writing inode tables: done                            
Creating journal (32768 blocks): done
Writing superblocks and filesystem accounting information: done   

root@smarcimx8mq4g:/data/caam# mount /dev/mapper/encrypted /mnt

root@smarcimx8mq4g:/data/caam# date &amp;gt; /mnt/date.txt

root@smarcimx8mq4g:/data/caam# reboot

The system is going down for reboot NOW!

root@smarcimx8mq4g:/data/caam# cat randomkey | keyctl padd logon logkey: @s
165039862

root@smarcimx8mq4g:/data/caam# dmsetup -v create encrypted --table "0 $(blockdev --getsz /dev/mmcblk1p3) crypt capi:tk(cbc(aes))-plain :36:logon:logkey: 0 /dev/mmcblk1p3 0 1 sector_size:512"
Name:              encrypted
State:             ACTIVE
Read Ahead:        256
Tables present:    LIVE
Open count:        0
Event number:      0
Major, minor:      252, 0
Number of targets: 1

root@smarcimx8mq4g:/data/caam# mount /dev/mapper/encrypted /mnt
mount: /mnt: wrong fs type, bad option, bad superblock on /dev/mapper/encrypted, missing codepage or helper program, or other error.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've also tried:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@smarcimx8mq4g:~# dmsetup -v load encrypted --table "0 $(blockdev --getsz /dev/mmcblk1p3) crypt capi:tk(cbc(aes))-plain :36:logon:logkey: 0 /dev/mmcblk1p3 0 1 sector_size:512"
device-mapper: reload ioctl on encrypted failed: No such device or address
Command failed.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;(I expect that nothing other than "create" will create the /dev/mapper/encrypted node.)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;How do I use dm-crypt to get access to the encrypted data, using the same key, after a reboot (which loses /dev/mapper/encrypted)?&lt;/P&gt;</description>
      <pubDate>Thu, 04 Apr 2024 10:15:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-CAAM-How-to-create-a-dm-crypt-block-device-in-dev-mapper/m-p/1840595#M222119</guid>
      <dc:creator>cmsd</dc:creator>
      <dc:date>2024-04-04T10:15:51Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 CAAM - How to create a dm-crypt block device in /dev/mapper without wiping it?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-CAAM-How-to-create-a-dm-crypt-block-device-in-dev-mapper/m-p/1840825#M222129</link>
      <description>&lt;P&gt;What I hadn't realised was that you MUST import the key from the black-blob (.bb) file after every reboot as the keys are session specific.&amp;nbsp; The initial "dmsetup -v create" command should be used on all subsequent reboots, with a newly imported key.&lt;/P&gt;</description>
      <pubDate>Thu, 04 Apr 2024 14:21:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-CAAM-How-to-create-a-dm-crypt-block-device-in-dev-mapper/m-p/1840825#M222129</guid>
      <dc:creator>cmsd</dc:creator>
      <dc:date>2024-04-04T14:21:13Z</dc:date>
    </item>
  </channel>
</rss>