<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How can we interface a Smart Card with iMX6 DualLite processor? in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-can-we-interface-a-Smart-Card-with-iMX6-DualLite-processor/m-p/248454#M22210</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Vinit,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It depends which smart card phy chip you are using, but at least to select the operaing voltage of 1.8,3.3, or 5 Volts, you need to add two more IO pins. If you write your phy chip, I will try to help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mehmet Ali Ipin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Mar 2014 06:50:51 GMT</pubDate>
    <dc:creator>MehmetAliIpin</dc:creator>
    <dc:date>2014-03-20T06:50:51Z</dc:date>
    <item>
      <title>How can we interface a Smart Card with iMX6 DualLite processor?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-we-interface-a-Smart-Card-with-iMX6-DualLite-processor/m-p/248453#M22209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My Smart&amp;nbsp; Card on one side interfaces the card and on the other side it interfaces the processor. Clock, I/O and reset signal are supposed to come from the processor. Now to which exact pin it has to be connected with processor? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jan 2014 06:30:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-we-interface-a-Smart-Card-with-iMX6-DualLite-processor/m-p/248453#M22209</guid>
      <dc:creator>admin</dc:creator>
      <dc:date>2014-01-22T06:30:17Z</dc:date>
    </item>
    <item>
      <title>Re: How can we interface a Smart Card with iMX6 DualLite processor?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-can-we-interface-a-Smart-Card-with-iMX6-DualLite-processor/m-p/248454#M22210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Vinit,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It depends which smart card phy chip you are using, but at least to select the operaing voltage of 1.8,3.3, or 5 Volts, you need to add two more IO pins. If you write your phy chip, I will try to help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mehmet Ali Ipin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Mar 2014 06:50:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-can-we-interface-a-Smart-Card-with-iMX6-DualLite-processor/m-p/248454#M22210</guid>
      <dc:creator>MehmetAliIpin</dc:creator>
      <dc:date>2014-03-20T06:50:51Z</dc:date>
    </item>
  </channel>
</rss>