<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX93 Multicore flexio</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Multicore-flexio/m-p/1839813#M222076</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;Hi &lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442" target="_self"&gt;&lt;SPAN class=""&gt;josephlinares&lt;/SPAN&gt;&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Thanks for your comments,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;1. Here do you mean to say that I should take care about the flexio-gpio pin which must not be used in cortex-A55 Linux dts file right?&lt;/P&gt;&lt;P&gt;2. And if not present in dts file than it is safe to access flexio-gpio pin from cortex-M33 core, is it true?&lt;/P&gt;</description>
    <pubDate>Wed, 03 Apr 2024 04:11:59 GMT</pubDate>
    <dc:creator>NZP</dc:creator>
    <dc:date>2024-04-03T04:11:59Z</dc:date>
    <item>
      <title>i.MX93 Multicore flexio</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Multicore-flexio/m-p/1839415#M222057</link>
      <description>&lt;P&gt;Hello experts,&lt;/P&gt;&lt;P&gt;I am working on i.mx93 in which cortex-a55 is running Linux, here at cortex-m33 side I want to use flexio moules as&amp;nbsp;felxio-pin (as gpio to toggle one pin), so for that I am using&amp;nbsp;&lt;STRONG&gt;flexio_pin_led_output &lt;/STRONG&gt;example code from this SDK_2_14_2_MIMX9352xxxxM. But after reading&amp;nbsp;readme.txt file I found below things.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Note
Please run the application in Low Power boot mode (without Linux BSP).
The IP module resource of the application is also used by Linux BSP.
Or, run with Single Boot mode by changing Linux BSP to avoid resource
conflict.&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. In Linux dts file I have not enabled any flexio related node, so my query is that is it safe to access flexio at cortex-m33 side?&lt;/P&gt;&lt;P&gt;2. Here I am worrying because readme.txt file denotes that&amp;nbsp;&lt;STRONG&gt;The IP module resource of the application is also used by Linux BSP.&amp;nbsp;&lt;/STRONG&gt;but I am not able to find where it is.&lt;/P&gt;&lt;P&gt;3. In nutshell my task is to safely access flexio from cortex-m33 side.&lt;/P&gt;&lt;P&gt;PS: I am referring&amp;nbsp;imx93-11x11-evk.dts file that I have attached below.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 13:41:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Multicore-flexio/m-p/1839415#M222057</guid>
      <dc:creator>NZP</dc:creator>
      <dc:date>2024-04-02T13:41:55Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 Multicore flexio</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Multicore-flexio/m-p/1839630#M222065</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;Confirmed, could not find any usage of &lt;STRONG&gt;&lt;EM&gt;MX93_PAD_GPIO_IO04__X&lt;/EM&gt;&lt;/STRONG&gt; in &lt;STRONG&gt;&lt;EM&gt;imx93-11x11-evk.dts&lt;/EM&gt;&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;But it's found under lpuart and aud-hat demos, consider looking at any DTS before using the &lt;STRONG&gt;&lt;EM&gt;flexio_pin_led_output.c &lt;/EM&gt;&lt;/STRONG&gt;demo.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 18:33:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Multicore-flexio/m-p/1839630#M222065</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-04-02T18:33:52Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 Multicore flexio</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Multicore-flexio/m-p/1839813#M222076</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;Hi &lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442" target="_self"&gt;&lt;SPAN class=""&gt;josephlinares&lt;/SPAN&gt;&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Thanks for your comments,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;1. Here do you mean to say that I should take care about the flexio-gpio pin which must not be used in cortex-A55 Linux dts file right?&lt;/P&gt;&lt;P&gt;2. And if not present in dts file than it is safe to access flexio-gpio pin from cortex-M33 core, is it true?&lt;/P&gt;</description>
      <pubDate>Wed, 03 Apr 2024 04:11:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Multicore-flexio/m-p/1839813#M222076</guid>
      <dc:creator>NZP</dc:creator>
      <dc:date>2024-04-03T04:11:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 Multicore flexio</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Multicore-flexio/m-p/1840417#M222110</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;1. I do.&lt;/P&gt;
&lt;P&gt;2. It is.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 04 Apr 2024 03:43:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-Multicore-flexio/m-p/1840417#M222110</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-04-04T03:43:07Z</dc:date>
    </item>
  </channel>
</rss>