<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX8 boot image build</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-boot-image-build/m-p/1839461#M222058</link>
    <description>&lt;P&gt;This was actually the result of not having exactly the right u-boot git repo checked out. Painful lesson.&lt;/P&gt;</description>
    <pubDate>Tue, 02 Apr 2024 14:34:07 GMT</pubDate>
    <dc:creator>dfurtney</dc:creator>
    <dc:date>2024-04-02T14:34:07Z</dc:date>
    <item>
      <title>iMX8 boot image build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-boot-image-build/m-p/1837952#M221944</link>
      <description>&lt;P&gt;I have built the Yocto project for imx8qxp and it works as expected. Following the LUG and YPUG i also built the imx-boot image by aggregating the required pieces. This boots, but ethernet is not working quite right (it appears up, I can ping out but nothing can get in) so TFTP doesn't work and I need it.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I noticed my final imx-boot file is about half the size of the yocto generated imx-boot. Looking through the recipes it is clear there is a lot more going on in the Yocto build but I really need to be able to do this without Yocto (for environment reasons).&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there something else I should be adding? Any help would be appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 29 Mar 2024 15:01:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-boot-image-build/m-p/1837952#M221944</guid>
      <dc:creator>dfurtney</dc:creator>
      <dc:date>2024-03-29T15:01:42Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 boot image build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-boot-image-build/m-p/1838037#M221950</link>
      <description>&lt;P&gt;you can refer to the chapter 4.5.13 How to build imx-boot image by using imx-mkimage of linux user guide, which has detailed steps, for imx-mkimage, you can find it from&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/imx-mkimage" target="_blank"&gt;https://github.com/nxp-imx/imx-mkimage&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 30 Mar 2024 01:45:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-boot-image-build/m-p/1838037#M221950</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-03-30T01:45:49Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8 boot image build</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8-boot-image-build/m-p/1839461#M222058</link>
      <description>&lt;P&gt;This was actually the result of not having exactly the right u-boot git repo checked out. Painful lesson.&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 14:34:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8-boot-image-build/m-p/1839461#M222058</guid>
      <dc:creator>dfurtney</dc:creator>
      <dc:date>2024-04-02T14:34:07Z</dc:date>
    </item>
  </channel>
</rss>