<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Efficientdet build issue in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Efficientdet-build-issue/m-p/1839028#M222028</link>
    <description>&lt;P&gt;Hi team,&lt;BR /&gt;I am trying to build the efficientdet-imx project and run it on imx8mp board.&amp;nbsp;&lt;BR /&gt;I am following this documentation:&lt;BR /&gt;&lt;A title="https://github.com/nxp-imx/efficientdet-imx" href="https://github.com/nxp-imx/efficientdet-imx" target="_blank" rel="noreferrer noopener"&gt;https://github.com/nxp-imx/efficientdet-imx&lt;/A&gt;&lt;/P&gt;&lt;P&gt;But it seems that the build process for the dependencies have changed.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;From the root directory of Tensorflow github, go to&amp;nbsp;tensorflow/lite/tools/make&amp;nbsp;and run&amp;nbsp;download_dependencies.sh&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Tensorflow have deprecated the use of Makefile for builds.&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;For Linux users, refer to&amp;nbsp;&lt;A title="https://docs.opencv.org/master/d7/d9f/tutorial_linux_install.html" href="https://docs.opencv.org/master/d7/d9f/tutorial_linux_install.html" target="_blank" rel="noreferrer noopener"&gt;https://docs.opencv.org/master/d7/d9f/tutorial_linux_install.html&lt;/A&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Also, while following OpenCV build process we are facing the following issue:&lt;/P&gt;&lt;P&gt;/home/progna/Downloads/toolchains/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu/bin/../lib/gcc/aarch64-linux-gnu/8.3.0/../../../../aarch64-linux-gnu/bin/ld: ../../3rdparty/ippicv/ippicv_lnx/icv/lib/intel64/libippicv.a(ippcpufeatures.o): Relocations in generic ELF (EM: 62)&lt;BR /&gt;/home/progna/Downloads/toolchains/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu/bin/../lib/gcc/aarch64-linux-gnu/8.3.0/../../../../aarch64-linux-gnu/bin/ld: ../../3rdparty/ippicv/ippicv_lnx/icv/lib/intel64/libippicv.a(ippcpufeatures.o): Relocations in generic ELF (EM: 62)&lt;BR /&gt;/home/progna/Downloads/toolchains/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu/bin/../lib/gcc/aarch64-linux-gnu/8.3.0/../../../../aarch64-linux-gnu/bin/ld: ../../3rdparty/ippicv/ippicv_lnx/icv/lib/intel64/libippicv.a: error adding symbols: file in wrong format&lt;BR /&gt;collect2: error: ld returned 1 exit status&lt;BR /&gt;make[2]: *** [modules/core/CMakeFiles/opencv_core.dir/build.make:1465: lib/libopencv_core.so.4.9.0] Error 1&lt;BR /&gt;make[1]: *** [CMakeFiles/Makefile2:2196: modules/core/CMakeFiles/opencv_core.dir/all] Error 2&lt;BR /&gt;make: *** [Makefile:163: all] Error 2&lt;/P&gt;&lt;P&gt;has context menu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, these are my queries:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Which cross compiler to use to compile the dependencies and the project for imx8mp board.&lt;/LI&gt;&lt;LI&gt;How to build the updated tensorflow lite using CMake.&lt;/LI&gt;&lt;LI&gt;How to fix the compilation issue for OpenCV.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;GitHub - nxp-imx/efficientdet-imx: EfficientDet is a family of object detection models for which we provide basic enablement on i.MX8 NXP boards.&lt;/P&gt;&lt;P&gt;EfficientDet is a family of object detection models for which we provide basic enablement on i.MX8 NXP boards. - nxp-imx/efficientdet-imx&lt;/P&gt;</description>
    <pubDate>Tue, 02 Apr 2024 06:53:55 GMT</pubDate>
    <dc:creator>rit2905</dc:creator>
    <dc:date>2024-04-02T06:53:55Z</dc:date>
    <item>
      <title>Efficientdet build issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Efficientdet-build-issue/m-p/1839028#M222028</link>
      <description>&lt;P&gt;Hi team,&lt;BR /&gt;I am trying to build the efficientdet-imx project and run it on imx8mp board.&amp;nbsp;&lt;BR /&gt;I am following this documentation:&lt;BR /&gt;&lt;A title="https://github.com/nxp-imx/efficientdet-imx" href="https://github.com/nxp-imx/efficientdet-imx" target="_blank" rel="noreferrer noopener"&gt;https://github.com/nxp-imx/efficientdet-imx&lt;/A&gt;&lt;/P&gt;&lt;P&gt;But it seems that the build process for the dependencies have changed.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;From the root directory of Tensorflow github, go to&amp;nbsp;tensorflow/lite/tools/make&amp;nbsp;and run&amp;nbsp;download_dependencies.sh&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Tensorflow have deprecated the use of Makefile for builds.&amp;nbsp;&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;For Linux users, refer to&amp;nbsp;&lt;A title="https://docs.opencv.org/master/d7/d9f/tutorial_linux_install.html" href="https://docs.opencv.org/master/d7/d9f/tutorial_linux_install.html" target="_blank" rel="noreferrer noopener"&gt;https://docs.opencv.org/master/d7/d9f/tutorial_linux_install.html&lt;/A&gt;&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Also, while following OpenCV build process we are facing the following issue:&lt;/P&gt;&lt;P&gt;/home/progna/Downloads/toolchains/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu/bin/../lib/gcc/aarch64-linux-gnu/8.3.0/../../../../aarch64-linux-gnu/bin/ld: ../../3rdparty/ippicv/ippicv_lnx/icv/lib/intel64/libippicv.a(ippcpufeatures.o): Relocations in generic ELF (EM: 62)&lt;BR /&gt;/home/progna/Downloads/toolchains/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu/bin/../lib/gcc/aarch64-linux-gnu/8.3.0/../../../../aarch64-linux-gnu/bin/ld: ../../3rdparty/ippicv/ippicv_lnx/icv/lib/intel64/libippicv.a(ippcpufeatures.o): Relocations in generic ELF (EM: 62)&lt;BR /&gt;/home/progna/Downloads/toolchains/gcc-arm-8.3-2019.03-x86_64-aarch64-linux-gnu/bin/../lib/gcc/aarch64-linux-gnu/8.3.0/../../../../aarch64-linux-gnu/bin/ld: ../../3rdparty/ippicv/ippicv_lnx/icv/lib/intel64/libippicv.a: error adding symbols: file in wrong format&lt;BR /&gt;collect2: error: ld returned 1 exit status&lt;BR /&gt;make[2]: *** [modules/core/CMakeFiles/opencv_core.dir/build.make:1465: lib/libopencv_core.so.4.9.0] Error 1&lt;BR /&gt;make[1]: *** [CMakeFiles/Makefile2:2196: modules/core/CMakeFiles/opencv_core.dir/all] Error 2&lt;BR /&gt;make: *** [Makefile:163: all] Error 2&lt;/P&gt;&lt;P&gt;has context menu&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, these are my queries:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Which cross compiler to use to compile the dependencies and the project for imx8mp board.&lt;/LI&gt;&lt;LI&gt;How to build the updated tensorflow lite using CMake.&lt;/LI&gt;&lt;LI&gt;How to fix the compilation issue for OpenCV.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;GitHub - nxp-imx/efficientdet-imx: EfficientDet is a family of object detection models for which we provide basic enablement on i.MX8 NXP boards.&lt;/P&gt;&lt;P&gt;EfficientDet is a family of object detection models for which we provide basic enablement on i.MX8 NXP boards. - nxp-imx/efficientdet-imx&lt;/P&gt;</description>
      <pubDate>Tue, 02 Apr 2024 06:53:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Efficientdet-build-issue/m-p/1839028#M222028</guid>
      <dc:creator>rit2905</dc:creator>
      <dc:date>2024-04-02T06:53:55Z</dc:date>
    </item>
    <item>
      <title>Re: Efficientdet build issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Efficientdet-build-issue/m-p/1841744#M222204</link>
      <description>&lt;P&gt;FYI.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.tensorflow.org/lite/guide/build_cmake" target="_blank"&gt;https://www.tensorflow.org/lite/guide/build_cmake&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://docs.opencv.org/4.x/d0/d76/tutorial_arm_crosscompile_with_cmake.html" target="_blank"&gt;https://docs.opencv.org/4.x/d0/d76/tutorial_arm_crosscompile_with_cmake.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 07 Apr 2024 08:44:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Efficientdet-build-issue/m-p/1841744#M222204</guid>
      <dc:creator>jimmychan</dc:creator>
      <dc:date>2024-04-07T08:44:12Z</dc:date>
    </item>
  </channel>
</rss>