<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic iMX8MM Chromium cannot play MP4 video in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MM-Chromium-cannot-play-MP4-video/m-p/1834604#M221735</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am using Kirkstone 5.15.32 to build for the imx8mm-evk 'imx-image-full' and also added Chromium&amp;nbsp;96.0.4664.110 to the image. From the image we are trying to run a mp4 video (1280p) resolution on the chromium browser but it doesn't play it. No errors from console as well. We then tried to play a webm format video. The browser does play but the video was smooth can see stuttering all along. When we use gst-launch to run the both format video plays fine (using playbin pipeline)&lt;/P&gt;&lt;P&gt;We are not seeing the same with imx8mp evk. So the query is,&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Does imx8mm support propriety codecs like&amp;nbsp;mp4 in the chromium browser?&lt;/P&gt;&lt;P&gt;2. Are imx8mm h/w capabilities not fully utilised from chromium? if so are there any flags needs to be set in chromium recipe to make it work. Thanks&lt;/P&gt;</description>
    <pubDate>Mon, 25 Mar 2024 11:39:21 GMT</pubDate>
    <dc:creator>raajeshk88</dc:creator>
    <dc:date>2024-03-25T11:39:21Z</dc:date>
    <item>
      <title>iMX8MM Chromium cannot play MP4 video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MM-Chromium-cannot-play-MP4-video/m-p/1834604#M221735</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; I am using Kirkstone 5.15.32 to build for the imx8mm-evk 'imx-image-full' and also added Chromium&amp;nbsp;96.0.4664.110 to the image. From the image we are trying to run a mp4 video (1280p) resolution on the chromium browser but it doesn't play it. No errors from console as well. We then tried to play a webm format video. The browser does play but the video was smooth can see stuttering all along. When we use gst-launch to run the both format video plays fine (using playbin pipeline)&lt;/P&gt;&lt;P&gt;We are not seeing the same with imx8mp evk. So the query is,&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. Does imx8mm support propriety codecs like&amp;nbsp;mp4 in the chromium browser?&lt;/P&gt;&lt;P&gt;2. Are imx8mm h/w capabilities not fully utilised from chromium? if so are there any flags needs to be set in chromium recipe to make it work. Thanks&lt;/P&gt;</description>
      <pubDate>Mon, 25 Mar 2024 11:39:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MM-Chromium-cannot-play-MP4-video/m-p/1834604#M221735</guid>
      <dc:creator>raajeshk88</dc:creator>
      <dc:date>2024-03-25T11:39:21Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MM Chromium cannot play MP4 video</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MM-Chromium-cannot-play-MP4-video/m-p/1842522#M222262</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/95841"&gt;@raajeshk88&lt;/a&gt;,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support.&lt;/P&gt;
&lt;P&gt;You can try with the following flags for the best Chromium performance.&lt;/P&gt;
&lt;P&gt;chromium --no-sandbox --no-first-run --noerrdialogs --start-fullscreen --start-maximized --disable-notifications --disable-infobars --kiosk --incognito --fullscreen --test-type --disable-popup-blocking --enable-gpu-rasterization&lt;/P&gt;
&lt;P&gt;Have a great day!&lt;/P&gt;</description>
      <pubDate>Mon, 08 Apr 2024 15:19:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MM-Chromium-cannot-play-MP4-video/m-p/1842522#M222262</guid>
      <dc:creator>brian14</dc:creator>
      <dc:date>2024-04-08T15:19:04Z</dc:date>
    </item>
  </channel>
</rss>