<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPin muxing</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Pin-muxing/m-p/1833265#M221628</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;I am using I.MX8M plus based SOC.&lt;BR /&gt;In that I wan to use a particular pin for GPIO purpose.&lt;BR /&gt;From I.MX8M plus application note document from NXP website, I am able to see in &lt;STRONG&gt;chapter 8, section 8.1 External signals and pin multiplexing .&lt;BR /&gt;&lt;/STRONG&gt;Page number 1295 , in that port names : HDMI_HPD and&amp;nbsp;HDMI_HPD_O&lt;BR /&gt;Are the two pins I am trying to reuse.&lt;BR /&gt;How can I find, these pins are connected which GPIO number?&lt;BR /&gt;Because I wan to edit my DTS file,&amp;nbsp;&lt;BR /&gt;Can you please help me on this ?&lt;/P&gt;</description>
    <pubDate>Thu, 21 Mar 2024 23:42:17 GMT</pubDate>
    <dc:creator>Rabiraj</dc:creator>
    <dc:date>2024-03-21T23:42:17Z</dc:date>
    <item>
      <title>Pin muxing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-muxing/m-p/1833265#M221628</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I am using I.MX8M plus based SOC.&lt;BR /&gt;In that I wan to use a particular pin for GPIO purpose.&lt;BR /&gt;From I.MX8M plus application note document from NXP website, I am able to see in &lt;STRONG&gt;chapter 8, section 8.1 External signals and pin multiplexing .&lt;BR /&gt;&lt;/STRONG&gt;Page number 1295 , in that port names : HDMI_HPD and&amp;nbsp;HDMI_HPD_O&lt;BR /&gt;Are the two pins I am trying to reuse.&lt;BR /&gt;How can I find, these pins are connected which GPIO number?&lt;BR /&gt;Because I wan to edit my DTS file,&amp;nbsp;&lt;BR /&gt;Can you please help me on this ?&lt;/P&gt;</description>
      <pubDate>Thu, 21 Mar 2024 23:42:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-muxing/m-p/1833265#M221628</guid>
      <dc:creator>Rabiraj</dc:creator>
      <dc:date>2024-03-21T23:42:17Z</dc:date>
    </item>
    <item>
      <title>Re: Pin muxing</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Pin-muxing/m-p/1834150#M221700</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230915"&gt;@Rabiraj&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can search in&amp;nbsp;arch/arm64/boot/dts/freescale/imx8mp-pinfunc.h&lt;/P&gt;
&lt;P&gt;For example, you can reuse HDMI_HPD pad as GPIO3_IO29&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;#define MX8MP_IOMUXC_HDMI_HPD__HDMIMIX_HDMI_HPD                      0x24C 0x4AC 0x000 0x0 0x0
#define MX8MP_IOMUXC_HDMI_HPD__AUDIOMIX_HDMI_HPD_O                   0x24C 0x4AC 0x000 0x1 0x0
#define MX8MP_IOMUXC_HDMI_HPD__I2C6_SDA                              0x24C 0x4AC 0x5D0 0x3 0x3
#define MX8MP_IOMUXC_HDMI_HPD__CAN2_RX                               0x24C 0x4AC 0x550 0x4 0x3
#define MX8MP_IOMUXC_HDMI_HPD__GPIO3_IO29                            0x24C 0x4AC 0x000 0x5 0x0
&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 25 Mar 2024 02:40:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Pin-muxing/m-p/1834150#M221700</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-03-25T02:40:28Z</dc:date>
    </item>
  </channel>
</rss>