<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem with UART framing error on custom i.MX7ULP board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-with-UART-framing-error-on-custom-i-MX7ULP-board/m-p/1832928#M221598</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a custom i.MX7ULP board that has4 UARTs, one for the serial interface for linux. I am having a problem as when I set the baud rate higher than 2400, I cannot receive more than 8 characters. It always stops at 8. I sometimes get a framing error when looking with a digital discovery analyser. This seems weird as all 3 uarts that I tested on have the same problem. It works without problem at 2400 but when I set at the default 115200, it just stops at the 8th character and cannot receive anything else. I have attached the dts files for my board as I suspect it may be an issue with the clock or something, but I am not sure. UART5 6 and 7 are the problem.&lt;/P&gt;</description>
    <pubDate>Thu, 21 Mar 2024 11:59:10 GMT</pubDate>
    <dc:creator>Alexandre50000</dc:creator>
    <dc:date>2024-03-21T11:59:10Z</dc:date>
    <item>
      <title>Problem with UART framing error on custom i.MX7ULP board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-with-UART-framing-error-on-custom-i-MX7ULP-board/m-p/1832928#M221598</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am working on a custom i.MX7ULP board that has4 UARTs, one for the serial interface for linux. I am having a problem as when I set the baud rate higher than 2400, I cannot receive more than 8 characters. It always stops at 8. I sometimes get a framing error when looking with a digital discovery analyser. This seems weird as all 3 uarts that I tested on have the same problem. It works without problem at 2400 but when I set at the default 115200, it just stops at the 8th character and cannot receive anything else. I have attached the dts files for my board as I suspect it may be an issue with the clock or something, but I am not sure. UART5 6 and 7 are the problem.&lt;/P&gt;</description>
      <pubDate>Thu, 21 Mar 2024 11:59:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-with-UART-framing-error-on-custom-i-MX7ULP-board/m-p/1832928#M221598</guid>
      <dc:creator>Alexandre50000</dc:creator>
      <dc:date>2024-03-21T11:59:10Z</dc:date>
    </item>
  </channel>
</rss>