<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックKernel Error when writing to CAAM Encrypted Partition</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Error-when-writing-to-CAAM-Encrypted-Partition/m-p/1832365#M221548</link>
    <description>&lt;P&gt;We are currently running into an issue were we are getting a kernel error every once in a while when writing to an encrypted partition set up following AN12714 Rev. 2. Sometimes the kernel will report a crash saying "Unable to handle kernel paging request at virtual address". I was able to recreate the crash by using the dd command to write a large file to the encrypted partition. However, it does not seem to cause the crash every time. Below is some more information on our hardware setup:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;i.MX8QM&lt;UL&gt;&lt;LI&gt;custom board closely resembling the i.MX8QM MEK (same RAM layout/chip/settings)&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;linux-imx : lf-6.1.22-2.0.0&lt;/LI&gt;&lt;LI&gt;differences from AN12714&lt;UL&gt;&lt;LI&gt;encrypted.img is 10GB instead of 32MB&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Do you have any idea what the cause of this crash could be? is there any issue to how we are using the CAAM?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/173661"&gt;@rlgagliardo&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 20 Mar 2024 22:57:53 GMT</pubDate>
    <dc:creator>gilmoreat</dc:creator>
    <dc:date>2024-03-20T22:57:53Z</dc:date>
    <item>
      <title>Kernel Error when writing to CAAM Encrypted Partition</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Error-when-writing-to-CAAM-Encrypted-Partition/m-p/1832365#M221548</link>
      <description>&lt;P&gt;We are currently running into an issue were we are getting a kernel error every once in a while when writing to an encrypted partition set up following AN12714 Rev. 2. Sometimes the kernel will report a crash saying "Unable to handle kernel paging request at virtual address". I was able to recreate the crash by using the dd command to write a large file to the encrypted partition. However, it does not seem to cause the crash every time. Below is some more information on our hardware setup:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;i.MX8QM&lt;UL&gt;&lt;LI&gt;custom board closely resembling the i.MX8QM MEK (same RAM layout/chip/settings)&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;linux-imx : lf-6.1.22-2.0.0&lt;/LI&gt;&lt;LI&gt;differences from AN12714&lt;UL&gt;&lt;LI&gt;encrypted.img is 10GB instead of 32MB&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Do you have any idea what the cause of this crash could be? is there any issue to how we are using the CAAM?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/173661"&gt;@rlgagliardo&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 20 Mar 2024 22:57:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Error-when-writing-to-CAAM-Encrypted-Partition/m-p/1832365#M221548</guid>
      <dc:creator>gilmoreat</dc:creator>
      <dc:date>2024-03-20T22:57:53Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Error when writing to CAAM Encrypted Partition</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Error-when-writing-to-CAAM-Encrypted-Partition/m-p/1835403#M221804</link>
      <description>&lt;P&gt;Have you tried to refer to the&amp;nbsp;&amp;lt;&lt;SPAN class="fontstyle0"&gt;10 Security&amp;gt;&amp;nbsp;&lt;/SPAN&gt;Linux user Guide&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf" target="_self"&gt;IMX_LINUX_USERS_GUIDE.pdf&lt;/A&gt;. an12714 was not recommended.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Tue, 26 Mar 2024 11:10:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Error-when-writing-to-CAAM-Encrypted-Partition/m-p/1835403#M221804</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-03-26T11:10:35Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Error when writing to CAAM Encrypted Partition</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Error-when-writing-to-CAAM-Encrypted-Partition/m-p/1836623#M221870</link>
      <description>&lt;P&gt;Thanks for the reply. After further troubleshooting, it looks like it is not specifically tied to the CAAM encryption. I was able to get an crash by just creating 6 threads of "yes &amp;gt; /dev/null".&amp;nbsp;&lt;/P&gt;&lt;P&gt;I was looking through the&amp;nbsp;IMX8_1N94W errata document and&amp;nbsp;ERR050104 mentioned a cache coherency issue. Could this be related to the crash? Is there already a patch in the kernel to address this issue?&lt;/P&gt;</description>
      <pubDate>Wed, 27 Mar 2024 17:31:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Error-when-writing-to-CAAM-Encrypted-Partition/m-p/1836623#M221870</guid>
      <dc:creator>gilmoreat</dc:creator>
      <dc:date>2024-03-27T17:31:16Z</dc:date>
    </item>
    <item>
      <title>Re: Kernel Error when writing to CAAM Encrypted Partition</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Kernel-Error-when-writing-to-CAAM-Encrypted-Partition/m-p/1896210#M225635</link>
      <description>&lt;P&gt;We had something similar - the issue seemed to be resolved by dropping the clock frequency down from 1.6GHz to 1.3GHz.&lt;/P&gt;</description>
      <pubDate>Sat, 29 Jun 2024 17:09:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Kernel-Error-when-writing-to-CAAM-Encrypted-Partition/m-p/1896210#M225635</guid>
      <dc:creator>rlgagliardo</dc:creator>
      <dc:date>2024-06-29T17:09:59Z</dc:date>
    </item>
  </channel>
</rss>