<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Configure kernel using menuconfig inside yocto in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Configure-kernel-using-menuconfig-inside-yocto/m-p/1830244#M221410</link>
    <description>&lt;P&gt;Hi,&lt;BR /&gt;I am trying to configure the kernel using menuconfig.&lt;BR /&gt;I am able to download the linux-imx kernel and build it.&lt;BR /&gt;then use make menuconfig and, GUI prompt is appearing for editing.&lt;BR /&gt;I want to do the same with my yocto BSP.&lt;BR /&gt;I am using phyCore-i.mx 8m plus SOM&lt;BR /&gt;Can you say me, which command should I use ?&lt;/P&gt;</description>
    <pubDate>Mon, 18 Mar 2024 10:46:57 GMT</pubDate>
    <dc:creator>Rabiraj</dc:creator>
    <dc:date>2024-03-18T10:46:57Z</dc:date>
    <item>
      <title>Configure kernel using menuconfig inside yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configure-kernel-using-menuconfig-inside-yocto/m-p/1830244#M221410</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I am trying to configure the kernel using menuconfig.&lt;BR /&gt;I am able to download the linux-imx kernel and build it.&lt;BR /&gt;then use make menuconfig and, GUI prompt is appearing for editing.&lt;BR /&gt;I want to do the same with my yocto BSP.&lt;BR /&gt;I am using phyCore-i.mx 8m plus SOM&lt;BR /&gt;Can you say me, which command should I use ?&lt;/P&gt;</description>
      <pubDate>Mon, 18 Mar 2024 10:46:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configure-kernel-using-menuconfig-inside-yocto/m-p/1830244#M221410</guid>
      <dc:creator>Rabiraj</dc:creator>
      <dc:date>2024-03-18T10:46:57Z</dc:date>
    </item>
    <item>
      <title>Re: Configure kernel using menuconfig inside yocto</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Configure-kernel-using-menuconfig-inside-yocto/m-p/1831198#M221466</link>
      <description>&lt;P&gt;bitbake -c menuconfig linux-imx&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Tue, 19 Mar 2024 13:27:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Configure-kernel-using-menuconfig-inside-yocto/m-p/1831198#M221466</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2024-03-19T13:27:23Z</dc:date>
    </item>
  </channel>
</rss>