<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Add custom packages in yocto final image.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Add-custom-packages-in-yocto-final-image/m-p/1827412#M221229</link>
    <description>&lt;P&gt;I am using an &lt;STRONG&gt;I.MX8M&lt;/STRONG&gt; plus processor.&amp;nbsp;&lt;BR /&gt;I am using Yocto for building my final image.&lt;BR /&gt;I can successfully create a custom meta-layer and a recipe.&lt;BR /&gt;Where I can also have my application code and compile my final image.&lt;BR /&gt;My application code is written using a Python programming language.&lt;BR /&gt;I need a few packages to be installed for that python application to run.&lt;BR /&gt;I can add the packages in build/local.conf file.&lt;BR /&gt;like :&amp;nbsp;&lt;BR /&gt;&lt;SPAN class=""&gt;IMAGE_INSTALL:append&amp;nbsp;=&amp;nbsp;"&amp;nbsp;python3"&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;IMAGE_INSTALL:append&amp;nbsp;=&amp;nbsp;"&amp;nbsp;python3-scons"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;But I don't want to add in local.conf file which is in build directory.&lt;BR /&gt;Can you suggest me a way to add any packages using my recipe itself, instead of using any existing recipe.&lt;BR /&gt;Is it possible to do, if yes , please help me with that?&lt;/P&gt;</description>
    <pubDate>Wed, 13 Mar 2024 17:49:57 GMT</pubDate>
    <dc:creator>Rabiraj</dc:creator>
    <dc:date>2024-03-13T17:49:57Z</dc:date>
    <item>
      <title>Add custom packages in yocto final image.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Add-custom-packages-in-yocto-final-image/m-p/1827412#M221229</link>
      <description>&lt;P&gt;I am using an &lt;STRONG&gt;I.MX8M&lt;/STRONG&gt; plus processor.&amp;nbsp;&lt;BR /&gt;I am using Yocto for building my final image.&lt;BR /&gt;I can successfully create a custom meta-layer and a recipe.&lt;BR /&gt;Where I can also have my application code and compile my final image.&lt;BR /&gt;My application code is written using a Python programming language.&lt;BR /&gt;I need a few packages to be installed for that python application to run.&lt;BR /&gt;I can add the packages in build/local.conf file.&lt;BR /&gt;like :&amp;nbsp;&lt;BR /&gt;&lt;SPAN class=""&gt;IMAGE_INSTALL:append&amp;nbsp;=&amp;nbsp;"&amp;nbsp;python3"&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;IMAGE_INSTALL:append&amp;nbsp;=&amp;nbsp;"&amp;nbsp;python3-scons"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;But I don't want to add in local.conf file which is in build directory.&lt;BR /&gt;Can you suggest me a way to add any packages using my recipe itself, instead of using any existing recipe.&lt;BR /&gt;Is it possible to do, if yes , please help me with that?&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 17:49:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Add-custom-packages-in-yocto-final-image/m-p/1827412#M221229</guid>
      <dc:creator>Rabiraj</dc:creator>
      <dc:date>2024-03-13T17:49:57Z</dc:date>
    </item>
  </channel>
</rss>