<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Installing Packages in IMX6ull</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1827035#M221207</link>
    <description>&lt;P&gt;hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206761"&gt;@Chavira&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;i have build an image using the steps in the guide for IMx6. i can see the file with extension .wic.zst. i would like to know how to flash this into an sdcard.&lt;BR /&gt;i understand this is the command to run :&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;uuu -b sd_all &amp;lt;bootloader&amp;gt; &amp;lt;rootfs (.wic)&amp;gt;&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;but my problem is i cant understand which bootloader file to use as there as multiple files iwt name u-boot and in this example i can see the files used are having extension sd.bin_flas_evk but i cant find a file with this extension in my folder.&lt;/P&gt;&lt;P&gt;Can you please let me know the file to be used as bootloader.&lt;/P&gt;&lt;P&gt;Also when i try the above command with the file as u-boot.imx i get&lt;/P&gt;&lt;P&gt;Wait for unknown drivers...&lt;/P&gt;&lt;P&gt;kind of errors. even though the card reader is detected by the system.&lt;/P&gt;&lt;P&gt;I am using a VM for building&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please help me if you have any suggestion or solution to this&lt;/P&gt;</description>
    <pubDate>Wed, 13 Mar 2024 09:51:11 GMT</pubDate>
    <dc:creator>athul_am</dc:creator>
    <dc:date>2024-03-13T09:51:11Z</dc:date>
    <item>
      <title>Installing Packages in IMX6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1815512#M220405</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have just acquired the latest imx6 board and i am trying install some libraries in it.&lt;/P&gt;&lt;P&gt;I tried using apt,apt-get commands but that&amp;nbsp; doesnt work as i am using the image given in the box itself.&lt;/P&gt;&lt;P&gt;So can someone please let me know if i can install libraries in the board and if it is possible how to do it?&lt;/P&gt;&lt;P&gt;I am using the board for this 1st time so any help will be really good.&lt;/P&gt;&lt;P&gt;i am using imx6ull and the OS the image has is NXP i.mx Release Distro version 4.9.88-2.0.0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Athul&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Feb 2024 10:55:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1815512#M220405</guid>
      <dc:creator>athul_am</dc:creator>
      <dc:date>2024-02-26T10:55:47Z</dc:date>
    </item>
    <item>
      <title>Re: Installing Packages in IMX6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1815812#M220435</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226643"&gt;@athul_am&lt;/a&gt;!&lt;/P&gt;&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;&lt;P&gt;To add any package based on our BSP you have to compile the image.&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;You have to add the next on the conf/local.conf .&lt;/P&gt;&lt;P&gt;Examples:&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;IMAGE_INSTALL += "pcsc-lite"&lt;BR /&gt;IMAGE_INSTALL += "pcsc-lite-dev"&lt;BR /&gt;IMAGE_INSTALL += "pcsc-lite-lib"&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;And then compile the image using the command bitbake &amp;lt;image&amp;gt;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;The image could be "imx-image-multimedia",&amp;nbsp;&lt;BR /&gt;"imx-image-full",&amp;nbsp;&lt;BR /&gt;"imx-image-core", etc.&lt;/P&gt;&lt;P&gt;Best Regads!&lt;/P&gt;&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Mon, 26 Feb 2024 17:09:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1815812#M220435</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-02-26T17:09:02Z</dc:date>
    </item>
    <item>
      <title>Re: Installing Packages in IMX6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1816045#M220447</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thank you for the Response.&lt;/P&gt;&lt;P&gt;So i cant install anything&amp;nbsp; directly in the image right?&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Athul&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 02:02:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1816045#M220447</guid>
      <dc:creator>athul_am</dc:creator>
      <dc:date>2024-02-27T02:02:28Z</dc:date>
    </item>
    <item>
      <title>Re: Installing Packages in IMX6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1816360#M220467</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Since i cant install any library i am trying to cross compile the libraries i need to do install using a toolchain the toolchain i am using for the same is&amp;nbsp;&lt;A href="https://developer.arm.com/-/media/Files/downloads/gnu/13.2.rel1/binrel/arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-linux-gnueabihf.tar.xz?rev=adb0c0238c934aeeaa12c09609c5e6fc&amp;amp;hash=68DA67DE12CBAD82A0FA4B75247E866155C93053" target="_blank"&gt;https://developer.arm.com/-/media/Files/downloads/gnu/13.2.rel1/binrel/arm-gnu-toolchain-13.2.rel1-x86_64-arm-none-linux-gnueabihf.tar.xz?rev=adb0c0238c934aeeaa12c09609c5e6fc&amp;amp;hash=68DA67DE12CBAD82A0FA4B75247E866155C93053.&lt;/A&gt;&lt;/P&gt;&lt;P&gt;i am able to compile the boost lib but not the the openssl and vsomeip libs i get compiler broken for vsomeip and&amp;nbsp;crypto/aes/aesv8-armx.S: Assembler messages:&lt;BR /&gt;crypto/aes/aesv8-armx.S:4: Error: unknown architecture `armv8-a+crypto' error for openssl&amp;nbsp;&lt;/P&gt;&lt;P&gt;Am i using the wrong toolchain or this is some other issue?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Athul&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 08:41:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1816360#M220467</guid>
      <dc:creator>athul_am</dc:creator>
      <dc:date>2024-02-27T08:41:19Z</dc:date>
    </item>
    <item>
      <title>Re: Installing Packages in IMX6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1816584#M220480</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226643"&gt;@athul_am&lt;/a&gt;!&lt;BR /&gt;&lt;BR /&gt;You have to compile the toolchain.&lt;BR /&gt;&lt;BR /&gt;Please check the next guide for the same.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Detailed-Operations-For-Standalone-On-Linux-BSP-of-I-MX/ta-p/1118682" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Detailed-Operations-For-Standalone-On-Linux-BSP-of-I-MX/ta-p/1118682&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 13:35:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1816584#M220480</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-02-27T13:35:03Z</dc:date>
    </item>
    <item>
      <title>Re: Installing Packages in IMX6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1827035#M221207</link>
      <description>&lt;P&gt;hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206761"&gt;@Chavira&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;i have build an image using the steps in the guide for IMx6. i can see the file with extension .wic.zst. i would like to know how to flash this into an sdcard.&lt;BR /&gt;i understand this is the command to run :&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;uuu -b sd_all &amp;lt;bootloader&amp;gt; &amp;lt;rootfs (.wic)&amp;gt;&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;but my problem is i cant understand which bootloader file to use as there as multiple files iwt name u-boot and in this example i can see the files used are having extension sd.bin_flas_evk but i cant find a file with this extension in my folder.&lt;/P&gt;&lt;P&gt;Can you please let me know the file to be used as bootloader.&lt;/P&gt;&lt;P&gt;Also when i try the above command with the file as u-boot.imx i get&lt;/P&gt;&lt;P&gt;Wait for unknown drivers...&lt;/P&gt;&lt;P&gt;kind of errors. even though the card reader is detected by the system.&lt;/P&gt;&lt;P&gt;I am using a VM for building&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please help me if you have any suggestion or solution to this&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 09:51:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1827035#M221207</guid>
      <dc:creator>athul_am</dc:creator>
      <dc:date>2024-03-13T09:51:11Z</dc:date>
    </item>
    <item>
      <title>Re: Installing Packages in IMX6ull</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1827211#M221217</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/226643"&gt;@athul_am&lt;/a&gt;!&lt;BR /&gt;&lt;BR /&gt;No, only with the Yocto Project.&lt;BR /&gt;&lt;BR /&gt;Sorry for the mistake!&lt;BR /&gt;&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 13:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Installing-Packages-in-IMX6ull/m-p/1827211#M221217</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-03-13T13:38:57Z</dc:date>
    </item>
  </channel>
</rss>