<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IMX8m-plus ECSPI2 MISO problem</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8m-plus-ECSPI2-MISO-problem/m-p/1826596#M221162</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;Are the settings for speed equal in both sides?&lt;/P&gt;
&lt;P&gt;Have you tried with other modules maybe from other vendors?&lt;/P&gt;
&lt;P&gt;I would strongly recommend to try to reproduce within two boards and if this is not possible, UART3P3 has a pinmux ability for ECSPI1.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 12 Mar 2024 22:18:51 GMT</pubDate>
    <dc:creator>JosephAtNXP</dc:creator>
    <dc:date>2024-03-12T22:18:51Z</dc:date>
    <item>
      <title>IMX8m-plus ECSPI2 MISO problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8m-plus-ECSPI2-MISO-problem/m-p/1826360#M221151</link>
      <description>&lt;LI-SPOILER&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;We use SOM IMX8m-plus form Compulab. An external spi module is connected to this SOM via ECSPI2 interface. This module is the only one connected to this ECSPI2, there are no other devices. When I connect the oscilloscope to the spi lines, the CS, MOSI and SCK lines behave correctly. But there is a problem with the MISO line.&lt;BR /&gt;&lt;BR /&gt;When it is disconnected from the SOM imx8, the correct data from the external module is visible on the oscilloscope. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MISO_connected.jpg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/267890iADBBE7072FFA1F0E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="MISO_connected.jpg" alt="MISO_connected.jpg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;MISO_connected.jpg&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;BR /&gt;But if I connect MISO line to SOM imx8, the data changes.&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MISO_disconected.JPEG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/267889i47F771504EEAF0BE/image-size/medium?v=v2&amp;amp;px=400" role="button" title="MISO_disconected.JPEG" alt="MISO_disconected.JPEG" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;MISO_disconected.JPEG&lt;/span&gt;&lt;/span&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;BR /&gt;We checked the external spi module and hardware, everything works well.&lt;BR /&gt;&lt;BR /&gt;We assume that the problem is in the IMX8 ECSPI settings.&lt;BR /&gt;&lt;BR /&gt;Are there any additional settings in the device tree or the kernel driver for ECSPI?&lt;BR /&gt;&lt;BR /&gt;I will be very grateful if you can send an example of how to properly set up a MISO line.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Thank you.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/LI-SPOILER&gt;</description>
      <pubDate>Tue, 12 Mar 2024 15:27:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8m-plus-ECSPI2-MISO-problem/m-p/1826360#M221151</guid>
      <dc:creator>Tolmachov</dc:creator>
      <dc:date>2024-03-12T15:27:14Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8m-plus ECSPI2 MISO problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8m-plus-ECSPI2-MISO-problem/m-p/1826596#M221162</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;Are the settings for speed equal in both sides?&lt;/P&gt;
&lt;P&gt;Have you tried with other modules maybe from other vendors?&lt;/P&gt;
&lt;P&gt;I would strongly recommend to try to reproduce within two boards and if this is not possible, UART3P3 has a pinmux ability for ECSPI1.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 12 Mar 2024 22:18:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8m-plus-ECSPI2-MISO-problem/m-p/1826596#M221162</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-03-12T22:18:51Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8m-plus ECSPI2 MISO problem</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8m-plus-ECSPI2-MISO-problem/m-p/1827022#M221205</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Thank you very much for your answer.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Yes, master and slave work at the same speed.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;We also tried connecting this external module to the Raspberry Pi, it works.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;We observe such strange behavior of miso only on SOM IMX8m-plus.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Perhaps there are some specific settings for the miso pin or spi controller?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;We have also already seen a similar problem on this forum without an answer. &lt;A href="https://community.nxp.com/t5/i-MX-Processors/IMX8QM-SPI-MISO-line-not-working/td-p/1441266" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/IMX8QM-SPI-MISO-line-not-working/td-p/1441266&lt;/A&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Mar 2024 09:38:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8m-plus-ECSPI2-MISO-problem/m-p/1827022#M221205</guid>
      <dc:creator>Tolmachov</dc:creator>
      <dc:date>2024-03-13T09:38:23Z</dc:date>
    </item>
  </channel>
</rss>