<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックU-Boot Frame Buffer Problem upon Reboot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-Frame-Buffer-Problem-upon-Reboot/m-p/248220#M22108</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am using IMX6Q Nitrogen6x Board from Boundary Devices. I have an BMP Image to be displayed onto HDMI Display, whenever u-boot starts. I have enabled BMP feature in U-Boot and a script is employed to automatically display the image when u-boot starts. When I power cycle the board (remove the power connector and plug it back), I am able to see the image. But when I issue a reboot after booting into ubuntu, and enter u-boot, this image is not getting displayed. I feel my Frame Buffer is messed up when I reboot. Has anyone come across this issue? If so, let me know how did you overcome it. Any pointers or suggestions are much appreciated. Also let me know if I should suspect HDMI registers (As per my understanding upon reboot, all hdmi registers are taken to reset state, which is same as just powered state). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FYI:&lt;/P&gt;&lt;P&gt;The version of u-boot that I am using is the "production" branch from&amp;nbsp; &lt;A href="https://github.com/boundarydevices/u-boot-imx6" title="https://github.com/boundarydevices/u-boot-imx6"&gt;boundarydevices/u-boot-imx6 · GitHub&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE class="shell plain"&gt;&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Balaji V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 21 May 2013 05:38:39 GMT</pubDate>
    <dc:creator>Balaji_ng</dc:creator>
    <dc:date>2013-05-21T05:38:39Z</dc:date>
    <item>
      <title>U-Boot Frame Buffer Problem upon Reboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-Frame-Buffer-Problem-upon-Reboot/m-p/248220#M22108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; I am using IMX6Q Nitrogen6x Board from Boundary Devices. I have an BMP Image to be displayed onto HDMI Display, whenever u-boot starts. I have enabled BMP feature in U-Boot and a script is employed to automatically display the image when u-boot starts. When I power cycle the board (remove the power connector and plug it back), I am able to see the image. But when I issue a reboot after booting into ubuntu, and enter u-boot, this image is not getting displayed. I feel my Frame Buffer is messed up when I reboot. Has anyone come across this issue? If so, let me know how did you overcome it. Any pointers or suggestions are much appreciated. Also let me know if I should suspect HDMI registers (As per my understanding upon reboot, all hdmi registers are taken to reset state, which is same as just powered state). &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FYI:&lt;/P&gt;&lt;P&gt;The version of u-boot that I am using is the "production" branch from&amp;nbsp; &lt;A href="https://github.com/boundarydevices/u-boot-imx6" title="https://github.com/boundarydevices/u-boot-imx6"&gt;boundarydevices/u-boot-imx6 · GitHub&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;CODE class="shell plain"&gt;&lt;/CODE&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Balaji V&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2013 05:38:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-Frame-Buffer-Problem-upon-Reboot/m-p/248220#M22108</guid>
      <dc:creator>Balaji_ng</dc:creator>
      <dc:date>2013-05-21T05:38:39Z</dc:date>
    </item>
    <item>
      <title>Re: U-Boot Frame Buffer Problem upon Reboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-Frame-Buffer-Problem-upon-Reboot/m-p/248221#M22109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Finally could resolve this problem. Please refer to the comments in the following link.&lt;/P&gt;&lt;P&gt;&lt;A href="http://boundarydevices.com/dvi-support-on-i-mx6-boards/" title="http://boundarydevices.com/dvi-support-on-i-mx6-boards/"&gt;http://boundarydevices.com/dvi-support-on-i-mx6-boards/&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Sep 2013 05:52:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-Frame-Buffer-Problem-upon-Reboot/m-p/248221#M22109</guid>
      <dc:creator>Balaji_ng</dc:creator>
      <dc:date>2013-09-04T05:52:46Z</dc:date>
    </item>
  </channel>
</rss>