<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックimx8mp ecspi miso runtime correction</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ecspi-miso-runtime-correction/m-p/1824095#M220966</link>
    <description>&lt;P&gt;we are using ecspi2 on ima8mp to connect extern ADC. if running spi on rather high speeds (20MHz) we have a runtime between SCLK and MISO of ~3 bits caused by ADUM1401 for galvanic insulation. i know from renesas rz/t1 we use in other system that there is a configurable runtime correction for MISO compared to SCLK that is great for handling such issues.&lt;/P&gt;&lt;P&gt;I searched the imx8mp manual but did not find something like this. is there a possibility to have that on imx8mp, of playing arround with polarity and phase does not help anymore?&lt;/P&gt;</description>
    <pubDate>Fri, 08 Mar 2024 10:44:14 GMT</pubDate>
    <dc:creator>martmanmtx</dc:creator>
    <dc:date>2024-03-08T10:44:14Z</dc:date>
    <item>
      <title>imx8mp ecspi miso runtime correction</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ecspi-miso-runtime-correction/m-p/1824095#M220966</link>
      <description>&lt;P&gt;we are using ecspi2 on ima8mp to connect extern ADC. if running spi on rather high speeds (20MHz) we have a runtime between SCLK and MISO of ~3 bits caused by ADUM1401 for galvanic insulation. i know from renesas rz/t1 we use in other system that there is a configurable runtime correction for MISO compared to SCLK that is great for handling such issues.&lt;/P&gt;&lt;P&gt;I searched the imx8mp manual but did not find something like this. is there a possibility to have that on imx8mp, of playing arround with polarity and phase does not help anymore?&lt;/P&gt;</description>
      <pubDate>Fri, 08 Mar 2024 10:44:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ecspi-miso-runtime-correction/m-p/1824095#M220966</guid>
      <dc:creator>martmanmtx</dc:creator>
      <dc:date>2024-03-08T10:44:14Z</dc:date>
    </item>
    <item>
      <title>Re: imx8mp ecspi miso runtime correction</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ecspi-miso-runtime-correction/m-p/1824286#M220984</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/230671"&gt;@martmanmtx&lt;/a&gt;!&lt;BR /&gt;Thank you for contacting NXP Support!&lt;BR /&gt;&lt;BR /&gt;By hardware, our IP doesn't have that feature but you can refer to our Linux Reference Manual, maybe you can implement the feature on software modifying our driver.&lt;BR /&gt;&lt;BR /&gt;Sorry for the mistake!&lt;BR /&gt;&lt;BR /&gt;Best Regards!&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Fri, 08 Mar 2024 16:26:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx8mp-ecspi-miso-runtime-correction/m-p/1824286#M220984</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-03-08T16:26:39Z</dc:date>
    </item>
  </channel>
</rss>