<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LIBUSB_ERROR_TIMEOUT in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-TIMEOUT/m-p/1822439#M220857</link>
    <description>&lt;P&gt;Im using IMX8MP board in that using fastboot 0 command im&amp;nbsp; flashing the device using UUU Tool i executed the uuu -v -b boot.lst command which will load the initramfs and kernel and boot the device and then linuxrc script will be executed after initramfs loaded then i executed the uuu -v -b emmc_burn_bsp.lst command which will make the partitions and flash the uboot and rootfs to the device partition but when im flashing the rootfs with ext4.verity file which size is 950 MB is flashing upto the 25% but after the it is throwing the LIBUSB_ERROR_TIMEOUT error but it flashed full image of rootfs.tar.bz2 extension which size is 160 MB so for this do i need to enable any kernel configs or any patches do i need to apply please give me the information any package should be added&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 07 Mar 2024 05:40:12 GMT</pubDate>
    <dc:creator>Ajayvk</dc:creator>
    <dc:date>2024-03-07T05:40:12Z</dc:date>
    <item>
      <title>LIBUSB_ERROR_TIMEOUT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-TIMEOUT/m-p/1822439#M220857</link>
      <description>&lt;P&gt;Im using IMX8MP board in that using fastboot 0 command im&amp;nbsp; flashing the device using UUU Tool i executed the uuu -v -b boot.lst command which will load the initramfs and kernel and boot the device and then linuxrc script will be executed after initramfs loaded then i executed the uuu -v -b emmc_burn_bsp.lst command which will make the partitions and flash the uboot and rootfs to the device partition but when im flashing the rootfs with ext4.verity file which size is 950 MB is flashing upto the 25% but after the it is throwing the LIBUSB_ERROR_TIMEOUT error but it flashed full image of rootfs.tar.bz2 extension which size is 160 MB so for this do i need to enable any kernel configs or any patches do i need to apply please give me the information any package should be added&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Mar 2024 05:40:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-TIMEOUT/m-p/1822439#M220857</guid>
      <dc:creator>Ajayvk</dc:creator>
      <dc:date>2024-03-07T05:40:12Z</dc:date>
    </item>
    <item>
      <title>Re: LIBUSB_ERROR_TIMEOUT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-TIMEOUT/m-p/1822557#M220861</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228421"&gt;@Ajayvk&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;BR clear="none" /&gt;&amp;nbsp;&lt;BR clear="none" /&gt;For Linux try to use "sudo".&lt;BR clear="none" /&gt;&amp;nbsp;&lt;BR clear="none" /&gt;For Windows try to open the PowerShell with administrator permissions.&lt;BR clear="none" /&gt;&amp;nbsp;&lt;BR clear="none" /&gt;If the problem persists, try to delete and download the uuu tool again.&lt;BR clear="none" /&gt;&amp;nbsp;&lt;BR clear="none" /&gt;Another cause can be the USB cable or the host computer, try changing the cable and the host computer if needed.&lt;BR clear="none" /&gt;&amp;nbsp;&lt;BR clear="none" /&gt;&amp;nbsp;&lt;A href="https://github.com/nxp-imx/mfgtools/releases/tag/uuu_1.5.125" target="_blank" rel="noopener" shape="rect"&gt;https://github.com/nxp-imx/mfgtools/releases/tag/uuu_1.5.125&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Wed, 06 Mar 2024 14:18:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-TIMEOUT/m-p/1822557#M220861</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-03-06T14:18:06Z</dc:date>
    </item>
    <item>
      <title>Re: LIBUSB_ERROR_TIMEOUT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-TIMEOUT/m-p/1822559#M220862</link>
      <description>&lt;P&gt;Thank you for the information I will try it&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Mar 2024 14:22:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-TIMEOUT/m-p/1822559#M220862</guid>
      <dc:creator>Ajayvk</dc:creator>
      <dc:date>2024-03-06T14:22:05Z</dc:date>
    </item>
    <item>
      <title>Re: LIBUSB_ERROR_TIMEOUT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-TIMEOUT/m-p/1822998#M220887</link>
      <description>&lt;P&gt;hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206761"&gt;@Chavira&lt;/a&gt;&amp;nbsp;I tried with your uuu tool but same Bulk(W):LIBUSB_TIMEOUT_ERROR is still&amp;nbsp; coming ,so do i need to configure anything because when i flash the 160 mB image it is working fine but the image which has size of 900MB it is throwing this error at Bulk(W):LIBUSB_TIMEOUT_ERROR so please give more information.&lt;/P&gt;</description>
      <pubDate>Thu, 07 Mar 2024 06:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-TIMEOUT/m-p/1822998#M220887</guid>
      <dc:creator>Ajayvk</dc:creator>
      <dc:date>2024-03-07T06:00:45Z</dc:date>
    </item>
    <item>
      <title>Re: LIBUSB_ERROR_TIMEOUT</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-TIMEOUT/m-p/1823632#M220938</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228421"&gt;@Ajayvk&lt;/a&gt;!&lt;BR /&gt;&lt;BR /&gt;Can you provide a detailed log of all the processes that you are doing, please?&lt;BR /&gt;&lt;BR /&gt;Is the image that are you referring is the kernel image?&lt;BR /&gt;&lt;BR /&gt;You can refer to the uuu usage with their User Manual&lt;BR /&gt;&lt;BR /&gt;Best Regards!&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Thu, 07 Mar 2024 21:10:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LIBUSB-ERROR-TIMEOUT/m-p/1823632#M220938</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-03-07T21:10:07Z</dc:date>
    </item>
  </channel>
</rss>