<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: lvds output not working on imx8qm in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/lvds-output-not-working-on-imx8qm/m-p/1819987#M220691</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225423"&gt;@Ahelion&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer the Android Quick Start Guide:&lt;A href="https://www.nxp.com.cn/docs/en/quick-reference-guide/ANDROID_QUICK_START_GUIDE.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/quick-reference-guide/ANDROID_QUICK_START_GUIDE.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;To test the LVDS-to-HDMI display, use the i.MX mini SAS cable to connect the LVDS-to-HDMI adapter to the "LVDS0/LVDS1" port.&lt;/P&gt;
&lt;P&gt;To test LVDS-to-HDMI/MIPI-DSI-to-HDMI display,&lt;STRONG&gt; it does not need to use the -d option&lt;/STRONG&gt;. Four display ports of LVDS0_CH0, LVDS1_CH0, MIPI_DSI0, and MIPI_DSI1 can be used for display individually or together.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Zhiming_Liu_0-1709511358235.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266139iFF587875C8E15A8E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Zhiming_Liu_0-1709511358235.png" alt="Zhiming_Liu_0-1709511358235.png" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
    <pubDate>Mon, 04 Mar 2024 00:17:06 GMT</pubDate>
    <dc:creator>Zhiming_Liu</dc:creator>
    <dc:date>2024-03-04T00:17:06Z</dc:date>
    <item>
      <title>lvds output not working on imx8qm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/lvds-output-not-working-on-imx8qm/m-p/1818806#M220593</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The hdmi connector on my mek device fell of, now I want to use the lvds, using the adapter that came in the imx8qm-mek demo box. I have no ideea how to get it to work.&lt;/P&gt;&lt;P&gt;I flashed the sd card via uuu, parameter hdmi, the NXP logo appears on my monitor ( connected via hdmi adapter to lvds), and then nothing, once linux starts display goes to sleep. I have tried the lvds1 dtbs :&lt;/P&gt;&lt;P&gt;vbmeta-imx8qm-lvds1-panel.img also, same result ( had to modify the script a bit to accept it )&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Here is the flash log:&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;PS C:\work\nxp\android-13.0.0_2.2.0_image_8qmek&amp;gt; .\uuu_imx_android_flash.bat -f imx8qm -a -e -t sd_all -u dual -d hdmi&lt;BR /&gt;This script is validated with uuu 1.4.182 version, it is recommended to align with this version.&lt;BR /&gt;dual bootloader is supported&lt;BR /&gt;dtbo is supported&lt;BR /&gt;dual slot is supported&lt;BR /&gt;dynamic partition is supported&lt;BR /&gt;vendor_boot is supported&lt;BR /&gt;init_boot is supported&lt;BR /&gt;generate lines to flash spl-imx8qm-dual.bin to the partition of bootloader0&lt;BR /&gt;generate lines to flash partition-table-dual.img to the partition of gpt&lt;BR /&gt;generate lines to flash bootloader-imx8qm-dual.img to the partition of bootloader_a&lt;BR /&gt;generate lines to flash dtbo-imx8qm-hdmi.img to the partition of dtbo_a&lt;BR /&gt;generate lines to flash vendor_boot.img to the partition of vendor_boot_a&lt;BR /&gt;generate lines to flash init_boot.img to the partition of init_boot_a&lt;BR /&gt;generate lines to flash boot.img to the partition of boot_a&lt;BR /&gt;generate lines to flash vbmeta-imx8qm-hdmi.img to the partition of vbmeta_a&lt;BR /&gt;generate lines to flash super.img to the partition of super&lt;BR /&gt;uuu script generated, start to invoke uuu with the generated uuu script&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.4.182-0-ga561ed7&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;Any help will be appreciated.&lt;/P&gt;&lt;P&gt;Br, Mircea&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 13:46:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/lvds-output-not-working-on-imx8qm/m-p/1818806#M220593</guid>
      <dc:creator>Ahelion</dc:creator>
      <dc:date>2024-02-29T13:46:30Z</dc:date>
    </item>
    <item>
      <title>Re: lvds output not working on imx8qm</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/lvds-output-not-working-on-imx8qm/m-p/1819987#M220691</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/225423"&gt;@Ahelion&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer the Android Quick Start Guide:&lt;A href="https://www.nxp.com.cn/docs/en/quick-reference-guide/ANDROID_QUICK_START_GUIDE.pdf" target="_blank"&gt;https://www.nxp.com.cn/docs/en/quick-reference-guide/ANDROID_QUICK_START_GUIDE.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;To test the LVDS-to-HDMI display, use the i.MX mini SAS cable to connect the LVDS-to-HDMI adapter to the "LVDS0/LVDS1" port.&lt;/P&gt;
&lt;P&gt;To test LVDS-to-HDMI/MIPI-DSI-to-HDMI display,&lt;STRONG&gt; it does not need to use the -d option&lt;/STRONG&gt;. Four display ports of LVDS0_CH0, LVDS1_CH0, MIPI_DSI0, and MIPI_DSI1 can be used for display individually or together.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Zhiming_Liu_0-1709511358235.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/266139iFF587875C8E15A8E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Zhiming_Liu_0-1709511358235.png" alt="Zhiming_Liu_0-1709511358235.png" /&gt;&lt;/span&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Mon, 04 Mar 2024 00:17:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/lvds-output-not-working-on-imx8qm/m-p/1819987#M220691</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2024-03-04T00:17:06Z</dc:date>
    </item>
  </channel>
</rss>