<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: U-Boot FASTBOOT flash commands for QSPI storage for iMX8M Nano EVK board in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-FASTBOOT-flash-commands-for-QSPI-storage-for-iMX8M-Nano/m-p/1819855#M220684</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Yes, it is not supported by default, you may use fastboot and use uboot command to download uboot. Is the same procedure we have for UUU tool.&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://github.com/nxp-imx/mfgtools/blob/master/uuu/qspi_burn_loader.lst" target="_blank"&gt;https://github.com/nxp-imx/mfgtools/blob/master/uuu/qspi_burn_loader.lst&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Fri, 01 Mar 2024 23:54:34 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2024-03-01T23:54:34Z</dc:date>
    <item>
      <title>U-Boot FASTBOOT flash commands for QSPI storage for iMX8M Nano EVK board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-FASTBOOT-flash-commands-for-QSPI-storage-for-iMX8M-Nano/m-p/1819596#M220661</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have generated the bootloader image for QSPI storage (32MB) for my iMX8M Nano EVK board using this command:&lt;BR /&gt;make SOC=iMX8MN flash_evk_flexspi&lt;/P&gt;&lt;P&gt;I got flash.bin in folder iMX8M/flash.bin. This image is build with IVT Header.&lt;/P&gt;&lt;P&gt;I want to download this image from host PC to target board using u-boot's fastboot.&lt;/P&gt;&lt;P&gt;But the operation is not successful and there is an error on device side and host side:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Device Side:&lt;/STRONG&gt;&lt;BR /&gt;u-boot=&amp;gt; fastboot usb 0&lt;BR /&gt;Starting download of 1440960 bytes&lt;BR /&gt;..........&lt;BR /&gt;downloading of 1440960 bytes finished&lt;BR /&gt;cannot get the partion info for fbmisc&lt;BR /&gt;fastboot_get_lock_stat: error in get mmc part&lt;BR /&gt;Not support flash command for current device 255&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Host Side:&lt;/STRONG&gt;&lt;BR /&gt;$ sudo fastboot flash bootloader iMX8M/flash.bin&lt;BR /&gt;target reported max download size of 1073741824 bytes&lt;BR /&gt;sending 'bootloader' (1407 KB)...&lt;BR /&gt;OKAY [ 0.346s]&lt;BR /&gt;writing 'bootloader'...&lt;BR /&gt;FAILED (remote: failed to flash device)&lt;BR /&gt;finished. total time: 0.360s&lt;BR /&gt;$&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;This procedure works well for SD or eMMC storage but not for QSPI storage.&lt;/P&gt;&lt;P&gt;Is fastboot not supported for QSPI NOR flash Storage ?&lt;/P&gt;&lt;P&gt;If there is any patch that needs to be applied in uboot-imx's code to make it work for QSPI storage, please share it.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Saurabh&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 13:55:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-FASTBOOT-flash-commands-for-QSPI-storage-for-iMX8M-Nano/m-p/1819596#M220661</guid>
      <dc:creator>skbansal222</dc:creator>
      <dc:date>2024-03-01T13:55:26Z</dc:date>
    </item>
    <item>
      <title>Re: U-Boot FASTBOOT flash commands for QSPI storage for iMX8M Nano EVK board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/U-Boot-FASTBOOT-flash-commands-for-QSPI-storage-for-iMX8M-Nano/m-p/1819855#M220684</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Yes, it is not supported by default, you may use fastboot and use uboot command to download uboot. Is the same procedure we have for UUU tool.&lt;BR /&gt;&lt;BR /&gt;&lt;A href="https://github.com/nxp-imx/mfgtools/blob/master/uuu/qspi_burn_loader.lst" target="_blank"&gt;https://github.com/nxp-imx/mfgtools/blob/master/uuu/qspi_burn_loader.lst&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 23:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/U-Boot-FASTBOOT-flash-commands-for-QSPI-storage-for-iMX8M-Nano/m-p/1819855#M220684</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2024-03-01T23:54:34Z</dc:date>
    </item>
  </channel>
</rss>