<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX 8M Quad 4GB LPDDR4 RAM in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1819188#M220621</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202673"&gt;@pengyong_zhang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;P&gt;After I have removed and created firmware environment again, I have checked imx8mq_evk.h content as follows.&lt;/P&gt;&lt;LI-CODE lang="c"&gt;#define CONFIG_SYS_SDRAM_BASE	0x40000000
#define PHYS_SDRAM				0x40000000
//#define PHYS_SDRAM_SIZE			0xC0000000 /* 3GB DDR */
#define PHYS_SDRAM_SIZE			0x100000000	/* 4 GB DDR */

#define CONFIG_MXC_UART_BASE		UART1_BASE_ADDR

#define CONFIG_SUPPORT_PASSING_ATAGS 1
#define CONFIG_SETUP_MEMORY_TAGS 1
#define CONFIG_CMDLINE_TAG 1
#define CONFIG_INITRD_TAG 1&lt;/LI-CODE&gt;&lt;P&gt;When content contains&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;#define CONFIG_SUPPORT_PASSING_ATAGS 1&lt;/STRONG&gt;&lt;/EM&gt;, I can boot up my target device and I can see log with &lt;EM&gt;&lt;STRONG&gt;DRAM: 4 GiB&lt;/STRONG&gt;&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;Again, thanks for you and NXP Teams help.&lt;/P&gt;</description>
    <pubDate>Fri, 01 Mar 2024 03:45:56 GMT</pubDate>
    <dc:creator>Alex_Chang_633</dc:creator>
    <dc:date>2024-03-01T03:45:56Z</dc:date>
    <item>
      <title>i.MX 8M Quad 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1818434#M220565</link>
      <description>&lt;P&gt;Hi Teams,&lt;/P&gt;&lt;P&gt;We tried to extend &lt;EM&gt;&lt;STRONG&gt;i.MX 8M Quad from 3 GB RAM to 4 GB RAM&lt;/STRONG&gt;&lt;/EM&gt;.&amp;nbsp;&lt;/P&gt;&lt;P&gt;(&lt;EM&gt;&lt;STRONG&gt;Windows 10 22H2&lt;/STRONG&gt;&lt;/EM&gt; with WSL2 &lt;STRONG&gt;&lt;EM&gt;Ubuntu 20.04 LTS&lt;/EM&gt;&lt;/STRONG&gt;, BSP Package is from NXP: &lt;EM&gt;&lt;STRONG&gt;W21H2-1-5-0-imx-windows-bsp.zip&lt;/STRONG&gt;&lt;/EM&gt;)&lt;/P&gt;&lt;P&gt;We have created *.ds by&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;MX8M_LPDDR4_RPA_v33.xlsx&lt;/STRONG&gt;&lt;/EM&gt;. We also ran &lt;EM&gt;&lt;STRONG&gt;NXP i.MX/Mscale DDR Tool 3.31&lt;/STRONG&gt;&lt;/EM&gt; with specific &lt;EM&gt;&lt;STRONG&gt;DDR Script&lt;/STRONG&gt;&lt;/EM&gt; and calibration&amp;nbsp;successful.&lt;/P&gt;&lt;P&gt;After that, we have updated:&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;uboot-imx/include/configs/imx8mq_evk.h&lt;/STRONG&gt;&lt;/EM&gt; as follows.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="c"&gt;#define CONFIG_SYS_SDRAM_BASE   0x40000000
#define PHYS_SDRAM              0x40000000
#define PHYS_SDRAM_SIZE			0xC0000000	/* 3GB DDR */
/* We append extend definition as follows */
#define PHYS_SDRAM_2			0x100000000
#define PHYS_SDRAM_2_SIZE		0x40000000	/* 1 GB */&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Then, we have replaced:&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;uboot-imx/board/freescale/imx8mq_evk/lpddr4_timing.c&lt;/STRONG&gt;&lt;/EM&gt; by the code that was generated by &lt;EM&gt;&lt;STRONG&gt;NXP i.MX/Mscale DDR Tool 3.31&lt;/STRONG&gt;&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;After we have deployed our new firmware to the target board, it will keep restarting.&lt;BR /&gt;But we can see the RAM was extended to 4 GB as follows.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;U-Boot SPL 2022.04-00001-gcbab410fa1-dirty (Feb 29 2024 - 14:54:06 +0800)
Can't find PMIC:PFUZE100
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3200MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0:  RNG instantiated
Normal Boot
Trying to boot from MMC2


U-Boot 2022.04-00001-gcbab410fa1-dirty (Feb 29 2024 - 14:54:06 +0800)

CPU:   i.MX8MQ rev2.1 1300 MHz (running at 800 MHz)
CPU:   Industrial temperature grade (-40C to 105C) at 30C
Reset cause: POR
Model: NXP i.MX8MQ EVK
DRAM:  4 GiB
setup_typec: tcpc init failed, err=-5
Core:  78 devices, 26 uclasses, devicetree: separate
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (1280 x 720)
        [0] display-controller@32e00000, video
        [1] hdmi@32c00000, display
In:    serial
Out:   serial
Err:   serial
SEC0:  RNG instantiated

 BuildInfo:
  - ATF 28ad156

switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Net:   Could not get PHY for FEC0: addr 0
Could not get PHY for FEC0: addr 0
No ethernet found.

Fastboot: Normal
Normal Boot
starting USB...
Bus usb@38100000: Failed to initialize board for imx8m USB
probe failed, error -5
Bus usb@38200000: Register 2000140 NbrPorts 2
Starting the controller
USB XHCI 1.10
scanning bus usb@38200000 for devices... unable to get device descriptor (error=-1)
6 USB Device(s) found
       scanning usb for storage devices... 0 Storage Device(s) found
## Loading kernel from FIT Image at 40480000 ...
   Using 'conf-1' configuration
   Verifying Hash Integrity ... OK
   Trying 'uefi' kernel subimage
     Description:  UEFI
     Created:      2024-02-29   6:56:03 UTC
     Type:         Kernel Image
     Compression:  gzip compressed
     Data Start:   0x404800a4
     Data Size:    841710 Bytes = 822 KiB
     Architecture: AArch64
     OS:           Linux
     Load Address: 0x50004000
     Entry Point:  0x50004000
     Hash algo:    sha256
     Hash value:   bf84fec8d0696216fcc80cd8c2206ad2d5dbac240fe26a3715e78f3fd1f5ed06
   Verifying Hash Integrity ... sha256+ OK
   Uncompressing Kernel Image
FDT and ATAGS support not compiled in

resetting ...&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, can you give us some advice about this question? Are we missing any steps? Or maybe there's something we're doing wrong.&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 07:23:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1818434#M220565</guid>
      <dc:creator>Alex_Chang_633</dc:creator>
      <dc:date>2024-02-29T07:23:15Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Quad 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1818538#M220577</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229604"&gt;@Alex_Chang_633&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please change the value of&amp;nbsp;&amp;nbsp;&lt;SPAN&gt;PHYS_SDRAM_SIZE = 0x1 0000 0000, And re-try your test.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;B.R&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 08:54:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1818538#M220577</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2024-02-29T08:54:18Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Quad 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1818583#M220579</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202673"&gt;@pengyong_zhang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for your quick reply.&lt;/P&gt;&lt;P&gt;We have changed&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;imx8mq_evk.h&lt;/STRONG&gt;&lt;/EM&gt; as follows.&lt;/P&gt;&lt;LI-CODE lang="c"&gt;#define CONFIG_SYS_SDRAM_BASE   0x40000000
#define PHYS_SDRAM              0x40000000
#define PHYS_SDRAM_SIZE			0x100000000	/* 4 GB DDR */&lt;/LI-CODE&gt;&lt;P&gt;But after we have deployed new firmware to our microSD card and boot from it, the target board has the same problem to keep restarting as follows.&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;U-Boot SPL 2022.04-00001-gcbab410fa1-dirty (Feb 29 2024 - 17:10:55 +0800)
Can't find PMIC:PFUZE100
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3200MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0:  RNG instantiated
Normal Boot
Trying to boot from MMC2


U-Boot 2022.04-00001-gcbab410fa1-dirty (Feb 29 2024 - 17:10:55 +0800)

CPU:   i.MX8MQ rev2.1 1300 MHz (running at 800 MHz)
CPU:   Industrial temperature grade (-40C to 105C) at 30C
Reset cause: POR
Model: NXP i.MX8MQ EVK
DRAM:  4 GiB
setup_typec: tcpc init failed, err=-5
Core:  78 devices, 26 uclasses, devicetree: separate
MMC:   FSL_SDHC: 0, FSL_SDHC: 1
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0 (1280 x 720)
        [0] display-controller@32e00000, video
        [1] hdmi@32c00000, display
In:    serial
Out:   serial
Err:   serial
SEC0:  RNG instantiated

 BuildInfo:
  - ATF 28ad156

switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Net:   Could not get PHY for FEC0: addr 0
Could not get PHY for FEC0: addr 0
No ethernet found.

Fastboot: Normal
Normal Boot
starting USB...
Bus usb@38100000: Failed to initialize board for imx8m USB
probe failed, error -5
Bus usb@38200000: Register 2000140 NbrPorts 2
Starting the controller
USB XHCI 1.10
scanning bus usb@38200000 for devices... 6 USB Device(s) found
       scanning usb for storage devices... 0 Storage Device(s) found
## Loading kernel from FIT Image at 40480000 ...
   Using 'conf-1' configuration
   Verifying Hash Integrity ... OK
   Trying 'uefi' kernel subimage
     Description:  UEFI
     Created:      2024-02-29   9:12:49 UTC
     Type:         Kernel Image
     Compression:  gzip compressed
     Data Start:   0x404800a4
     Data Size:    841710 Bytes = 822 KiB
     Architecture: AArch64
     OS:           Linux
     Load Address: 0x50004000
     Entry Point:  0x50004000
     Hash algo:    sha256
     Hash value:   5451f418158fc61aa3b4d94ef76195282652b15e2a4d42bbc0e6ae982c013069
   Verifying Hash Integrity ... sha256+ OK
   Uncompressing Kernel Image
FDT and ATAGS support not compiled in

resetting ...&lt;/LI-CODE&gt;&lt;P&gt;Thanks for you and NXP Teams support.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 09:18:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1818583#M220579</guid>
      <dc:creator>Alex_Chang_633</dc:creator>
      <dc:date>2024-02-29T09:18:59Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Quad 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1819090#M220611</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229604"&gt;@Alex_Chang_633&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;according this message in boot log:&lt;/P&gt;
&lt;PRE class="lia-code-sample  language-markup"&gt;&lt;CODE&gt;FDT and ATAGS support not compiled in&lt;/CODE&gt;&lt;/PRE&gt;
&lt;P&gt;&lt;SPAN&gt;it looks like than built uboot without&lt;/SPAN&gt;&lt;/P&gt;
&lt;DIV&gt;
&lt;DIV&gt;&lt;EM&gt;#define CONFIG_SUPPORT_PASSING_ATAGS 1.&lt;/EM&gt;&lt;/DIV&gt;
&lt;DIV&gt;&lt;SPAN&gt;This line should be added in to the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;EM&gt;include/configs/imx8mq_evk.h&lt;/EM&gt;&amp;nbsp;when the&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;&lt;EM&gt;patches/uboot-imx.patch is applied by running&lt;/EM&gt;&amp;nbsp;the ./Init.sh script.&lt;/SPAN&gt;&lt;/DIV&gt;
&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;DIV&gt;&lt;SPAN&gt;- Can you make sure please, that all the patches in the "patches" folder were correctly applied?&lt;BR /&gt;&lt;/SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pengyong_zhang_0-1709256567805.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/265917iB9E99975DBAEC932/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pengyong_zhang_0-1709256567805.png" alt="pengyong_zhang_0-1709256567805.png" /&gt;&lt;/span&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;- Are you able to build the firmware from the BSP for&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;i.MX 8M Quad EVK and boot with it to the Windows 10 IoT?&lt;/SPAN&gt;&lt;/P&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;P&gt;Best Regards&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 01:30:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1819090#M220611</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2024-03-01T01:30:35Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Quad 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1819137#M220616</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202673"&gt;@pengyong_zhang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your quick reply!&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT color="#0000FF"&gt;&lt;SPAN&gt;&amp;nbsp;Are you able to build the firmware from the BSP for&amp;nbsp;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;SPAN&gt;&lt;FONT color="#0000FF"&gt;i.MX 8M Quad EVK and boot with it to the Windows 10 IoT?&lt;/FONT&gt;&lt;BR /&gt;Yes, if I didn't modify&lt;EM&gt;&lt;STRONG&gt; #define&amp;nbsp;PHYS_SDRAM_SIZE&lt;/STRONG&gt;&lt;/EM&gt; value, I can run &lt;EM&gt;&lt;STRONG&gt;./buildme64.sh -b MX8M_EVK -t all -c&lt;/STRONG&gt;&lt;/EM&gt; and burn that firmware into microSD with Windows 10 IoT to boot up target device&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;&lt;FONT color="#0000FF"&gt;Can you make sure please, that all the patches in the "patches" folder were correctly applied?&lt;/FONT&gt;&lt;BR /&gt;I tried to repeat all procedures from the manual to prepare environment again. (&lt;EM&gt;&lt;STRONG&gt;i.MX Windows 10 IoT User’s Guide - 2.2 Building ARM64 Firmware&lt;/STRONG&gt;&lt;/EM&gt;)&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="nxp-win10-iot-bsp.01.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/265922i736C628818C84A0D/image-size/large?v=v2&amp;amp;px=999" role="button" title="nxp-win10-iot-bsp.01.png" alt="nxp-win10-iot-bsp.01.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I will try to rebuild firmware and test again and share my result here.&lt;/P&gt;&lt;P&gt;Thanks for you and NXP Teams help.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 02:37:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1819137#M220616</guid>
      <dc:creator>Alex_Chang_633</dc:creator>
      <dc:date>2024-03-01T02:37:01Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Quad 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1819151#M220617</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202673"&gt;@pengyong_zhang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;After I have created environment again (run &lt;EM&gt;&lt;STRONG&gt;./Init.sh&lt;/STRONG&gt;&lt;/EM&gt; without any error)&lt;/P&gt;&lt;P&gt;The situation is the same as follows. How do I make sure those patches have&amp;nbsp;&lt;SPAN&gt;applied correctly?&lt;/SPAN&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="nxp-win10-iot-bsp.02.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/265927iAB92F6751B1A1C74/image-size/large?v=v2&amp;amp;px=999" role="button" title="nxp-win10-iot-bsp.02.png" alt="nxp-win10-iot-bsp.02.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for you and NXP Team support.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 02:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1819151#M220617</guid>
      <dc:creator>Alex_Chang_633</dc:creator>
      <dc:date>2024-03-01T02:59:25Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Quad 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1819188#M220621</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202673"&gt;@pengyong_zhang&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;P&gt;After I have removed and created firmware environment again, I have checked imx8mq_evk.h content as follows.&lt;/P&gt;&lt;LI-CODE lang="c"&gt;#define CONFIG_SYS_SDRAM_BASE	0x40000000
#define PHYS_SDRAM				0x40000000
//#define PHYS_SDRAM_SIZE			0xC0000000 /* 3GB DDR */
#define PHYS_SDRAM_SIZE			0x100000000	/* 4 GB DDR */

#define CONFIG_MXC_UART_BASE		UART1_BASE_ADDR

#define CONFIG_SUPPORT_PASSING_ATAGS 1
#define CONFIG_SETUP_MEMORY_TAGS 1
#define CONFIG_CMDLINE_TAG 1
#define CONFIG_INITRD_TAG 1&lt;/LI-CODE&gt;&lt;P&gt;When content contains&amp;nbsp;&lt;EM&gt;&lt;STRONG&gt;#define CONFIG_SUPPORT_PASSING_ATAGS 1&lt;/STRONG&gt;&lt;/EM&gt;, I can boot up my target device and I can see log with &lt;EM&gt;&lt;STRONG&gt;DRAM: 4 GiB&lt;/STRONG&gt;&lt;/EM&gt;.&lt;/P&gt;&lt;P&gt;Again, thanks for you and NXP Teams help.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 03:45:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1819188#M220621</guid>
      <dc:creator>Alex_Chang_633</dc:creator>
      <dc:date>2024-03-01T03:45:56Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Quad 4GB LPDDR4 RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1819265#M220629</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229604"&gt;@Alex_Chang_633&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I'm glad to help you out, You are welcome.&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 06:01:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Quad-4GB-LPDDR4-RAM/m-p/1819265#M220629</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2024-03-01T06:01:08Z</dc:date>
    </item>
  </channel>
</rss>