<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Difference between i.MX8DXL and its Solo-Core-Variant in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-i-MX8DXL-and-its-Solo-Core-Variant/m-p/1818670#M220587</link>
    <description>&lt;P&gt;As I wrote, I have an already working board with an i.MX8DXL on it. Everything works fine. It is started be U-Boot and then loads the Linux-Kernel with the given Devicetree and even Debian runs smoothly with every peripherie on the Board.&lt;/P&gt;&lt;P&gt;Now, I only want to port it to an i.MX8SX (or SL? or SX? it reads: MIMX8SL1 CVNFZAB). I thought (perhaps my failure), that I could bring it up with my DXL-BSP. But that doesn't work. It does exactly - nothing.&lt;/P&gt;&lt;P&gt;So my question is: what is the difference between the two processors which prevent the Solo-Core from booting.&lt;/P&gt;</description>
    <pubDate>Thu, 29 Feb 2024 10:15:50 GMT</pubDate>
    <dc:creator>steffendoster</dc:creator>
    <dc:date>2024-02-29T10:15:50Z</dc:date>
    <item>
      <title>Difference between i.MX8DXL and its Solo-Core-Variant</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-i-MX8DXL-and-its-Solo-Core-Variant/m-p/1818523#M220576</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;I have a working custom i.MX8DXL-Board with 512MB RAM up and running. Everything looks fine. Now I wanted to use its little Solo-Core-Brother too.&lt;/P&gt;&lt;P&gt;I thought, it &amp;lt;&amp;lt;might&amp;gt;&amp;gt; be as easy as with the i.MX6DL and the i.MX6Solo, where the Dual-Core-U-Boot and -Devicetree is also suitable for the i.MX6Solo. (Linux was a little sad about not finding the second core, but booted with no problems)&lt;/P&gt;&lt;P&gt;But on i.MX8DXL this seems to not be the case.&lt;/P&gt;&lt;P&gt;Can anyone point me the direction what to check? Is it perhaps ATF or SCU? Is there a special firmware I have to use? (All I see is DXL-Firmware, for example: mx8&lt;STRONG&gt;dxl&lt;/STRONG&gt;b0-ahab-container.img)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/37066"&gt;@igorpadykov&lt;/a&gt;: Yes, I know you don't support this, and yes, I know where the documentation is.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 09:07:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-i-MX8DXL-and-its-Solo-Core-Variant/m-p/1818523#M220576</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2024-02-29T09:07:26Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between i.MX8DXL and its Solo-Core-Variant</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-i-MX8DXL-and-its-Solo-Core-Variant/m-p/1818625#M220584</link>
      <description>&lt;P&gt;not sure what you need check? do you need uboot image for imx6dl/6s?&amp;nbsp; or you need to know where is the location of uboot image after you build the board? if you mean build the imx6 uboot image, you can find the chapter 3 Porting U-Boot of enclosed file, imx6dl is not complicated as imx8dxl&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 09:44:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-i-MX8DXL-and-its-Solo-Core-Variant/m-p/1818625#M220584</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-02-29T09:44:48Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between i.MX8DXL and its Solo-Core-Variant</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-i-MX8DXL-and-its-Solo-Core-Variant/m-p/1818670#M220587</link>
      <description>&lt;P&gt;As I wrote, I have an already working board with an i.MX8DXL on it. Everything works fine. It is started be U-Boot and then loads the Linux-Kernel with the given Devicetree and even Debian runs smoothly with every peripherie on the Board.&lt;/P&gt;&lt;P&gt;Now, I only want to port it to an i.MX8SX (or SL? or SX? it reads: MIMX8SL1 CVNFZAB). I thought (perhaps my failure), that I could bring it up with my DXL-BSP. But that doesn't work. It does exactly - nothing.&lt;/P&gt;&lt;P&gt;So my question is: what is the difference between the two processors which prevent the Solo-Core from booting.&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 10:15:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-i-MX8DXL-and-its-Solo-Core-Variant/m-p/1818670#M220587</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2024-02-29T10:15:50Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between i.MX8DXL and its Solo-Core-Variant</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-i-MX8DXL-and-its-Solo-Core-Variant/m-p/1818680#M220588</link>
      <description>&lt;P&gt;I'm sorry, I replied to your post, but with the wrong "Reply"-Button.&lt;/P&gt;&lt;P&gt;I already know the Porting Guide, but only the i.MX8DXL is mentioned there. I don't see a i.MX8SXL/SL/SX or whatever.&lt;/P&gt;&lt;P&gt;So, i have a working&amp;nbsp;&lt;SPAN&gt;MIMX8DL1AVNFZAB, but the U-Boot doesn't work with&amp;nbsp;MIMX8SL1CVNFZAB.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 10:26:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-i-MX8DXL-and-its-Solo-Core-Variant/m-p/1818680#M220588</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2024-02-29T10:26:43Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between i.MX8DXL and its Solo-Core-Variant</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Difference-between-i-MX8DXL-and-its-Solo-Core-Variant/m-p/1820640#M220732</link>
      <description>&lt;P&gt;I GOT IT!&lt;/P&gt;&lt;P&gt;It was not an issue with the processor itself. It was a RAM misconfiguration:&lt;BR /&gt;I had the RAM Data-Lines in the &lt;SPAN&gt;RAM-Pin-Config&lt;/SPAN&gt; for the NXP-Eval-Board. But that is not our configuration, we have 0 to 0, 1 to 1 and so on.&lt;BR /&gt;Suprisingly the NXP-Configuration also worked for our Board, as long it had a 1GB RAM.But&lt;SPAN&gt;&amp;nbsp;with the change from DXL to SXL we also changed RAM from 1GB to 512MB, and the 512MB RAM didn't work with the wrong RAM-Config.&lt;BR /&gt;I corrected the RAM-Pin-Config and Tadaaaaa! It worked!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Mar 2024 14:50:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Difference-between-i-MX8DXL-and-its-Solo-Core-Variant/m-p/1820640#M220732</guid>
      <dc:creator>steffendoster</dc:creator>
      <dc:date>2024-03-04T14:50:39Z</dc:date>
    </item>
  </channel>
</rss>