<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [i.MX8MP] ISP: adding a new Sony 1080p sensor with ClearHDR technology. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1816928#M220499</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/23961"&gt;@artsiomstaliaro&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Have you got this imx662 sensor work?&lt;/P&gt;&lt;P&gt;I face exactly the same problem as you describe above. I have tried all possible settings in imx8mp ISP and none of them work.&lt;/P&gt;&lt;P&gt;When the ISP is configured to SENSOR_MODE_HDR_STITCH + SENSOR_STITCHING_DUAL_DCG_NOWAIT, or SENSOR_MODE_HDR_STITCH + SENSOR_STITCHING_L_AND_S, I got the camera show at 1fps with the frames roll over the screen. It seems that IMX8MP can not identify frame header code from sensor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 28 Feb 2024 01:26:16 GMT</pubDate>
    <dc:creator>TrinhVanKhai</dc:creator>
    <dc:date>2024-02-28T01:26:16Z</dc:date>
    <item>
      <title>[i.MX8MP] ISP: adding a new Sony 1080p sensor with ClearHDR technology.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1620458#M203108</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Im using&amp;nbsp;L5.15.71_2.2.0 Yocto package (with isp-imx-4.2.2.16.0).&lt;/P&gt;&lt;P&gt;I need to add a new Sony 1080p sensor with ClearHDR mode.&lt;/P&gt;&lt;P&gt;ClearHDR mode function description:&lt;BR /&gt;This function outputs 2 different gain data of same pixel. By combining these images, the image which is like high bit image or HDR image can be gotten. Clear HDR has the following two modes.&lt;BR /&gt;The lines for low and high gain line are alternately output after the Embedded data line.&lt;/P&gt;&lt;P&gt;in vvcam module driver there no option directly to enable ClearHDR mode, i see only 3 options:&lt;/P&gt;&lt;P&gt;SENSOR_MODE_LINEAR,&lt;BR /&gt;SENSOR_MODE_HDR_STITCH,&lt;BR /&gt;SENSOR_MODE_HDR_NATIVE,&lt;/P&gt;&lt;P&gt;I've tried&amp;nbsp;SENSOR_MODE_HDR_NATIVE - but i got a bit shifted picture.&lt;/P&gt;&lt;P&gt;What mode do i need to use?&lt;/P&gt;</description>
      <pubDate>Thu, 23 Mar 2023 04:31:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1620458#M203108</guid>
      <dc:creator>artsiomstaliaro</dc:creator>
      <dc:date>2023-03-23T04:31:34Z</dc:date>
    </item>
    <item>
      <title>Re: [i.MX8MP] ISP: adding a new Sony 1080p sensor with ClearHDR technology.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1622249#M203262</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/23961"&gt;@artsiomstaliaro&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;One can refer to&amp;nbsp;&lt;STRONG&gt;13.1.5.1 High-Dynamic Range (HDR)&lt;/STRONG&gt; in&amp;nbsp;i.MX 8M Plus Applications Processor Reference Manual&amp;nbsp;for HDR support.&lt;/P&gt;
&lt;P&gt;Please make sure that you have referred to&amp;nbsp;2.6.3 Native HDR Mode Porting in&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/iMX8MP_CAMERA_DISPLAY_GUIDE.pdf" target="_self"&gt;i.MX 8M Plus Camera and Display Guide&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 05:57:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1622249#M203262</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-03-27T05:57:20Z</dc:date>
    </item>
    <item>
      <title>Re: [i.MX8MP] ISP: adding a new Sony 1080p sensor with ClearHDR technology.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1622425#M203279</link>
      <description>&lt;P&gt;Thank you for pointing to the documentation. The documentation mentions only compressed modes for Native HDR, but my sensor doesn't use compressed mode but uses interleaved lines (1st line with High Gain, 2nd line with Low Gain).&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="artsiomstaliaro_1-1679906906284.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/216349i6E29668322C9A1A2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="artsiomstaliaro_1-1679906906284.png" alt="artsiomstaliaro_1-1679906906284.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;HG = High gain line, LG = low gain line.&lt;/P&gt;&lt;P&gt;Can you suggest the correct mode?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Mar 2023 08:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1622425#M203279</guid>
      <dc:creator>artsiomstaliaro</dc:creator>
      <dc:date>2023-03-27T08:49:50Z</dc:date>
    </item>
    <item>
      <title>Re: [i.MX8MP] ISP: adding a new Sony 1080p sensor with ClearHDR technology.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1623347#M203358</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/23961"&gt;@artsiomstaliaro&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;For&amp;nbsp;Native HDR mode, ISP Pipeline expects compressed HDR data.&lt;/P&gt;
&lt;P&gt;Please refer to&amp;nbsp;&lt;STRONG&gt;Figure 13-2. Native HDR&lt;/STRONG&gt; and &lt;STRONG&gt;Figure 13-3. DOL-HDR&lt;/STRONG&gt; in&amp;nbsp;MX 8M Plus Applications Processor Reference Manual for ISP Support in HDR mode.&lt;/P&gt;
&lt;P&gt;vvcam_mode_info_s structure values need to be set based on the camera sensor mode and output format supported.&lt;/P&gt;
&lt;P&gt;For Line-interleaved (staggered) HDR mode(uncompressed HDR data) SENSOR_MODE_HDR_STITCH&amp;nbsp; can be used and need to set .data_compress.enable = 0;&lt;/P&gt;
&lt;P&gt;Please refer to&amp;nbsp;&lt;STRONG&gt;2.6.2.2 Create Sensor V4L2 Driver in VVCAM&lt;/STRONG&gt; where&amp;nbsp;vvcam_mode_info_s has values for all the modes and output format supported in&amp;nbsp;pov2775 camera sensor.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Tue, 28 Mar 2023 12:19:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1623347#M203358</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-03-28T12:19:07Z</dc:date>
    </item>
    <item>
      <title>Re: [i.MX8MP] ISP: adding a new Sony 1080p sensor with ClearHDR technology.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1626323#M203566</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/201299"&gt;@Dhruvit&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;thank you for the suggestion. I did a test with 3 HDR modes sensors have:&lt;BR /&gt;&amp;nbsp;- ClearHDR: used&amp;nbsp;SENSOR_MODE_HDR_NATIVE + compress = 0. As a result, I got a shifted video, but it seems only a High Gain frame.&lt;/P&gt;&lt;P&gt;- DOL2-HDR: used&amp;nbsp;SENSOR_MODE_HDR_STITCH +&amp;nbsp;SENSOR_STITCHING_2DOL (also tried with&amp;nbsp;SENSOR_STITCHING_L_AND_S), video does not even starts.&lt;/P&gt;&lt;P&gt;- DOL3-HDR: used&amp;nbsp;SENSOR_MODE_HDR_STITCH +&amp;nbsp;SENSOR_STITCHING_3DOL , video does not even starts.&lt;/P&gt;&lt;P&gt;I'm using ISP version isp-imx-4.2.2.16.0 and in vvcam I found:&lt;/P&gt;&lt;P&gt;vvcam/isp/isp_hdr.c: commented out using "#if 0" settings for HDR stitching and so on.&lt;BR /&gt;I feel like there are some limitations with settings in ISP for handling this sensor's HDR formats.&amp;nbsp;&lt;BR /&gt;Maybe I should use new version of Linux Yocto with new version of ISP?&lt;/P&gt;</description>
      <pubDate>Fri, 31 Mar 2023 23:36:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1626323#M203566</guid>
      <dc:creator>artsiomstaliaro</dc:creator>
      <dc:date>2023-03-31T23:36:09Z</dc:date>
    </item>
    <item>
      <title>Re: [i.MX8MP] ISP: adding a new Sony 1080p sensor with ClearHDR technology.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1627701#M203716</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/23961"&gt;@artsiomstaliaro&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I hope you are doing well.&lt;/P&gt;
&lt;P&gt;These modes should be selected based on camera sensor used.&lt;/P&gt;
&lt;P&gt;Have you tried with&amp;nbsp;SENSOR_STITCHING_DUAL_DCG mode?&lt;/P&gt;
&lt;P&gt;Please refer to&amp;nbsp;&lt;STRONG&gt;13.1.5.1 High-Dynamic Range (HDR)&lt;/STRONG&gt;&amp;nbsp; in RM for supported modes in i.MX8MP.&lt;/P&gt;
&lt;P&gt;Please mention the camera sensor part number.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Maybe I should use new version of Linux Yocto with a new version of ISP?&lt;BR /&gt;[Ans]: One can refer to&lt;A href="https://www.nxp.com/docs/en/release-note/IMX_LINUX_RELEASE_NOTES.pdf" target="_self"&gt;&amp;nbsp;i.MX Linux Release Notes&lt;/A&gt;&amp;nbsp;for the latest ISP version and kernel changes as there are changes in the latest version of&amp;nbsp;&lt;A href="https://github.com/nxp-imx/isp-vvcam/blob/lf-6.1.y_1.0.0/vvcam/isp/isp_hdr.c" target="_self"&gt;isp-vvcam&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 04 Apr 2023 13:12:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1627701#M203716</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-04-04T13:12:10Z</dc:date>
    </item>
    <item>
      <title>Re: [i.MX8MP] ISP: adding a new Sony 1080p sensor with ClearHDR technology.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1632800#M204117</link>
      <description>Yes, I've tried SENSOR_STITCHING_DUAL_DCG without luck. Sensor is Sony IMX662</description>
      <pubDate>Thu, 13 Apr 2023 05:46:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1632800#M204117</guid>
      <dc:creator>artsiomstaliaro</dc:creator>
      <dc:date>2023-04-13T05:46:20Z</dc:date>
    </item>
    <item>
      <title>Re: [i.MX8MP] ISP: adding a new Sony 1080p sensor with ClearHDR technology.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1634702#M204314</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/23961"&gt;@artsiomstaliaro&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Customers have to set&amp;nbsp;&lt;STRONG&gt;vvcam_mode_info_s&lt;/STRONG&gt; based on the output format supported in the custom camera.&lt;/P&gt;
&lt;P&gt;One can set the stitching mode from the below table.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Screenshot from 2023-04-17 19-00-53.png" style="width: 746px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/219457i54378690D84EDA91/image-size/large?v=v2&amp;amp;px=999" role="button" title="Screenshot from 2023-04-17 19-00-53.png" alt="Screenshot from 2023-04-17 19-00-53.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Please make sure that you have configured other settings correctly as shown in&lt;STRONG&gt;&amp;nbsp;2.6.2.2 Create Sensor V4L2 Driver&lt;/STRONG&gt; in VVCAM in&amp;nbsp;i.MX 8M Plus Camera and Display Guide&lt;/P&gt;
&lt;P&gt;Please make sure that sensor registers are configured correctly for HDR mode.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please refer to&lt;A href="https://github.com/nxp-imx/isp-vvcam/tree/lf-5.15.y_2.0.0/vvcam/v4l2/sensor/ov2775" target="_self"&gt;&amp;nbsp;/vvcam/v4l2/sensor/ov2775/ov2775_mipi_v3.c&lt;/A&gt; in isp-vvcam where settings for&amp;nbsp;ov2775 sensor are given.&lt;/P&gt;
&lt;P&gt;Thanks &amp;amp; Regards,&lt;BR /&gt;Dhruvit Vasavada&lt;/P&gt;</description>
      <pubDate>Mon, 17 Apr 2023 13:41:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1634702#M204314</guid>
      <dc:creator>Dhruvit</dc:creator>
      <dc:date>2023-04-17T13:41:57Z</dc:date>
    </item>
    <item>
      <title>Re: [i.MX8MP] ISP: adding a new Sony 1080p sensor with ClearHDR technology.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1816928#M220499</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/23961"&gt;@artsiomstaliaro&lt;/a&gt; ,&lt;/P&gt;&lt;P&gt;Have you got this imx662 sensor work?&lt;/P&gt;&lt;P&gt;I face exactly the same problem as you describe above. I have tried all possible settings in imx8mp ISP and none of them work.&lt;/P&gt;&lt;P&gt;When the ISP is configured to SENSOR_MODE_HDR_STITCH + SENSOR_STITCHING_DUAL_DCG_NOWAIT, or SENSOR_MODE_HDR_STITCH + SENSOR_STITCHING_L_AND_S, I got the camera show at 1fps with the frames roll over the screen. It seems that IMX8MP can not identify frame header code from sensor.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Feb 2024 01:26:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1816928#M220499</guid>
      <dc:creator>TrinhVanKhai</dc:creator>
      <dc:date>2024-02-28T01:26:16Z</dc:date>
    </item>
    <item>
      <title>Re: [i.MX8MP] ISP: adding a new Sony 1080p sensor with ClearHDR technology.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1817998#M220548</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/190773"&gt;@TrinhVanKhai&lt;/a&gt;&amp;nbsp;yes it works.&lt;/P&gt;&lt;P&gt;Needs to tune frame parameters to fit into ISP requirements.&lt;/P&gt;</description>
      <pubDate>Wed, 28 Feb 2024 22:31:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-ISP-adding-a-new-Sony-1080p-sensor-with-ClearHDR/m-p/1817998#M220548</guid>
      <dc:creator>artsiomstaliaro</dc:creator>
      <dc:date>2024-02-28T22:31:11Z</dc:date>
    </item>
  </channel>
</rss>