<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8MP : Maximum baud rate for UART in Linux in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Maximum-baud-rate-for-UART-in-Linux/m-p/1815874#M220442</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;What is the maximum baudrate which can be achieved in UART on an imx8mp processor which is running Linux?&amp;nbsp; &amp;nbsp;I read in the MRM that up to 4.8Mbps can be achieved with increasing the module clock settings.&lt;/P&gt;&lt;P&gt;Has it been tried in Linux? If so, what changes would I have to make ? (device tree, defconfig etc)&lt;/P&gt;&lt;P&gt;If that baud rate is not achievable, what is the highest which can be achieved?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Mon, 26 Feb 2024 18:54:31 GMT</pubDate>
    <dc:creator>mahesh_hns</dc:creator>
    <dc:date>2024-02-26T18:54:31Z</dc:date>
    <item>
      <title>IMX8MP : Maximum baud rate for UART in Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Maximum-baud-rate-for-UART-in-Linux/m-p/1815874#M220442</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;What is the maximum baudrate which can be achieved in UART on an imx8mp processor which is running Linux?&amp;nbsp; &amp;nbsp;I read in the MRM that up to 4.8Mbps can be achieved with increasing the module clock settings.&lt;/P&gt;&lt;P&gt;Has it been tried in Linux? If so, what changes would I have to make ? (device tree, defconfig etc)&lt;/P&gt;&lt;P&gt;If that baud rate is not achievable, what is the highest which can be achieved?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 26 Feb 2024 18:54:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Maximum-baud-rate-for-UART-in-Linux/m-p/1815874#M220442</guid>
      <dc:creator>mahesh_hns</dc:creator>
      <dc:date>2024-02-26T18:54:31Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP : Maximum baud rate for UART in Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Maximum-baud-rate-for-UART-in-Linux/m-p/1818981#M220602</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;As said here:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/uart-support-with-up-to-4Mbps/m-p/1750756" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/uart-support-with-up-to-4Mbps/m-p/1750756&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;UART baudrate depende upon module clock of UART.&lt;BR /&gt;module_clock frequency must always be greater or equal to 16x the maximum baud rate.&lt;BR /&gt;&lt;BR /&gt;You may refer to the same thread for device tree configuration.&lt;BR /&gt;&lt;BR /&gt;Best reagrds/Saludos,&lt;BR /&gt;Aldo.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 19:43:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Maximum-baud-rate-for-UART-in-Linux/m-p/1818981#M220602</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2024-02-29T19:43:48Z</dc:date>
    </item>
  </channel>
</rss>