<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Problem facing when booting from emmc with imx8m plus evk board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-facing-when-booting-from-emmc-with-imx8m-plus-evk-board/m-p/1815360#M220398</link>
    <description>&lt;P&gt;Same problem here. Did you find a solution in the meantime?&lt;/P&gt;</description>
    <pubDate>Mon, 26 Feb 2024 08:30:46 GMT</pubDate>
    <dc:creator>uCChecker</dc:creator>
    <dc:date>2024-02-26T08:30:46Z</dc:date>
    <item>
      <title>Problem facing when booting from emmc with imx8m plus evk board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-facing-when-booting-from-emmc-with-imx8m-plus-evk-board/m-p/1284145#M174680</link>
      <description>&lt;P&gt;Hello, When I try to boot from emmc, the output goes on printing this repeatedly till I don't disconnect the board, I am unable to go beyond it. My board is imx8mplus evk board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;U-Boot SPL 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 4000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/P&gt;&lt;P&gt;U-Boot SPL 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 4000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/P&gt;&lt;P&gt;U-Boot SPL 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 4000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/P&gt;&lt;P&gt;U-Boot SPL 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 4000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/P&gt;&lt;P&gt;U-Boot SPL 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 4000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/P&gt;&lt;P&gt;U-Boot SPL 2020.04-5.10.9-1.0.0+gad7b74b415 (Mar 05 2021 - 07:05:56 +0000)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 4000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;image offset 0x8000, pagesize 0x200, ivt offset 0x0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 28 May 2021 12:08:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-facing-when-booting-from-emmc-with-imx8m-plus-evk-board/m-p/1284145#M174680</guid>
      <dc:creator>kenizgandhi</dc:creator>
      <dc:date>2021-05-28T12:08:21Z</dc:date>
    </item>
    <item>
      <title>Re: Problem facing when booting from emmc with imx8m plus evk board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-facing-when-booting-from-emmc-with-imx8m-plus-evk-board/m-p/1815360#M220398</link>
      <description>&lt;P&gt;Same problem here. Did you find a solution in the meantime?&lt;/P&gt;</description>
      <pubDate>Mon, 26 Feb 2024 08:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-facing-when-booting-from-emmc-with-imx8m-plus-evk-board/m-p/1815360#M220398</guid>
      <dc:creator>uCChecker</dc:creator>
      <dc:date>2024-02-26T08:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: Problem facing when booting from emmc with imx8m plus evk board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-facing-when-booting-from-emmc-with-imx8m-plus-evk-board/m-p/1815370#M220399</link>
      <description>&lt;P&gt;I think it is even worse...&lt;/P&gt;&lt;P&gt;U-Boot SPL 2020.04-5.4.70-2.3.2+g185bdaaaf5 (Apr 02 2021 - 17:52:17 +0000)&lt;BR /&gt;DDRINFO: start DRAM init&lt;BR /&gt;DDRINFO: DRAM rate 4000MTS&lt;BR /&gt;DDRINFO:ddrphy calibration done&lt;BR /&gt;DDRINFO: ddrmix config done&lt;BR /&gt;Normal Boot&lt;BR /&gt;Trying to boot from BOOTROM&lt;BR /&gt;image offset 0x0, pagesize 0x200, ivt offset 0x0&lt;BR /&gt;NOTICE: BL31: v2.2(release):imx_5.4.70_er5-4-g2a2678646&lt;BR /&gt;NOTICE: BL31: Built : 17:52:11, Apr 2 2021&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;U-Boot 2020.04-5.4.70-2.3.2+g185bdaaaf5 (Apr 02 2021 - 17:52:17 +0000)&lt;/P&gt;&lt;P&gt;CPU: i.MX8MP[8] rev1.1 1800 MHz (running at 1200 MHz)&lt;BR /&gt;CPU: Commercial temperature grade (0C to 95C) at 26C&lt;BR /&gt;Reset cause: POR&lt;BR /&gt;Model: NXP i.MX8MPlus LPDDR4 EVK board&lt;BR /&gt;DRAM: 6 GiB&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C2 0x50]&lt;BR /&gt;SNK.Power3.0 on CC2&lt;BR /&gt;PDO 0: type 0, 5000 mV, 3000 mA [E]&lt;BR /&gt;PDO 1: type 0, 9000 mV, 3000 mA []&lt;BR /&gt;PDO 2: type 0, 15000 mV, 3000 mA []&lt;BR /&gt;PDO 3: type 0, 20000 mV, 3000 mA []&lt;BR /&gt;Requesting PDO 3: 20000 mV, 2250 mA&lt;BR /&gt;Source accept request&lt;BR /&gt;PD source ready!&lt;BR /&gt;tcpc_pd_receive_message: Polling ALERT register, TCPC_ALERT_RX_STATUS bit failed, ret = -62&lt;BR /&gt;Power supply on USB2&lt;BR /&gt;TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]&lt;BR /&gt;MMC: FSL_SDHC: 1, FSL_SDHC: 2&lt;BR /&gt;Loading Environment from MMC... *** Warning - bad CRC, using default environment&lt;/P&gt;&lt;P&gt;[*]-Video Link 0Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;/P&gt;&lt;P&gt;[0] lcd-controller@32e80000, video&lt;BR /&gt;[1] mipi_dsi@32e60000, video_bridge&lt;BR /&gt;[2] adv7535@3d, panel&lt;BR /&gt;Can't find cec device id=0x3c&lt;BR /&gt;fail to probe panel device adv7535@3d&lt;BR /&gt;fail to get display timings&lt;BR /&gt;probe video device failed, ret -19&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;BuildInfo:&lt;BR /&gt;- ATF 2a26786&lt;BR /&gt;- U-Boot 2020.04-5.4.70-2.3.2+g185bdaaaf5&lt;/P&gt;&lt;P&gt;switch to partitions #0, OK&lt;BR /&gt;mmc2(part 0) is current device&lt;BR /&gt;flash target is MMC:2&lt;BR /&gt;Net:&lt;BR /&gt;Warning: ethernet@30be0000 using MAC address from ROM&lt;/P&gt;&lt;P&gt;Warning: ethernet@30bf0000 using MAC address from ROM&lt;BR /&gt;eth0: ethernet@30be0000, eth1: ethernet@30bf0000 [PRIME]&lt;BR /&gt;Fastboot: Normal&lt;BR /&gt;Normal Boot&lt;BR /&gt;Hit any key to stop autoboot: 2&lt;/P&gt;</description>
      <pubDate>Mon, 26 Feb 2024 08:41:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-facing-when-booting-from-emmc-with-imx8m-plus-evk-board/m-p/1815370#M220399</guid>
      <dc:creator>uCChecker</dc:creator>
      <dc:date>2024-02-26T08:41:45Z</dc:date>
    </item>
  </channel>
</rss>