<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: iMX8MPlus and PTN3366 Compatibility Issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MPlus-and-PTN3366-Compatibility-Issue/m-p/1814089#M220333</link>
    <description>&lt;P&gt;Hello, I hope you are doing well.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Am I correct in thinking that the iMX8MPlus is looking for a sink resistance to drive the signals? If so, how can I make this work with the PTN3366 which requires these series capacitors?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;It could be possible but it is strange since those capacitors are needed as is mentioned on datasheet.&lt;/P&gt;
&lt;P&gt;Did you try to change equalizer settings?&lt;/P&gt;
&lt;P&gt;Did you consider squelch function? Where IC only operates when input signal is above minimum threshold (VRX_DIFFp-p).&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Thu, 22 Feb 2024 20:29:20 GMT</pubDate>
    <dc:creator>JorgeCas</dc:creator>
    <dc:date>2024-02-22T20:29:20Z</dc:date>
    <item>
      <title>iMX8MPlus and PTN3366 Compatibility Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MPlus-and-PTN3366-Compatibility-Issue/m-p/1813137#M220271</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;I have designed a SBC project which uses the i.MX 8M Plus CPU. I need to convert the HDMI outputs to LVDS which required me to shift the HDMI outputs from 1.8V to 3.3V. To do this I chose the PTN3366.&lt;BR /&gt;&lt;BR /&gt;Now that I have received boards I am finding that there is an issue with the HDMI signals. The PTN3366 calls for AC coupling on all differential pair inputs as shown by the below screenshot from the datasheet:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="CSchutte_0-1708548983137.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/264365i8A73A0BA659C65B2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="CSchutte_0-1708548983137.png" alt="CSchutte_0-1708548983137.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;However, I am now finding that when I include AC coupling capacitors on my HDMI outputs from the iMX8, the HDMI signals disappear. If I short past the capacitors directly to the PTN3366 then the signals re-appear. It looks like the HDMI signals need some kind of sink resistance in order to be driven that the capacitor is blocking it from seeing.&lt;BR /&gt;&lt;BR /&gt;Am I correct in thinking that the iMX8MPlus is looking for a sink resistance to drive the signals? If so, how can I make this work with the PTN3366 which requires these series capacitors?&lt;BR /&gt;&lt;BR /&gt;Thanks!&lt;BR /&gt;Connor&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 21:00:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MPlus-and-PTN3366-Compatibility-Issue/m-p/1813137#M220271</guid>
      <dc:creator>CSchutte</dc:creator>
      <dc:date>2024-02-21T21:00:37Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MPlus and PTN3366 Compatibility Issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MPlus-and-PTN3366-Compatibility-Issue/m-p/1814089#M220333</link>
      <description>&lt;P&gt;Hello, I hope you are doing well.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;Am I correct in thinking that the iMX8MPlus is looking for a sink resistance to drive the signals? If so, how can I make this work with the PTN3366 which requires these series capacitors?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;It could be possible but it is strange since those capacitors are needed as is mentioned on datasheet.&lt;/P&gt;
&lt;P&gt;Did you try to change equalizer settings?&lt;/P&gt;
&lt;P&gt;Did you consider squelch function? Where IC only operates when input signal is above minimum threshold (VRX_DIFFp-p).&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Thu, 22 Feb 2024 20:29:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MPlus-and-PTN3366-Compatibility-Issue/m-p/1814089#M220333</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2024-02-22T20:29:20Z</dc:date>
    </item>
  </channel>
</rss>