<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: IMX8MP flash in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-flash/m-p/1814057#M220331</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228421"&gt;@Ajayvk&lt;/a&gt;!&lt;BR /&gt;Thank you for contacting NXP Support!&lt;BR /&gt;&lt;BR /&gt;Is not the same as the Download mode using the boot switches, but to flash the board using the uuu tool works fine.&lt;BR /&gt;&lt;BR /&gt;You can try to use the command and then use the command "uuu -lsusb" on your host and you can see the device.&lt;BR /&gt;&lt;BR /&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
    <pubDate>Thu, 22 Feb 2024 18:45:16 GMT</pubDate>
    <dc:creator>Chavira</dc:creator>
    <dc:date>2024-02-22T18:45:16Z</dc:date>
    <item>
      <title>IMX8MP flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-flash/m-p/1813672#M220308</link>
      <description>&lt;P&gt;does fastboot 0 command will make imx8mp board to usb serial download mode?&lt;/P&gt;</description>
      <pubDate>Thu, 22 Feb 2024 09:29:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-flash/m-p/1813672#M220308</guid>
      <dc:creator>Ajayvk</dc:creator>
      <dc:date>2024-02-22T09:29:36Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP flash</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-flash/m-p/1814057#M220331</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228421"&gt;@Ajayvk&lt;/a&gt;!&lt;BR /&gt;Thank you for contacting NXP Support!&lt;BR /&gt;&lt;BR /&gt;Is not the same as the Download mode using the boot switches, but to flash the board using the uuu tool works fine.&lt;BR /&gt;&lt;BR /&gt;You can try to use the command and then use the command "uuu -lsusb" on your host and you can see the device.&lt;BR /&gt;&lt;BR /&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Thu, 22 Feb 2024 18:45:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-flash/m-p/1814057#M220331</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2024-02-22T18:45:16Z</dc:date>
    </item>
  </channel>
</rss>