<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can not force IDR in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-not-force-IDR/m-p/1812938#M220257</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;When inserting a new IDR frame, drain your pipeline and reset.&amp;nbsp; There are only a few changes that are completely safe to do without a drain/reset.&amp;nbsp; Use mfxExtEncoderResetOption=ON to make sure that a new sequence is started.&lt;/P&gt;
&lt;P&gt;To ensure that mfxEncodeCtrl parameters correctly correspond to intended frame, allocate as many of them as surfaces used by the encoder.&amp;nbsp; &lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Wed, 21 Feb 2024 15:59:25 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-02-21T15:59:25Z</dc:date>
    <item>
      <title>Can not force IDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-not-force-IDR/m-p/1812072#M220185</link>
      <description>&lt;P&gt;Hello. I'm playing with encode_stream.c and test_enc_arm_elinux.c in imx-vpuwrap repository&lt;BR /&gt;&lt;BR /&gt;VPU wrapper version is&lt;BR /&gt;&lt;BR /&gt;vpu lib version : major.minor.rel=1.1.1&lt;BR /&gt;vpu fw version : major.minor.rel_rcode=1.1.1_r0&lt;BR /&gt;vpu wrapper version : major.minor.rel=3.0.0: VPUWRAPPER_ARM64_LINUX&lt;BR /&gt;&lt;BR /&gt;I'm receiving regular P-frame hen I'm trying to force IDR by setting field&amp;nbsp; sEncEncParam.nForceIPicture = 1.&lt;BR /&gt;&lt;BR /&gt;How do I correctly force IDR ?&lt;/P&gt;</description>
      <pubDate>Tue, 20 Feb 2024 16:48:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-not-force-IDR/m-p/1812072#M220185</guid>
      <dc:creator>marko1921</dc:creator>
      <dc:date>2024-02-20T16:48:32Z</dc:date>
    </item>
    <item>
      <title>Re: Can not force IDR</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-not-force-IDR/m-p/1812938#M220257</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;When inserting a new IDR frame, drain your pipeline and reset.&amp;nbsp; There are only a few changes that are completely safe to do without a drain/reset.&amp;nbsp; Use mfxExtEncoderResetOption=ON to make sure that a new sequence is started.&lt;/P&gt;
&lt;P&gt;To ensure that mfxEncodeCtrl parameters correctly correspond to intended frame, allocate as many of them as surfaces used by the encoder.&amp;nbsp; &lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 15:59:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-not-force-IDR/m-p/1812938#M220257</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-02-21T15:59:25Z</dc:date>
    </item>
  </channel>
</rss>