<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLibimxvpuapi and Docker Compatability</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Libimxvpuapi-and-Docker-Compatability/m-p/1812200#M220200</link>
    <description>&lt;P&gt;I'm working with an imx8mp and using a generated Yocto Image based off &lt;STRONG&gt;5.15-kirkstone&lt;/STRONG&gt; and a kernel version version &lt;STRONG&gt;5.15.52+g244c28a772f6&lt;/STRONG&gt;. I have successfully installed version 2.2.1 of libimxvpuapi library and am able to run the examples successfully. I'm working on a python3.10.7 application that is running inside a Docker container on the i.mx. I need to use the VPU library to decode an encoded H.264 video stream and post-processes it within my Python application. Ive looked into Python Bindings which should allow me to work with the library in python, but would the libimxvpuapi be compatible or configured to run within a Docker Container and successfully interact with the VPU?&lt;/P&gt;</description>
    <pubDate>Tue, 20 Feb 2024 21:52:59 GMT</pubDate>
    <dc:creator>hsuq7052</dc:creator>
    <dc:date>2024-02-20T21:52:59Z</dc:date>
    <item>
      <title>Libimxvpuapi and Docker Compatability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Libimxvpuapi-and-Docker-Compatability/m-p/1812200#M220200</link>
      <description>&lt;P&gt;I'm working with an imx8mp and using a generated Yocto Image based off &lt;STRONG&gt;5.15-kirkstone&lt;/STRONG&gt; and a kernel version version &lt;STRONG&gt;5.15.52+g244c28a772f6&lt;/STRONG&gt;. I have successfully installed version 2.2.1 of libimxvpuapi library and am able to run the examples successfully. I'm working on a python3.10.7 application that is running inside a Docker container on the i.mx. I need to use the VPU library to decode an encoded H.264 video stream and post-processes it within my Python application. Ive looked into Python Bindings which should allow me to work with the library in python, but would the libimxvpuapi be compatible or configured to run within a Docker Container and successfully interact with the VPU?&lt;/P&gt;</description>
      <pubDate>Tue, 20 Feb 2024 21:52:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Libimxvpuapi-and-Docker-Compatability/m-p/1812200#M220200</guid>
      <dc:creator>hsuq7052</dc:creator>
      <dc:date>2024-02-20T21:52:59Z</dc:date>
    </item>
    <item>
      <title>Re: Libimxvpuapi and Docker Compatability</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Libimxvpuapi-and-Docker-Compatability/m-p/1812947#M220259</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;You need at least the 6.1.55 to work with docker and libimxvpuapi.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/nxp-imx/imx-docker/blob/master/README.md" target="_blank"&gt;https://github.com/nxp-imx/imx-docker/blob/master/README.md&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 16:08:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Libimxvpuapi-and-Docker-Compatability/m-p/1812947#M220259</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-02-21T16:08:41Z</dc:date>
    </item>
  </channel>
</rss>