<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to generate EC Key pair in se050x based on user input in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-generate-EC-Key-pair-in-se050x-based-on-user-input/m-p/1811587#M220142</link>
    <description>&lt;P&gt;Hi Team,&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the nano-package code, we can see that an EC key pair is generated or a key is written to SE050 for the sign-in process. But for us the EC key pair must be generated inside SE050 based on user input, because the same key pair need be regenerated in case the device is lost.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please assist us in generating EC key pairs based on user input in SE050&amp;nbsp;&lt;SPAN&gt;and sign-in process.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sureshkumar R&lt;/P&gt;</description>
    <pubDate>Tue, 20 Feb 2024 07:55:06 GMT</pubDate>
    <dc:creator>krsuresh</dc:creator>
    <dc:date>2024-02-20T07:55:06Z</dc:date>
    <item>
      <title>How to generate EC Key pair in se050x based on user input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-generate-EC-Key-pair-in-se050x-based-on-user-input/m-p/1811587#M220142</link>
      <description>&lt;P&gt;Hi Team,&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the nano-package code, we can see that an EC key pair is generated or a key is written to SE050 for the sign-in process. But for us the EC key pair must be generated inside SE050 based on user input, because the same key pair need be regenerated in case the device is lost.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please assist us in generating EC key pairs based on user input in SE050&amp;nbsp;&lt;SPAN&gt;and sign-in process.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Sureshkumar R&lt;/P&gt;</description>
      <pubDate>Tue, 20 Feb 2024 07:55:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-generate-EC-Key-pair-in-se050x-based-on-user-input/m-p/1811587#M220142</guid>
      <dc:creator>krsuresh</dc:creator>
      <dc:date>2024-02-20T07:55:06Z</dc:date>
    </item>
    <item>
      <title>Re: How to generate EC Key pair in se050x based on user input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-generate-EC-Key-pair-in-se050x-based-on-user-input/m-p/1812359#M220214</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/210184"&gt;@krsuresh&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Such kind of tool is already there but not within the nano package, please download the full version of MW with the following link &lt;A href="https://www.nxp.com/webapp/Download?colCode=SE05x-PLUG-TRUST-MW&amp;amp;appType=license" target="_blank"&gt;https://www.nxp.com/webapp/Download?colCode=SE05x-PLUG-TRUST-MW&amp;amp;appType=license&lt;/A&gt; , and refer to the doc of simw-top/doc/cli-tool.html for details.&lt;/P&gt;
&lt;P&gt;This tool can work standalone as below or be used within some python script (Please refer to "simw-top\sss\plugin\openssl_provider\scripts\openssl_provisionEC.py" for details, alternatively please refer to simw-top/doc/pycli/Provisioning/readme.html for more details.).&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1708483954844.png" style="width: 615px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/264152i4BA9099AB3A2E8A5/image-dimensions/615x275?v=v2" width="615" height="275" role="button" title="Kan_Li_0-1708483954844.png" alt="Kan_Li_0-1708483954844.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope that helps,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 03:00:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-generate-EC-Key-pair-in-se050x-based-on-user-input/m-p/1812359#M220214</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2024-02-21T03:00:46Z</dc:date>
    </item>
    <item>
      <title>Re: How to generate EC Key pair in se050x based on user input</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-generate-EC-Key-pair-in-se050x-based-on-user-input/m-p/1812364#M220215</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/59276"&gt;@Kan_Li&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thanks for the quick response. I will check it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sureshkumar R&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 03:05:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-generate-EC-Key-pair-in-se050x-based-on-user-input/m-p/1812364#M220215</guid>
      <dc:creator>krsuresh</dc:creator>
      <dc:date>2024-02-21T03:05:04Z</dc:date>
    </item>
  </channel>
</rss>