<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How to enable MAIN clock and AUDIO PLL clock at same time in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-MAIN-clock-and-AUDIO-PLL-clock-at-same-time/m-p/1809351#M219999</link>
    <description>&lt;P&gt;I attached audio pll clock to ctimer0 (CLOCK_AttachClk(kAUDIO_PLL_to_CTIMER0)), but read an offset between ctimer0 and system clock. Output of ctimer0 is around 100 ms later than system clock.&lt;/P&gt;&lt;P&gt;If I attach main clock to ctimer0 (CLOCK_AttachClk(kMAIN_CLK_to_CTIMER0)), I read the same value from ctimer0 and system clock.&lt;/P&gt;&lt;P&gt;And because of the system design, I must use audio pll clock.&lt;/P&gt;&lt;P&gt;So is there a way to enable main clock and audio pll clock at the same time?&lt;/P&gt;&lt;P&gt;Or any other way to read similar value?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Thu, 15 Feb 2024 17:55:25 GMT</pubDate>
    <dc:creator>zenghuchen</dc:creator>
    <dc:date>2024-02-15T17:55:25Z</dc:date>
    <item>
      <title>How to enable MAIN clock and AUDIO PLL clock at same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-MAIN-clock-and-AUDIO-PLL-clock-at-same-time/m-p/1809351#M219999</link>
      <description>&lt;P&gt;I attached audio pll clock to ctimer0 (CLOCK_AttachClk(kAUDIO_PLL_to_CTIMER0)), but read an offset between ctimer0 and system clock. Output of ctimer0 is around 100 ms later than system clock.&lt;/P&gt;&lt;P&gt;If I attach main clock to ctimer0 (CLOCK_AttachClk(kMAIN_CLK_to_CTIMER0)), I read the same value from ctimer0 and system clock.&lt;/P&gt;&lt;P&gt;And because of the system design, I must use audio pll clock.&lt;/P&gt;&lt;P&gt;So is there a way to enable main clock and audio pll clock at the same time?&lt;/P&gt;&lt;P&gt;Or any other way to read similar value?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 15 Feb 2024 17:55:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-MAIN-clock-and-AUDIO-PLL-clock-at-same-time/m-p/1809351#M219999</guid>
      <dc:creator>zenghuchen</dc:creator>
      <dc:date>2024-02-15T17:55:25Z</dc:date>
    </item>
    <item>
      <title>Re: How to enable MAIN clock and AUDIO PLL clock at same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-MAIN-clock-and-AUDIO-PLL-clock-at-same-time/m-p/1810031#M220020</link>
      <description>&lt;P&gt;Hello, I hope you are doing well.&lt;/P&gt;
&lt;P&gt;Could you please share us which processor are you using?&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Feb 2024 14:51:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-MAIN-clock-and-AUDIO-PLL-clock-at-same-time/m-p/1810031#M220020</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2024-02-16T14:51:13Z</dc:date>
    </item>
    <item>
      <title>Re: How to enable MAIN clock and AUDIO PLL clock at same time</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-MAIN-clock-and-AUDIO-PLL-clock-at-same-time/m-p/1810059#M220025</link>
      <description>&lt;P&gt;Sure. I am using RT595.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Feb 2024 14:48:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/How-to-enable-MAIN-clock-and-AUDIO-PLL-clock-at-same-time/m-p/1810059#M220025</guid>
      <dc:creator>zenghuchen</dc:creator>
      <dc:date>2024-02-16T14:48:34Z</dc:date>
    </item>
  </channel>
</rss>