<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: External 24MHz Clock For i.MX8QM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/External-24MHz-Clock-For-i-MX8QM/m-p/1806648#M219957</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;Your initial reply was likely referencing a different chip. Thank you for correcting it so quickly.&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
    <pubDate>Wed, 14 Feb 2024 16:25:33 GMT</pubDate>
    <dc:creator>HWasti</dc:creator>
    <dc:date>2024-02-14T16:25:33Z</dc:date>
    <item>
      <title>External 24MHz Clock For i.MX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-24MHz-Clock-For-i-MX8QM/m-p/1805220#M219875</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The i.MX8QM datasheet, in Section 4.1.4 states: " &lt;SPAN&gt;The system clock input requires a crystal using the internal oscillator amplifier."&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Later in footnote 4 it states: "Fundamental frequency crystal with internal oscillator amplifier."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;In numerous places in this section, the document explicitly mentions crystal and external clock for RTC_XTALI, but never for XTALI. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;This implies that an external clock is not supported.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But later in Section 4.5.1 is titled "XTALI and&amp;nbsp;RTC_XTALI (Clock Inputs) DC Parameters" implying that external clock input is supported for XTALI.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;But in that section, it talks only about VIH and VIL for RTC_XTALI and is completely silent about high speed XTALI.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;1) For applications where the system will always be running and will never go into standby or shutdown modes, can an external 24MHz oscillator, connected to XTALI pin, be used?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;2) What are the voltage levels for this external clock input?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;hwasti&lt;/P&gt;</description>
      <pubDate>Mon, 12 Feb 2024 12:02:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-24MHz-Clock-For-i-MX8QM/m-p/1805220#M219875</guid>
      <dc:creator>HWasti</dc:creator>
      <dc:date>2024-02-12T12:02:03Z</dc:date>
    </item>
    <item>
      <title>Re: External 24MHz Clock For i.MX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-24MHz-Clock-For-i-MX8QM/m-p/1806635#M219953</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;1) For applications where the system will always be running and will never go into standby or shutdown modes, can an external 24MHz oscillator, connected to XTALI pin, be used?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Yes, the chip has two XTAL modules, 24MHz XTAL and 32KHz XTAL modules (All of these modules needs to use an external clock source, you could use our MEK as reference, &lt;STRONG&gt;you can use a crystal or oscillator&lt;/STRONG&gt;).&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;2) What are the voltage levels for this external clock input?&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;The 24 MHz oscillator can be driven with an external signal at the XTALI pin. The input voltage should never exceed the oscillator supply voltage (VDD_SCU_XTAL_1P8).&lt;/P&gt;
&lt;P&gt;The 32 KHz oscillator can be driven with an external signal at the RTC_XTALI pin. The input voltage should never exceed the oscillator supply voltage (VDD_SNVS_LDO_1P8_CAP).&lt;/P&gt;
&lt;P&gt;Here the specifications:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="JorgeCas_1-1707927137994.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/263158i4D6631BFC89A0B00/image-size/medium?v=v2&amp;amp;px=400" role="button" title="JorgeCas_1-1707927137994.png" alt="JorgeCas_1-1707927137994.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;JorgeCas_1-1707927137994.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;The processor can also accept a 1.8 V logic level clock. The specification input voltages for are the next:&lt;/P&gt;
&lt;P&gt;VIH between (0.5 X VDD +0.5v) and VDD&lt;/P&gt;
&lt;P&gt;VIL between 0 and (0.5 VDD - 0.5v)&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Feb 2024 16:14:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-24MHz-Clock-For-i-MX8QM/m-p/1806635#M219953</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2024-02-14T16:14:15Z</dc:date>
    </item>
    <item>
      <title>Re: External 24MHz Clock For i.MX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-24MHz-Clock-For-i-MX8QM/m-p/1806648#M219957</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;Your initial reply was likely referencing a different chip. Thank you for correcting it so quickly.&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Feb 2024 16:25:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-24MHz-Clock-For-i-MX8QM/m-p/1806648#M219957</guid>
      <dc:creator>HWasti</dc:creator>
      <dc:date>2024-02-14T16:25:33Z</dc:date>
    </item>
    <item>
      <title>Re: External 24MHz Clock For i.MX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-24MHz-Clock-For-i-MX8QM/m-p/1806660#M219958</link>
      <description>&lt;P&gt;Answer corrected, I apologize for the confusion.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Wed, 14 Feb 2024 16:13:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-24MHz-Clock-For-i-MX8QM/m-p/1806660#M219958</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2024-02-14T16:13:27Z</dc:date>
    </item>
  </channel>
</rss>