<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [IMX8DXL_OrangeBox] Unable to receive IPv4 in DHCP in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1806590#M219950</link>
    <description>&lt;P&gt;Thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt;&amp;nbsp;and&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/11276"&gt;@ebony_zhu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'll share the detailed steps&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/11276"&gt;@ebony_zhu&lt;/a&gt;&amp;nbsp;once I get the info from our engineering.&lt;/P&gt;&lt;P&gt;If it helps, we use this repository - &lt;A href="https://github.com/nxp-imx/meta-imx-orangebox" target="_blank"&gt;https://github.com/nxp-imx/meta-imx-orangebox&lt;/A&gt; to build the image&lt;/P&gt;&lt;P&gt;and flush to SD with the command &lt;EM&gt;unzstd -f --stdout ./sample.img | sudo dd of=dev/sda bs=1M conv=fsync&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I'll update accordingly.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 14 Feb 2024 14:19:36 GMT</pubDate>
    <dc:creator>imx8dxl-OB</dc:creator>
    <dc:date>2024-02-14T14:19:36Z</dc:date>
    <item>
      <title>[IMX8DXL_OrangeBox] Unable to receive IPv4 in DHCP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1805292#M219880</link>
      <description>&lt;P&gt;Good day!&lt;/P&gt;&lt;P&gt;We configured i.MX 8DXL EVK Rev B0 using an image based on repo&amp;nbsp;&lt;A href="https://github.com/nxp-imx/meta-imx-orangebox" target="_blank" rel="nofollow noopener noreferrer"&gt;https://github.com/nxp-imx/meta-imx-orangebox&lt;/A&gt;&lt;/P&gt;&lt;P&gt;However, the network interface failed via the board's ethernet interface (100Base-T) to receive IPv4 address via DHCP. It keeps on getting APIPA/private IP - 169.*.*.*.&lt;/P&gt;&lt;P&gt;&lt;EM&gt;# ifconfig&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;eth0 Link encap:Ethernet HWaddr DE:74:25:E9:86:C2&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;inet addr:169.254.202.241 Bcast:169.254.255.255 Mask:255.255.0.0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;inet6 addr: fe80::ca67:595:9aaa:6f6d/64 Scope:Link&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;RX packets:10 errors:0 dropped:0 overruns:0 frame:0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;TX packets:31 errors:0 dropped:0 overruns:0 carrier:0&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;collisions:0 txqueuelen:1000&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;RX bytes:3780 (3.6 KiB) TX bytes:3002 (2.9 KiB)&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;Interrupt:80&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Tried to update/add static IP for etho on &lt;EM&gt;/etc/network/interfaces&amp;nbsp;&lt;/EM&gt;but still receives the APIPA IP.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;The LAN we are using is verified to work properly either direct on the router or using another switch.&lt;/P&gt;&lt;P&gt;The network devices are able to issue DHCP IPs and connect to the internet.&lt;/P&gt;&lt;P&gt;How can we force the DHCP/IPv4 to the board?&lt;/P&gt;&lt;P&gt;Anything we possibly missed on the config.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you in advance for kind help.&lt;/P&gt;</description>
      <pubDate>Mon, 12 Feb 2024 14:27:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1805292#M219880</guid>
      <dc:creator>imx8dxl-OB</dc:creator>
      <dc:date>2024-02-12T14:27:24Z</dc:date>
    </item>
    <item>
      <title>Re: [IMX8DXL_OrangeBox] Unable to receive IPv4 in DHCP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1805528#M219895</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;What is the branch you built BSP with?&lt;/P&gt;
&lt;P&gt;Did you say that you have tried other routers?&lt;/P&gt;
&lt;P&gt;The most likely situation is a firewall setting on the router side that cannot answer/listen to the board, followed by there are not IP addresses available.&lt;/P&gt;
&lt;P&gt;If this none of this has helped, I'd try to &lt;A href="https://askubuntu.com/questions/912020/arp-is-displaying-weird-ip-addresses-in-the-169-range" target="_self"&gt;perform this&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 12 Feb 2024 22:23:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1805528#M219895</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-02-12T22:23:45Z</dc:date>
    </item>
    <item>
      <title>Re: [IMX8DXL_OrangeBox] Unable to receive IPv4 in DHCP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1805952#M219921</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your response.&lt;/P&gt;&lt;P&gt;We used this BSP 6.1.36-2.1.0.&lt;/P&gt;&lt;P&gt;Yes, tried other router also. The network setup/devices we're using works with the other NXP i.MX8 board that we setup recently (using different repo&amp;nbsp;&lt;SPAN&gt;&lt;SPAN class=""&gt;i.MX Linux Yocto Project BSP 6.1.22_2.0.0 Release &lt;A title="https://github.com/nxp-imx/meta-imx" href="https://github.com/nxp-imx/meta-imx" target="_blank" rel="noreferrer noopener"&gt;https://github.com/nxp-imx/meta-imx&lt;/A&gt;)&lt;/SPAN&gt;&lt;/SPAN&gt; - the i.MX 8XLite EVK and able to get an IP via DHCP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Unfortunately, flushing the arp from the new box -&amp;nbsp;i.MX 8DXL EVK Rev B0 still unable to get an IP.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Tue, 13 Feb 2024 16:00:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1805952#M219921</guid>
      <dc:creator>imx8dxl-OB</dc:creator>
      <dc:date>2024-02-13T16:00:22Z</dc:date>
    </item>
    <item>
      <title>Re: [IMX8DXL_OrangeBox] Unable to receive IPv4 in DHCP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1806081#M219925</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Now we're sure that's a configuration for orangebox image that may be missing but I can't provide further information due to orangebox is an internal product.&lt;/P&gt;
&lt;P&gt;Please contact your sales person for this matter.&lt;/P&gt;
&lt;P&gt;Thank you!&lt;/P&gt;</description>
      <pubDate>Tue, 13 Feb 2024 19:02:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1806081#M219925</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-02-13T19:02:14Z</dc:date>
    </item>
    <item>
      <title>Re: [IMX8DXL_OrangeBox] Unable to receive IPv4 in DHCP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1806174#M219929</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227510"&gt;@imx8dxl-OB&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please share the detailed steps of how you configurated the Yocto BSP and compiled the image.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ebony&lt;/P&gt;</description>
      <pubDate>Tue, 13 Feb 2024 22:36:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1806174#M219929</guid>
      <dc:creator>ebony_zhu</dc:creator>
      <dc:date>2024-02-13T22:36:17Z</dc:date>
    </item>
    <item>
      <title>Re: [IMX8DXL_OrangeBox] Unable to receive IPv4 in DHCP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1806590#M219950</link>
      <description>&lt;P&gt;Thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206442"&gt;@JosephAtNXP&lt;/a&gt;&amp;nbsp;and&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/11276"&gt;@ebony_zhu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'll share the detailed steps&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/11276"&gt;@ebony_zhu&lt;/a&gt;&amp;nbsp;once I get the info from our engineering.&lt;/P&gt;&lt;P&gt;If it helps, we use this repository - &lt;A href="https://github.com/nxp-imx/meta-imx-orangebox" target="_blank"&gt;https://github.com/nxp-imx/meta-imx-orangebox&lt;/A&gt; to build the image&lt;/P&gt;&lt;P&gt;and flush to SD with the command &lt;EM&gt;unzstd -f --stdout ./sample.img | sudo dd of=dev/sda bs=1M conv=fsync&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;I'll update accordingly.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Feb 2024 14:19:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1806590#M219950</guid>
      <dc:creator>imx8dxl-OB</dc:creator>
      <dc:date>2024-02-14T14:19:36Z</dc:date>
    </item>
    <item>
      <title>Re: [IMX8DXL_OrangeBox] Unable to receive IPv4 in DHCP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1806796#M219965</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227510"&gt;@imx8dxl-OB&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes please share your steps. I'm sharing my steps here as I built the image and tested DHCP, and it worked fine:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;$&amp;nbsp;repo init -u &lt;A href="https://github.com/nxp-imx/imx-manifest" target="_blank"&gt;https://github.com/nxp-imx/imx-manifest&lt;/A&gt; -b imx-linux-mickledore -m imx-6.1.36-2.1.0_orangebox.xml&lt;/P&gt;&lt;P&gt;$&amp;nbsp;repo sync&lt;/P&gt;&lt;P&gt;$ source ./sources/meta-imx-orangebox/tools/setup.sh bld-orangebox&lt;/P&gt;&lt;P&gt;$ bitbake imx-image-core&lt;/P&gt;&lt;P&gt;Then program the generated&amp;nbsp;imx-boot-imx8dxl-orangebox-sd.bin-flash_spl and&amp;nbsp;imx8dxl-orangebox/imx-image-core-imx8dxl-orangebox.wic.zst to eMMC or SD&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ebony&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Feb 2024 20:21:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1806796#M219965</guid>
      <dc:creator>ebony_zhu</dc:creator>
      <dc:date>2024-02-14T20:21:31Z</dc:date>
    </item>
    <item>
      <title>Re: [IMX8DXL_OrangeBox] Unable to receive IPv4 in DHCP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1809458#M220001</link>
      <description>&lt;P&gt;Will do share and thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/11276"&gt;@ebony_zhu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One thing to take note and was observed is that using the default image (boots via emmc) that comes with the box have the same behavior of unable to get IP and just have the private/APIPA IP.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Setting static using&amp;nbsp;&lt;SPAN&gt;&lt;SPAN class=""&gt;/etc/network/interface results also to private/APIPA IP.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;</description>
      <pubDate>Thu, 15 Feb 2024 19:45:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1809458#M220001</guid>
      <dc:creator>imx8dxl-OB</dc:creator>
      <dc:date>2024-02-15T19:45:13Z</dc:date>
    </item>
    <item>
      <title>Re: [IMX8DXL_OrangeBox] Unable to receive IPv4 in DHCP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1810065#M220026</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/11276"&gt;@ebony_zhu&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;We tried the steps you shared and results to an error.&lt;/P&gt;&lt;P&gt;Kindly see attached log file.&lt;/P&gt;&lt;P&gt;Is it possible to provide an image to us? Also, is it feasible to do diagnostic on the board specifically&lt;/P&gt;&lt;P&gt;the ethernet/network interface?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Feb 2024 14:51:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1810065#M220026</guid>
      <dc:creator>imx8dxl-OB</dc:creator>
      <dc:date>2024-02-16T14:51:26Z</dc:date>
    </item>
    <item>
      <title>Re: [IMX8DXL_OrangeBox] Unable to receive IPv4 in DHCP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1812110#M220191</link>
      <description>&lt;P&gt;Many thanks&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/11276"&gt;@ebony_zhu&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;DHCP/IP works now on the box using the image shared.&lt;/P&gt;&lt;P&gt;Programmed it to eMMC as advised.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Feb 2024 17:58:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1812110#M220191</guid>
      <dc:creator>imx8dxl-OB</dc:creator>
      <dc:date>2024-02-20T17:58:56Z</dc:date>
    </item>
    <item>
      <title>Re: [IMX8DXL_OrangeBox] Unable to receive IPv4 in DHCP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1813174#M220274</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/227510"&gt;@imx8dxl-OB&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The supported Linux host distributions are:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Ubuntu 20.04 (LTS)&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Ubuntu 22.04 (LTS)&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Fedora 38&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;CentOS Stream 8&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Debian GNU/Linux 11 (Bullseye)&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Debian GNU/Linux 12 (Bookworm)&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;OpenSUSE Leap 15.4&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;AlmaLinux 8&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;AlmaLinux 9&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Rocky 9&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;If your host is not one of those, please compile the BSP with docker:&amp;nbsp;&lt;A href="https://github.com/nxp-imx/imx-docker" target="_blank" rel="noopener"&gt;https://github.com/nxp-imx/imx-docker&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ebony&lt;/P&gt;</description>
      <pubDate>Wed, 21 Feb 2024 22:21:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8DXL-OrangeBox-Unable-to-receive-IPv4-in-DHCP/m-p/1813174#M220274</guid>
      <dc:creator>ebony_zhu</dc:creator>
      <dc:date>2024-02-21T22:21:34Z</dc:date>
    </item>
  </channel>
</rss>