<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processorsのトピックissue on CAN communication while enabling RT PREEMPT  in Linux</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/issue-on-CAN-communication-while-enabling-RT-PREEMPT-in-Linux/m-p/1802315#M219689</link>
    <description>&lt;P&gt;Hai NXP team&lt;/P&gt;&lt;P&gt;We are presently using the RTC PCF85263A with an iMX6ULL processor, running Linux 5.15.52 on Yocto 4.0. Additionally,&lt;/P&gt;&lt;P&gt;I have added this RT-Patch to my Linux kernel even though it is not the same version as my Linux kernel:&lt;/P&gt;&lt;P&gt;&lt;A href="https://mirrors.edge.kernel.org/pub/linux/kernel/projects/rt/5.15/older/patch-5.15.55-rt48.patch.gz" target="_blank"&gt;https://mirrors.edge.kernel.org/pub/linux/kernel/projects/rt/5.15/older/patch-5.15.55-rt48.patch.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Additionally, I have enabled the CONFIG_PREEMPT_RT in the kernel. Before enabling this, every interface was working perfectly. However, after enabling it, I can't send or receive CAN data. Is there anything I need to change or am I missing out on something? Please let me know.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Akash&lt;/P&gt;</description>
    <pubDate>Tue, 06 Feb 2024 05:04:45 GMT</pubDate>
    <dc:creator>AkashL_</dc:creator>
    <dc:date>2024-02-06T05:04:45Z</dc:date>
    <item>
      <title>issue on CAN communication while enabling RT PREEMPT  in Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/issue-on-CAN-communication-while-enabling-RT-PREEMPT-in-Linux/m-p/1802315#M219689</link>
      <description>&lt;P&gt;Hai NXP team&lt;/P&gt;&lt;P&gt;We are presently using the RTC PCF85263A with an iMX6ULL processor, running Linux 5.15.52 on Yocto 4.0. Additionally,&lt;/P&gt;&lt;P&gt;I have added this RT-Patch to my Linux kernel even though it is not the same version as my Linux kernel:&lt;/P&gt;&lt;P&gt;&lt;A href="https://mirrors.edge.kernel.org/pub/linux/kernel/projects/rt/5.15/older/patch-5.15.55-rt48.patch.gz" target="_blank"&gt;https://mirrors.edge.kernel.org/pub/linux/kernel/projects/rt/5.15/older/patch-5.15.55-rt48.patch.gz&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Additionally, I have enabled the CONFIG_PREEMPT_RT in the kernel. Before enabling this, every interface was working perfectly. However, after enabling it, I can't send or receive CAN data. Is there anything I need to change or am I missing out on something? Please let me know.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Akash&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 05:04:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/issue-on-CAN-communication-while-enabling-RT-PREEMPT-in-Linux/m-p/1802315#M219689</guid>
      <dc:creator>AkashL_</dc:creator>
      <dc:date>2024-02-06T05:04:45Z</dc:date>
    </item>
    <item>
      <title>Re: issue on CAN communication while enabling RT PREEMPT  in Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/issue-on-CAN-communication-while-enabling-RT-PREEMPT-in-Linux/m-p/1802917#M219726</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Unfortunately I cannot open your patch file, could you share it here?&lt;BR /&gt;Also, please make sure that you have ported your patch correctly for the kernel version you're using.&lt;/P&gt;
&lt;P&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 19:27:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/issue-on-CAN-communication-while-enabling-RT-PREEMPT-in-Linux/m-p/1802917#M219726</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2024-02-06T19:27:37Z</dc:date>
    </item>
    <item>
      <title>Re: issue on CAN communication while enabling RT PREEMPT  in Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/issue-on-CAN-communication-while-enabling-RT-PREEMPT-in-Linux/m-p/1803197#M219743</link>
      <description>&lt;P&gt;hello&amp;nbsp;AldoG,&lt;BR /&gt;As I mentioned earlier, we are using Linux version 5.15.52. However, I couldn't find the exact kernel version for the Real-Time (RT) Patch. So, we applied the patch for version 5.15.54, which I have attached since versions 5.15.52, 5.15.53, and 5.15.54 were not available.&lt;/P&gt;&lt;P&gt;I successfully added the patch to my kernel, except for two files in the kernel source. I manually added these two files, but they were not included in the patch due to a line mismatch.&lt;/P&gt;&lt;P&gt;It's important to mention that in this patch, CONFIG_PREEMPT_RT is not enabled, but CONFIG_PREEMPT is enabled. after that we enable&amp;nbsp;Fully Preemptible Kernel (CONFIG_PREEMPT_RT)&lt;/P&gt;&lt;DIV class=""&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 07 Feb 2024 07:31:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/issue-on-CAN-communication-while-enabling-RT-PREEMPT-in-Linux/m-p/1803197#M219743</guid>
      <dc:creator>AkashL_</dc:creator>
      <dc:date>2024-02-07T07:31:20Z</dc:date>
    </item>
  </channel>
</rss>