<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Timestamping Rising Edge Using Timer/PWM Module with iMX93</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Timestamping-Rising-Edge-Using-Timer-PWM-Module-with-iMX93/m-p/1802186#M219673</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;Actually, TPM is a HW unit that has the input capture mode which is used in high precision time record and there is an example that can get you started with the module under Cortex-M SDK.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_self"&gt;Please build the i.MX 93 SDK&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;The example is under &lt;EM&gt;SDK_2_14_2_MCIMX93-EVK.zip\boards\mcimx93evk\driver_examples\tpm\input_capture&lt;/EM&gt;.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Tue, 06 Feb 2024 00:16:45 GMT</pubDate>
    <dc:creator>JosephAtNXP</dc:creator>
    <dc:date>2024-02-06T00:16:45Z</dc:date>
    <item>
      <title>Timestamping Rising Edge Using Timer/PWM Module with iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Timestamping-Rising-Edge-Using-Timer-PWM-Module-with-iMX93/m-p/1801428#M219616</link>
      <description>&lt;P&gt;Dear NXP Support Team,&lt;/P&gt;&lt;P&gt;I am currently working on a project that involves synchronizing two sensors connected to the iMX93 processor. As part of this design, I need to capture the timestamp of a rising edge on one of the system-on-modules (SoM) inputs. It is crucial to perform this timestamping in hardware to avoid potential delays introduced by software-based solutions.&lt;/P&gt;&lt;P&gt;Upon reviewing Chapter 67 of NXP's iMX93 Reference Manual (IMX93RM), I noted that the Timer/PWM module is capable of performing input capture, which seems to align with my requirements. I would greatly appreciate your assistance in understanding how to utilize the Timer/PWM Module to timestamp a rising edge on the iMX93 Evaluation Kit. Specifically, if there are any application notes, reference implementations, demo code, relevant kernel module code, documentation, or tutorials available for using the Timer/PWM module, it would be immensely valuable to my current development efforts.&lt;/P&gt;&lt;P&gt;Thank you for your attention to this request, and I look forward to your assistance.&lt;/P&gt;&lt;P&gt;Sincerely,YE&lt;/P&gt;</description>
      <pubDate>Sun, 04 Feb 2024 12:29:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Timestamping-Rising-Edge-Using-Timer-PWM-Module-with-iMX93/m-p/1801428#M219616</guid>
      <dc:creator>yaen</dc:creator>
      <dc:date>2024-02-04T12:29:02Z</dc:date>
    </item>
    <item>
      <title>Re: Timestamping Rising Edge Using Timer/PWM Module with iMX93</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Timestamping-Rising-Edge-Using-Timer-PWM-Module-with-iMX93/m-p/1802186#M219673</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;Actually, TPM is a HW unit that has the input capture mode which is used in high precision time record and there is an example that can get you started with the module under Cortex-M SDK.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://mcuxpresso.nxp.com/en/welcome" target="_self"&gt;Please build the i.MX 93 SDK&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;The example is under &lt;EM&gt;SDK_2_14_2_MCIMX93-EVK.zip\boards\mcimx93evk\driver_examples\tpm\input_capture&lt;/EM&gt;.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 06 Feb 2024 00:16:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Timestamping-Rising-Edge-Using-Timer-PWM-Module-with-iMX93/m-p/1802186#M219673</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2024-02-06T00:16:45Z</dc:date>
    </item>
  </channel>
</rss>