<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: vpu encode H264 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/vpu-encode-H264/m-p/247917#M21960</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don´t know if it´s your case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sometime ago I had exactly the same error, but using gstreamer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem was that I was using "default" fps value to configure the camera, it was fps=15. And I was using the "default" fps value for the encoder, it was fps=30&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So it resulted in a wrong video.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you give this a try?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you share your command line?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Apr 2013 18:52:51 GMT</pubDate>
    <dc:creator>daiane_angolini</dc:creator>
    <dc:date>2013-04-24T18:52:51Z</dc:date>
    <item>
      <title>vpu encode H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vpu-encode-H264/m-p/247916#M21959</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I used the mxc_vpu_test to encode the video which captured from the camera, after sereral seconds captured, the encoded file generated, when I played the video, I find the play speed is a little fast, anyone can give me some advice to modify the code?&lt;/P&gt;&lt;P&gt;Thanks anyway!&lt;/P&gt;&lt;P&gt;Attachment file is the file generated.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-336135"&gt;out.h264.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Apr 2013 02:30:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vpu-encode-H264/m-p/247916#M21959</guid>
      <dc:creator>JayZhang</dc:creator>
      <dc:date>2013-04-02T02:30:04Z</dc:date>
    </item>
    <item>
      <title>Re: vpu encode H264</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/vpu-encode-H264/m-p/247917#M21960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don´t know if it´s your case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sometime ago I had exactly the same error, but using gstreamer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem was that I was using "default" fps value to configure the camera, it was fps=15. And I was using the "default" fps value for the encoder, it was fps=30&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So it resulted in a wrong video.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you give this a try?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you share your command line?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Apr 2013 18:52:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/vpu-encode-H264/m-p/247917#M21960</guid>
      <dc:creator>daiane_angolini</dc:creator>
      <dc:date>2013-04-24T18:52:51Z</dc:date>
    </item>
  </channel>
</rss>