<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SPI Slave Mode in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPI-Slave-Mode/m-p/1801083#M219588</link>
    <description>&lt;P&gt;Is there a driver, example or a user space application that configure the SPI module within imx8mn in slave mode? Thx!&lt;/P&gt;</description>
    <pubDate>Fri, 02 Feb 2024 19:55:34 GMT</pubDate>
    <dc:creator>moose</dc:creator>
    <dc:date>2024-02-02T19:55:34Z</dc:date>
    <item>
      <title>SPI Slave Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-Slave-Mode/m-p/1801083#M219588</link>
      <description>&lt;P&gt;Is there a driver, example or a user space application that configure the SPI module within imx8mn in slave mode? Thx!&lt;/P&gt;</description>
      <pubDate>Fri, 02 Feb 2024 19:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-Slave-Mode/m-p/1801083#M219588</guid>
      <dc:creator>moose</dc:creator>
      <dc:date>2024-02-02T19:55:34Z</dc:date>
    </item>
    <item>
      <title>Re: SPI Slave Mode</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPI-Slave-Mode/m-p/1801162#M219595</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196789"&gt;@moose&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can refer to&amp;nbsp;&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm/boot/dts/imx6ul-14x14-evk-ecspi-slave.dts" target="_self"&gt;arch/arm/boot/dts/imx6ul-14x14-evk-ecspi-slave.dts&lt;/A&gt;&amp;nbsp;and&amp;nbsp;&lt;A href="https://github.com/nxp-imx/linux-imx/blob/lf-6.1.y/arch/arm/boot/dts/imx6ul-14x14-evk-ecspi.dts" target="_self"&gt;arch/arm/boot/dts/imx6ul-14x14-evk-ecspi.dts&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Make sure not to use “cs-gpios” in dts.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You should use&amp;nbsp;should use “MX8MM_IOMUXC_ECSPI2_SS0_ECSPI2_SS0” instead of “MX8MM_IOMUXC_ECSPI2_SS0_GPIO5_IO13”.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Sat, 03 Feb 2024 00:58:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPI-Slave-Mode/m-p/1801162#M219595</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2024-02-03T00:58:23Z</dc:date>
    </item>
  </channel>
</rss>