<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Cannot check DEP/NX flag in imx6</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-check-DEP-NX-flag-in-imx6/m-p/1800051#M219530</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Neither the S32G and i.MX uses DEP / NX.&lt;/P&gt;
&lt;P&gt;DEP is used by default in Ubuntu. This is done via the NX bit if the CPU supports it, or emulated via memory segmentation if the CPU does not support it. For more details, see the &lt;A href="https://wiki.ubuntu.com/Security/Features#nx" target="_blank"&gt;non-executable memory feature item&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
    <pubDate>Thu, 01 Feb 2024 15:32:09 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-02-01T15:32:09Z</dc:date>
    <item>
      <title>Cannot check DEP/NX flag in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-check-DEP-NX-flag-in-imx6/m-p/1799780#M219515</link>
      <description>&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I built my image for imx6 board with yocto project that uses meta-freescale bsp.&lt;/P&gt;&lt;P&gt;Currently, we want to check if DEP/NX is enable but cannot find any information from:&lt;/P&gt;&lt;P&gt;dmesg | grep NX&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;also in cat /proc/cpuinfo, there is no "nx" flag.&lt;/P&gt;&lt;BLOCKQUOTE&gt;&lt;P&gt;processor : 0&lt;BR /&gt;BogoMIPS : 10.00&lt;BR /&gt;Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid&lt;BR /&gt;CPU implementer : 0x41&lt;BR /&gt;CPU architecture: 8&lt;BR /&gt;CPU variant : 0x0&lt;BR /&gt;CPU part : 0xd03&lt;BR /&gt;CPU revision : 4&lt;/P&gt;&lt;P&gt;processor : 1&lt;BR /&gt;BogoMIPS : 10.00&lt;BR /&gt;Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid&lt;BR /&gt;CPU implementer : 0x41&lt;BR /&gt;CPU architecture: 8&lt;BR /&gt;CPU variant : 0x0&lt;BR /&gt;CPU part : 0xd03&lt;BR /&gt;CPU revision : 4&lt;/P&gt;&lt;P&gt;processor : 2&lt;BR /&gt;BogoMIPS : 10.00&lt;BR /&gt;Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid&lt;BR /&gt;CPU implementer : 0x41&lt;BR /&gt;CPU architecture: 8&lt;BR /&gt;CPU variant : 0x0&lt;BR /&gt;CPU part : 0xd03&lt;BR /&gt;CPU revision : 4&lt;/P&gt;&lt;P&gt;processor : 3&lt;BR /&gt;BogoMIPS : 10.00&lt;BR /&gt;Features : fp asimd evtstrm aes pmull sha1 sha2 crc32 cpuid&lt;BR /&gt;CPU implementer : 0x41&lt;BR /&gt;CPU architecture: 8&lt;BR /&gt;CPU variant : 0x0&lt;BR /&gt;CPU part : 0xd03&lt;BR /&gt;CPU revision : 4&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I only check the other board S32G with meta-alb but still the same, I cannot check if flag DEP/NX is enable.&lt;BR /&gt;Could you please let me know if NXP board support NX bit? Or are there any bugs in BSP?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 01 Feb 2024 09:51:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-check-DEP-NX-flag-in-imx6/m-p/1799780#M219515</guid>
      <dc:creator>rockie_love_nxp</dc:creator>
      <dc:date>2024-02-01T09:51:34Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot check DEP/NX flag in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-check-DEP-NX-flag-in-imx6/m-p/1800051#M219530</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Neither the S32G and i.MX uses DEP / NX.&lt;/P&gt;
&lt;P&gt;DEP is used by default in Ubuntu. This is done via the NX bit if the CPU supports it, or emulated via memory segmentation if the CPU does not support it. For more details, see the &lt;A href="https://wiki.ubuntu.com/Security/Features#nx" target="_blank"&gt;non-executable memory feature item&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;regards&lt;/P&gt;</description>
      <pubDate>Thu, 01 Feb 2024 15:32:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-check-DEP-NX-flag-in-imx6/m-p/1800051#M219530</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-02-01T15:32:09Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot check DEP/NX flag in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-check-DEP-NX-flag-in-imx6/m-p/1800060#M219532</link>
      <description>&lt;P&gt;Hi Bio_TICFSL,&lt;/P&gt;&lt;P&gt;Thank you for your quick reply. So that means we cannot use DEP feature on i.MX series? Otherwise, should I implement it by myself?&lt;BR /&gt;As i read that from armv7, it's already supported XN bit. But I cannot find any method to test if that is used in Linux or not.&lt;/P&gt;</description>
      <pubDate>Thu, 01 Feb 2024 15:39:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-check-DEP-NX-flag-in-imx6/m-p/1800060#M219532</guid>
      <dc:creator>rockie_love_nxp</dc:creator>
      <dc:date>2024-02-01T15:39:31Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot check DEP/NX flag in imx6</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Cannot-check-DEP-NX-flag-in-imx6/m-p/1800905#M219578</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;in this case you should implement yourself.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 02 Feb 2024 14:24:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Cannot-check-DEP-NX-flag-in-imx6/m-p/1800905#M219578</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-02-02T14:24:37Z</dc:date>
    </item>
  </channel>
</rss>