<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCLK clarifications with SAI in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MCLK-clarifications-with-SAI/m-p/1799997#M219526</link>
    <description>&lt;P&gt;It isn't clear to me and I want to make sure I'm understanding the documentation correctly.&lt;/P&gt;&lt;P&gt;1. If we use the imx8m mini SAI as a slave then it is not necessary to use the imx8 MCLK, correct?&lt;/P&gt;&lt;P&gt;The documentation talks about using MCLK to generate the bit clock when master, but doesn't necessarily mention being used as a slave.&lt;/P&gt;&lt;P&gt;2. If we use the imx8m mini SAI5 as a master, it appears I can connect an external OSC to SAI2 MCLK and use that for SAI5.&amp;nbsp; Can I then output that same MCLK on the SAI5 MCLK pin?&lt;/P&gt;</description>
    <pubDate>Thu, 01 Feb 2024 14:42:52 GMT</pubDate>
    <dc:creator>imx_user8</dc:creator>
    <dc:date>2024-02-01T14:42:52Z</dc:date>
    <item>
      <title>MCLK clarifications with SAI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCLK-clarifications-with-SAI/m-p/1799997#M219526</link>
      <description>&lt;P&gt;It isn't clear to me and I want to make sure I'm understanding the documentation correctly.&lt;/P&gt;&lt;P&gt;1. If we use the imx8m mini SAI as a slave then it is not necessary to use the imx8 MCLK, correct?&lt;/P&gt;&lt;P&gt;The documentation talks about using MCLK to generate the bit clock when master, but doesn't necessarily mention being used as a slave.&lt;/P&gt;&lt;P&gt;2. If we use the imx8m mini SAI5 as a master, it appears I can connect an external OSC to SAI2 MCLK and use that for SAI5.&amp;nbsp; Can I then output that same MCLK on the SAI5 MCLK pin?&lt;/P&gt;</description>
      <pubDate>Thu, 01 Feb 2024 14:42:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCLK-clarifications-with-SAI/m-p/1799997#M219526</guid>
      <dc:creator>imx_user8</dc:creator>
      <dc:date>2024-02-01T14:42:52Z</dc:date>
    </item>
    <item>
      <title>Re: MCLK clarifications with SAI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCLK-clarifications-with-SAI/m-p/1801171#M219597</link>
      <description>&lt;P&gt;Hello, I hope you are doing well.&lt;/P&gt;
&lt;P&gt;1. Yes, that is correct.&lt;/P&gt;
&lt;P&gt;2. Could you please share me a diagram of desired connection? Maybe you could use SAI5 as master to provide clock signals to SAI2 working as slave.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Sat, 03 Feb 2024 03:52:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCLK-clarifications-with-SAI/m-p/1801171#M219597</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2024-02-03T03:52:00Z</dc:date>
    </item>
    <item>
      <title>Re: MCLK clarifications with SAI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCLK-clarifications-with-SAI/m-p/1801985#M219656</link>
      <description>&lt;P&gt;Thank you.&amp;nbsp; I believe you've answered my questions as I can do the first option.&amp;nbsp;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Feb 2024 15:24:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCLK-clarifications-with-SAI/m-p/1801985#M219656</guid>
      <dc:creator>imx_user8</dc:creator>
      <dc:date>2024-02-05T15:24:48Z</dc:date>
    </item>
    <item>
      <title>Re: MCLK clarifications with SAI</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MCLK-clarifications-with-SAI/m-p/1859751#M223333</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/229009"&gt;@imx_user8&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am also suffering the clock configuration similar with your No.2 question, would you please share how to configure? Thanks&lt;/P&gt;&lt;P&gt;My application is that, SAI2 MCLK came from external IC, we want to reuse SAI2 MCLK for PDM clock.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 06 May 2024 13:53:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MCLK-clarifications-with-SAI/m-p/1859751#M223333</guid>
      <dc:creator>zouhui</dc:creator>
      <dc:date>2024-05-06T13:53:04Z</dc:date>
    </item>
  </channel>
</rss>