<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Display Port max resolution on IMX8QM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Display-Port-max-resolution-on-IMX8QM/m-p/1798225#M219410</link>
    <description>&lt;P&gt;for imx8qm hdmi support:&lt;/P&gt;
&lt;P&gt;- HDMI -&amp;gt; 4K@60 &lt;BR /&gt;For HDMI 4K@60 you have to combine DC0-0 and DC0-1, which means you lose MIPI-DSI0 and LVDS0,&lt;BR /&gt;conversely if you use either of those interfaces you are limited to HDMI 4K30.&lt;/P&gt;</description>
    <pubDate>Wed, 31 Jan 2024 03:30:37 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2024-01-31T03:30:37Z</dc:date>
    <item>
      <title>Display Port max resolution on IMX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Port-max-resolution-on-IMX8QM/m-p/1798013#M219391</link>
      <description>&lt;P&gt;Hello, I'm looking at using the Display Port capabilities of the HDMI_TX on the IMX8QM and found in the imx-hdp.c driver that the resolution is capped to a max of 4k. The Display Port 1.3 spec supports up to 8k resolution, albeit at 30Hz.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="whitedouglasc_0-1706644749791.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/260864i85650D848CC9C98D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="whitedouglasc_0-1706644749791.png" alt="whitedouglasc_0-1706644749791.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am curious as to the cause of the 4k resolution cap. Is there a hardware limitation preventing any greater resolution or is there a newer version of the driver that removes the limits?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Tue, 30 Jan 2024 19:59:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Port-max-resolution-on-IMX8QM/m-p/1798013#M219391</guid>
      <dc:creator>whitedouglasc</dc:creator>
      <dc:date>2024-01-30T19:59:33Z</dc:date>
    </item>
    <item>
      <title>Re: Display Port max resolution on IMX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Port-max-resolution-on-IMX8QM/m-p/1798225#M219410</link>
      <description>&lt;P&gt;for imx8qm hdmi support:&lt;/P&gt;
&lt;P&gt;- HDMI -&amp;gt; 4K@60 &lt;BR /&gt;For HDMI 4K@60 you have to combine DC0-0 and DC0-1, which means you lose MIPI-DSI0 and LVDS0,&lt;BR /&gt;conversely if you use either of those interfaces you are limited to HDMI 4K30.&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 03:30:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Port-max-resolution-on-IMX8QM/m-p/1798225#M219410</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-01-31T03:30:37Z</dc:date>
    </item>
    <item>
      <title>Re: Display Port max resolution on IMX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Port-max-resolution-on-IMX8QM/m-p/1798841#M219455</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for the feedback. In my application it is fine to lose the DSI and LVDS interfaces. Display Port will be the only video interface used.&lt;/P&gt;&lt;P&gt;Given this information, is it not possible to exceed 4k resolution even at a lower refresh rate? I thought Display Port 1.3 supported 8k 30Hz while in SST mode.&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 15:19:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Port-max-resolution-on-IMX8QM/m-p/1798841#M219455</guid>
      <dc:creator>whitedouglasc</dc:creator>
      <dc:date>2024-01-31T15:19:26Z</dc:date>
    </item>
    <item>
      <title>Re: Display Port max resolution on IMX8QM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Display-Port-max-resolution-on-IMX8QM/m-p/1799601#M219505</link>
      <description>&lt;P&gt;couldn't support 8k&lt;/P&gt;</description>
      <pubDate>Thu, 01 Feb 2024 07:18:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Display-Port-max-resolution-on-IMX8QM/m-p/1799601#M219505</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2024-02-01T07:18:11Z</dc:date>
    </item>
  </channel>
</rss>