<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックLTIB build error for i.mx53</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-build-error-for-i-mx53/m-p/247852#M21935</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using LTIB to build rootfs for i.mx53 platform. I am using ubuntu 10.04 as host machine but when I run ./ltib I am getting the following error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Build path taken because: download only, no prebuilt rpm, &lt;/P&gt;&lt;P&gt;Testing network connectivity&lt;/P&gt;&lt;P&gt;No network download connection available&lt;/P&gt;&lt;P&gt;Can't get: rpm-4.0.4.tar.gz at ./ltib line 790.&lt;/P&gt;&lt;P&gt;could not glob rpm in: /tmp/rpm-akhil/RPMS/i686/rpm-fs-* at ./ltib line 2408.&lt;/P&gt;&lt;P&gt;traceback:&lt;/P&gt;&lt;P&gt; main::check_rpm_setup:2408&lt;/P&gt;&lt;P&gt; main::host_checks:1423&lt;/P&gt;&lt;P&gt; main:542&lt;/P&gt;&lt;P&gt;These packages failed to build&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think it is not detecting network proxy, how to change the proxy in .ltibrc file(I am not finding this file as mentioned in docs.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Sep 2013 09:53:40 GMT</pubDate>
    <dc:creator>akhiljhanwar</dc:creator>
    <dc:date>2013-09-24T09:53:40Z</dc:date>
    <item>
      <title>LTIB build error for i.mx53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-build-error-for-i-mx53/m-p/247852#M21935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using LTIB to build rootfs for i.mx53 platform. I am using ubuntu 10.04 as host machine but when I run ./ltib I am getting the following error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Build path taken because: download only, no prebuilt rpm, &lt;/P&gt;&lt;P&gt;Testing network connectivity&lt;/P&gt;&lt;P&gt;No network download connection available&lt;/P&gt;&lt;P&gt;Can't get: rpm-4.0.4.tar.gz at ./ltib line 790.&lt;/P&gt;&lt;P&gt;could not glob rpm in: /tmp/rpm-akhil/RPMS/i686/rpm-fs-* at ./ltib line 2408.&lt;/P&gt;&lt;P&gt;traceback:&lt;/P&gt;&lt;P&gt; main::check_rpm_setup:2408&lt;/P&gt;&lt;P&gt; main::host_checks:1423&lt;/P&gt;&lt;P&gt; main:542&lt;/P&gt;&lt;P&gt;These packages failed to build&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think it is not detecting network proxy, how to change the proxy in .ltibrc file(I am not finding this file as mentioned in docs.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Sep 2013 09:53:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-build-error-for-i-mx53/m-p/247852#M21935</guid>
      <dc:creator>akhiljhanwar</dc:creator>
      <dc:date>2013-09-24T09:53:40Z</dc:date>
    </item>
    <item>
      <title>Re: LTIB build error for i.mx53</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/LTIB-build-error-for-i-mx53/m-p/247853#M21936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may want to try to edit the &lt;EM&gt;etc/enviroment &lt;/EM&gt;file.&lt;/P&gt;&lt;P&gt;Yoy can set the proxy values in that file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2013 15:56:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/LTIB-build-error-for-i-mx53/m-p/247853#M21936</guid>
      <dc:creator>SergioSolis</dc:creator>
      <dc:date>2013-10-01T15:56:35Z</dc:date>
    </item>
  </channel>
</rss>