<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUsing external RTC from SCFW in IMX8QXP based board</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Using-external-RTC-from-SCFW-in-IMX8QXP-based-board/m-p/1796729#M219288</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have an external RTC on my custom board, which is connected to the SCU I2C. Could someone please confirm whether I can use it or not from SCFW?&lt;/P&gt;&lt;P&gt;Will I be only able to use the SNVS RTC from SCFW?&lt;/P&gt;&lt;P&gt;Will there be any internal driver which can communicate to an external RTC? Could someone please point me in the right direction?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 29 Jan 2024 09:11:02 GMT</pubDate>
    <dc:creator>_asif_muhammed_</dc:creator>
    <dc:date>2024-01-29T09:11:02Z</dc:date>
    <item>
      <title>Using external RTC from SCFW in IMX8QXP based board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-external-RTC-from-SCFW-in-IMX8QXP-based-board/m-p/1796729#M219288</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have an external RTC on my custom board, which is connected to the SCU I2C. Could someone please confirm whether I can use it or not from SCFW?&lt;/P&gt;&lt;P&gt;Will I be only able to use the SNVS RTC from SCFW?&lt;/P&gt;&lt;P&gt;Will there be any internal driver which can communicate to an external RTC? Could someone please point me in the right direction?&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/60336"&gt;@kerryzhou&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jan 2024 09:11:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-external-RTC-from-SCFW-in-IMX8QXP-based-board/m-p/1796729#M219288</guid>
      <dc:creator>_asif_muhammed_</dc:creator>
      <dc:date>2024-01-29T09:11:02Z</dc:date>
    </item>
    <item>
      <title>Re: Using external RTC from SCFW in IMX8QXP based board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-external-RTC-from-SCFW-in-IMX8QXP-based-board/m-p/1796943#M219316</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Should it be SC_R_SNVS (since that's where the RTC is located).&amp;nbsp; Please check it:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Timer-service/ta-p/1129194" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/System-Controller-Firmware-101-Timer-service/ta-p/1129194&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 29 Jan 2024 15:20:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-external-RTC-from-SCFW-in-IMX8QXP-based-board/m-p/1796943#M219316</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-01-29T15:20:41Z</dc:date>
    </item>
    <item>
      <title>Re: Using external RTC from SCFW in IMX8QXP based board</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Using-external-RTC-from-SCFW-in-IMX8QXP-based-board/m-p/1798266#M219417</link>
      <description>&lt;P&gt;Thank you Bio_TICFSL.I have gone through the document. It seems that it is an &lt;STRONG&gt;internal&lt;/STRONG&gt; RTC of SNVS.&lt;/P&gt;&lt;P&gt;Is it possible to interface an &lt;STRONG&gt;external&lt;/STRONG&gt; RTC to the SCU via the SCU_I2C?&lt;/P&gt;</description>
      <pubDate>Wed, 31 Jan 2024 04:58:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Using-external-RTC-from-SCFW-in-IMX8QXP-based-board/m-p/1798266#M219417</guid>
      <dc:creator>_asif_muhammed_</dc:creator>
      <dc:date>2024-01-31T04:58:02Z</dc:date>
    </item>
  </channel>
</rss>