<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX 8M Plus DDR inline ECC in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-DDR-inline-ECC/m-p/1795987#M219241</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to use the ECC feature of LPDDR4 memory with i.MX8MP. To do that, I enabled inline ECC with the i.MX 8 Register Programming Aid (RPA) tool and reflected the changes in lpddr4_timing.c. Then, when generating U-Boot, I set Device Drivers -&amp;gt; i.MX8M DDR controllers-&amp;gt;imx8mp inline ECC to Enable in menuconfig.&lt;/P&gt;&lt;P&gt;However, the following message is displayed when booting the Yocto Linux kernel, and the ECC feature is not enabled.&lt;/P&gt;&lt;DIV&gt;&lt;SPAN&gt;EDAC MC: Ver: 3.0.0&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;EDAC MC: ECC not enabled&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Please tell me if there are any missing steps or settings to use the ECC and EDAC features.&lt;/P&gt;</description>
    <pubDate>Fri, 26 Jan 2024 09:31:05 GMT</pubDate>
    <dc:creator>Fai1</dc:creator>
    <dc:date>2024-01-26T09:31:05Z</dc:date>
    <item>
      <title>i.MX 8M Plus DDR inline ECC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-DDR-inline-ECC/m-p/1795987#M219241</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I want to use the ECC feature of LPDDR4 memory with i.MX8MP. To do that, I enabled inline ECC with the i.MX 8 Register Programming Aid (RPA) tool and reflected the changes in lpddr4_timing.c. Then, when generating U-Boot, I set Device Drivers -&amp;gt; i.MX8M DDR controllers-&amp;gt;imx8mp inline ECC to Enable in menuconfig.&lt;/P&gt;&lt;P&gt;However, the following message is displayed when booting the Yocto Linux kernel, and the ECC feature is not enabled.&lt;/P&gt;&lt;DIV&gt;&lt;SPAN&gt;EDAC MC: Ver: 3.0.0&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;SPAN&gt;EDAC MC: ECC not enabled&lt;/SPAN&gt;&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Please tell me if there are any missing steps or settings to use the ECC and EDAC features.&lt;/P&gt;</description>
      <pubDate>Fri, 26 Jan 2024 09:31:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-DDR-inline-ECC/m-p/1795987#M219241</guid>
      <dc:creator>Fai1</dc:creator>
      <dc:date>2024-01-26T09:31:05Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 8M Plus DDR inline ECC</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-DDR-inline-ECC/m-p/2098153#M237256</link>
      <description>Hi, even i have the same issue. Did you find any solution for this ??&lt;BR /&gt;Please guide if so</description>
      <pubDate>Thu, 15 May 2025 12:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-8M-Plus-DDR-inline-ECC/m-p/2098153#M237256</guid>
      <dc:creator>Rajashekar-Bommideni</dc:creator>
      <dc:date>2025-05-15T12:48:20Z</dc:date>
    </item>
  </channel>
</rss>