<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Unable to handle kernel NULL pointer dereference at virtual address (iMX8MMini)</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-handle-kernel-NULL-pointer-dereference-at-virtual/m-p/1795470#M219211</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes it looks like a bug I will reported immediately thanks for the catch!.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Thu, 25 Jan 2024 14:22:28 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2024-01-25T14:22:28Z</dc:date>
    <item>
      <title>Unable to handle kernel NULL pointer dereference at virtual address (iMX8MMini)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-handle-kernel-NULL-pointer-dereference-at-virtual/m-p/1794790#M219160</link>
      <description>&lt;P&gt;I have a custom board with i.MX8Mini and LPDDR4 RAM, connected to a MIPI CSI2 (DPHY) camera streaming 1080p30.&lt;/P&gt;&lt;P&gt;We have a test application based on GStreamer that stops and starts video streaming every few seconds.&lt;/P&gt;&lt;P&gt;the application triggers a crash in the v4l2 driver stack after several cycles. This can range from 50 stop/start cycles to 100s or 1000s.&lt;/P&gt;&lt;P&gt;The callstack is always the same. The crash happens in the vb2_buffer_done(), and we think it may be the call to “atomic_dec(&amp;amp;q-&amp;gt;owned_by_drv_count);” in this function that triggers it. For a given image (OS + application), the virtual address is always the same (in the CS below 0x1f8).&lt;/P&gt;&lt;P&gt;Any idea what could be going wrong? Has something like this been reported already?&lt;/P&gt;&lt;P&gt;Nov 11 23:08:48 imx8mmbluebird kernel: Unable to handle kernel NULL pointer dereference at virtual address 00000000000001f8&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: Mem abort info:&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: ESR = 0x96000006&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: Exception class = DABT (current EL), IL = 32 bits&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: SET = 0, FnV = 0&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: EA = 0, S1PTW = 0&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: Data abort info:&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: ISV = 0, ISS = 0x00000006&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: CM = 0, WnR = 0&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: user pgtable: 4k pages, 48-bit VAs, pgdp = 0000000037ca5943&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: [00000000000001f8] pgd=000000004e2bc003, pud=000000004e296003, pmd=0000000000000000&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: Internal error: Oops: 96000006 [#1] PREEMPT SMP&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: Modules linked in: crc32_ce crct10dif_ce mxc_mipi_csi mx6s_capture gs3470_asl XXXXXXXXXXXXX_camera_mipi overlay galcore(O)&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: Process onvif_rtsp_app (pid: 3598, stack limit = 0x0000000097265435)&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: CPU: 0 PID: 3598 Comm: XXXXXXXXXXXXX Tainted: G O 4.19.35-1.1.0+g9ec518e5baca #1&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: Hardware name: XXXXXXXXXXXXX based on i.MX8MM - rev 6 (Burst) (DT)&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: pstate: 20000085 (nzCv daIf -PAN -UAO)&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: pc : __ll_sc___cmpxchg_case_acq_4+0x4/0x20&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: lr : _raw_spin_lock_irqsave+0x34/0x60&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: sp : ffff0000172aba20&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x29: ffff0000172aba20 x28: ffff800013f72300&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x27: ffff00000973b710 x26: ffff00000973b710&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x25: ffff80000ea14bd0 x24: ffff80000ea14930&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x23: 00000000000001f8 x22: 0000000000000007&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x21: 0000000000000000 x20: ffff80000ea14ad8&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x19: 0000000000000080 x18: 0000000000000000&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x17: 0000000000000000 x16: 0000000000000000&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x15: 0000000000000000 x14: 0000000000000000&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x13: 0000000000000000 x12: 0000000000000000&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x11: 0000000000000000 x10: 0000000000000000&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x9 : 0000000000000000 x8 : 0000000000000000&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x7 : 0000000000000200 x6 : 0000000000000000&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x5 : 0000000000000000 x4 : ffff80000ea14c88&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x3 : 00000000000001f8 x2 : 0000000000000001&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: x1 : 0000000000000000 x0 : 00000000000001f8&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: Call trace:&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: __ll_sc___cmpxchg_case_acq_4+0x4/0x20&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: vb2_buffer_done+0xa4/0x1b0&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: mx6s_stop_streaming+0xbc/0x298 [mx6s_capture]&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: __vb2_queue_cancel+0x2c/0x1c8&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: vb2_core_streamoff+0x20/0xa8&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: vb2_streamoff+0x18/0x60&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: mx6s_vidioc_streamoff+0x58/0xc0 [mx6s_capture]&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: v4l_streamoff+0x20/0x28&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: __video_do_ioctl+0x248/0x498&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: video_usercopy+0x268/0x4d0&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: video_ioctl2+0x14/0x20&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: v4l2_ioctl+0x40/0x118&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: do_vfs_ioctl+0xb8/0x890&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: ksys_ioctl+0x78/0xa8&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: __arm64_sys_ioctl+0x1c/0x28&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: el0_svc_common+0x84/0xf0&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: el0_svc_handler+0x2c/0x80&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: el0_svc+0x8/0xc&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: Code: 35ffff91 aa1003e0 d65f03c0 f9800011 (885ffc10)&lt;BR /&gt;Nov 11 23:08:48 imx8mmbluebird kernel: ---[ end trace 16bd3712444c4359 ]---&lt;/P&gt;</description>
      <pubDate>Wed, 24 Jan 2024 17:32:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-handle-kernel-NULL-pointer-dereference-at-virtual/m-p/1794790#M219160</guid>
      <dc:creator>vincentz63</dc:creator>
      <dc:date>2024-01-24T17:32:28Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to handle kernel NULL pointer dereference at virtual address (iMX8MMini)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-handle-kernel-NULL-pointer-dereference-at-virtual/m-p/1795470#M219211</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Yes it looks like a bug I will reported immediately thanks for the catch!.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Thu, 25 Jan 2024 14:22:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-handle-kernel-NULL-pointer-dereference-at-virtual/m-p/1795470#M219211</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2024-01-25T14:22:28Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to handle kernel NULL pointer dereference at virtual address (iMX8MMini)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Unable-to-handle-kernel-NULL-pointer-dereference-at-virtual/m-p/1819764#M220677</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Any progress on this?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 18:17:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Unable-to-handle-kernel-NULL-pointer-dereference-at-virtual/m-p/1819764#M220677</guid>
      <dc:creator>vincentz63</dc:creator>
      <dc:date>2024-03-01T18:17:39Z</dc:date>
    </item>
  </channel>
</rss>